Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Thuis #6: Installing the Raspberry Pi 3 in practice
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
  • Author Author: rhe123
  • Date Created: 26 Jun 2016 1:01 PM Date Created
  • Views 1593 views
  • Likes 3 likes
  • Comments 5 comments
  • z-wave
  • piiot
  • chef
  • wildfly
  • raspberrypi3
  • thuis
Related
Recommended

[Pi IoT] Thuis #6: Installing the Raspberry Pi 3 in practice

rhe123
rhe123
26 Jun 2016

Last week I explained how I'm using Chef to provision my Raspberry Pi's and the recipes in my Thuis cookbook. Back then I didn't have a Raspberry Pi 3 yet, so I tested it on an older model. This week the kit arrived, so I'll bring the bootstrapping in practice on the Raspberry Pi 3! Not everything went as expected, so this is a good subject for this blogpost.

 

The Kit

image

 

Installing the Raspberry Pi 3

As mentioned before I'm using raspbian-ua-netinst as a basis for my install, as this gives me a very lean install of Raspbian. The maintainers of the projects didn't update the installer yet for the Raspberry Pi 3, so there are some manual steps to go through for now. This is discussed in issue #375. It boils down to the following steps:

  1. Format the SD card
  2. Copy all files from the latest version to the SD card
  3. Fix the files for the Raspberry Pi 3:
    1. Copy (replace all) the files from the firmware repo using the handy tarball made by @eLvErDe
    2. Edit /boot/config.txt by adding the following at the end:

      [pi3] initramfs installer-rpi2.cpio.gz

  4. Insert the SD card in the Raspberry Pi and power it on
  5. Now wait until the installation finishes (it will take quite some time, when you don't have a screen attached wait until the ethernet connection becomes silent)
  6. SSH into the Raspberry using the default username root and password raspbian
  7. Now fix the kernel by installing and running rpi-update:

    apt-get install rpi-update rpi-update reboot now

  8. Edit /boot/config.txt again by changing [pi2] into [pi3]

 

The Raspberry Pi is now ready to be bootstrapped.

 

Bootstrapping Chef

Bootstrapping Chef is a matter of running one simple command from my workstation:

knife bootstrap 10.0.0.201 -t raspbian-jessie-chef.erb --ssh-user root --ssh-password 'raspbian' --node-name 'thuis-server-core' --run-list 'recipe[thuis::thuis-server-core]'

However I ran into a few complications. During my testing I didn't run into these because of the iterative process and some differences between the hardware of the two Raspberries.

 

Complication 1: systemd needs services to be reloaded

After installing WildFly the recipe tries to start the services; this however fails with a cryptic No such file or directory. The reason for this happens to be that systemd needs to be reloaded after adding new init-scripts. The WildFly recipe doesn't take care of this and therefor runs into the issue. To resolve the issue I forked the cookbook and added a systemctl daemon-reload command to it (see PR #38). This ensures it can start WildFly as expected.

 

Complication 2: For Z-Way bluetooth needs to be turned off

The RazBerry uses the serial IO pins on the Raspberry Pi, the same are used by the built-in Bluetooth connection as well. To be able to use the RazBerry and run Z-Way, Bluetooth has to be disabled. The original install script takes care of this, but after I converted it to be used in a Chef cookbook this didn't work anymore. That's why I converted these commands to Ruby blocks in my Chef recipe now. This looks as follows:image

ruby_block '/etc/inittab' do
 block do
  file = Chef::Util::FileEdit.new('/etc/inittab')
  file.search_file_delete_line(/[^:]*:[^:]*:respawn:\/sbin\/getty[^:]*ttyAMA0[^:]*/)
  file.write_file
 end
end

ruby_block '/boot/cmdline.txt' do
 block do
  file = Chef::Util::FileEdit.new('/boot/cmdline.txt')
  file.search_file_delete(/console=ttyAMA0,115200/)
  file.search_file_delete(/kgdboc=ttyAMA0,115200/)
  file.search_file_delete(/console=serial0,115200/)
  file.write_file
 end
end

ruby_block '/boot/config.txt' do
 block do
  file = Chef::Util::FileEdit.new('/boot/config.txt')
  file.insert_line_if_no_match(/dtoverlay=pi3-miniuart-bt/, 'dtoverlay=pi3-miniuart-bt')
  file.write_file
 end
end

 

Basically this deletes the serial connections from /etc/inittab and /boot/cmdline.txt and adds an option to /boot/config.txt to disable Bluetooth.

 

Complication 3: sudo commands not found

When trying to do a command using sudo, e.g. sudo shutdown now I got a Command not found error. This happens because /sbin and other secure directories are not on the PATH for a non-root user. When you use sudo it should be and for this a small piece of configuration is added for the sudo cookbook:

default['authorization']['sudo']['sudoers_defaults'] = [
  'env_reset',
  'secure_path="/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin"'
]

 

Configuring Z-Way

As I already have a working Z-Way setup at home the configuration is pretty easy. It boils down to:

  1. Browse to http://10.0.0.201:8083 (where 10.0.0.201 is the IP of your Raspberry)
  2. Choose a password of your own choice
  3. Restore the backups:
    1. For the controller (*.zbk): http://10.0.0.201:8083/expert/#/network/control
    2. And for the module automation (*.zab): http://10.0.0.201:8083/smarthome/#/admin
    3. If you used userModules then copy or install these again (their settings are part of the backup, but not the actual files)

 

Deploying an application to WildFly

This is easy as dropping an .ear of .war file to /opt/wildfly/standalone/deployments. Alternatively you can deploy the app as part of a Chef recipe like:

wildfly_deploy 'my-app-1.0.war' do
  url 'http://artifacts.company.com/artifacts/my-app.1.0.war'
  runtime_name 'my-app.war'
end

 

In the upcoming blogs I'll work on the Java app and integrating Z-Way with MQTT, then we'll do the actual deployment.

 

With the complications out of the way, the Raspberry Pi 3 is now fully ready to receive some app deployments, which is what I'll work on now!

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago in reply to georgekav +3
    Using the "enable_uart" property, as I did, the UART0 can again be used for serial communication with any HAT, like EnOceanPi. The BT is then moved to the miniUART, and is still usable. No need to cripple…
  • fvan
    fvan over 10 years ago +1
    Did you try the "enable_uart" property in the "/boot/config.txt" ? It restores the UART, and keeps the BT operational. The UART interface is then "ttyS0" instead of "ttyAMA0" though. It's described in…
  • georgekav
    georgekav over 10 years ago in reply to fvan +1
    I had also to disable bluetooth and remap uart for the enocean pi to work properly using the hardware uart0 like rhe123 . Also basically the recommended by enocean (paper titled: Raspberry Pi talks EnOcean…
Parents
  • fvan
    fvan over 10 years ago

    Did you try the "enable_uart" property in the "/boot/config.txt"? It restores the UART, and keeps the BT operational. The UART interface is then "ttyS0" instead of "ttyAMA0" though.

    It's described in my EnOceanPi paragraph: https://www.element14.com/community/community/design-challenges/pi-iot/blog/2016/06/14/pi-iot-alarm-clock-05-enocean-sen…

     

    Frederick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rhe123
    rhe123 over 10 years ago in reply to fvan

    That might indeed work as well! RazBerry suggests to turn off Bluetooth themselves, and I don't need Bluetooth, so I didn't look further. If I have some time left, I might try it. Thanks fvan! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rhe123
    rhe123 over 10 years ago in reply to fvan

    That might indeed work as well! RazBerry suggests to turn off Bluetooth themselves, and I don't need Bluetooth, so I didn't look further. If I have some time left, I might try it. Thanks fvan! image