PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Adapting Art to Viewers: Demonstration, Blog #10
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
  • Author Author: fmilburn
  • Date Created: 4 May 2019 12:41 AM Date Created
  • Views 4542 views
  • Likes 12 likes
  • Comments 25 comments
  • picasso
  • 3D Printing
  • picasso_desing
  • image recognition
  • raspberry pi camera v2
  • raspberry pi 3b+
  • ai
  • art
  • picasso_design_challenge
  • pi face
Related
Recommended

PiCasso Adapting Art to Viewers: Demonstration, Blog #10

fmilburn
fmilburn
4 May 2019

Art is often made to appeal to a specific set of viewers.  This is the 10th blog in a series exploring the idea of using AI to recognize a viewer and adapt art to their age or interest.  The intent is to encourage early art appreciation while being attractive to all household members.

image

In previous posts the build, facial recognition, art, and art viewer have been presented individually as the phases of the project progressed.  In this post the integrated project is demonstrated and compared to the original concept.  The block diagram is updated.

 

Updated Block Diagram

 

There have been several changes as the project progressed and these are reflected in the revised block diagram.  The more significant changes are:

  • Ultrasonic sensor removed - OpenCV and the camera do a good job sensing people and an ultrasonic sensor is not required
  • Pi Face and physical movement not implemented - this may be implemented in future but the current design has limited space to add the feature

image

 

Video Demonstration

 

I tidied up the wiring a bit and now have the full package working.  The integrated hardware and software is demonstrated in the following video.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hardware Happy Hour

 

There is a Hardware Happy Hour monthly here in Seattle where a group gets together at one of the local brew pubs and shows things they are working on.  If you are in Seattle the first Thursday of the month be sure and drop by. I had the PiCasso Art Deluxe on display last night and the retro look got a lot of attention as well as "what does it do?"...

image

 

Upcoming Work

 

While the original specifications and goals for the project have been largely met additional enhancements and refinements are planned.  There may not be another posting for a week or two due to personal commitments and the nature of the remaining work.  Upcoming work includes:

 

  • Refinement
  • Additional art
  • Final demonstration video
  • Completed documentation

 

Thanks for reading - comments and suggestions are always welcome.

 

Blogs in this Series

PiCasso Adapting Art to Viewers: Introduction  Blog #1

PiCasso Adapting Art to Viewers: OpenCV Face Detection, Blog #2

PiCasso Adapting Art to Viewers: Cabinet Design, Blog #3

PiCasso Adapting Art to Viewers: Pi talks to Pi, Blog #4

PiCasso Adapting Art to Viewers: Grandpa Shark, Blog #5

PiCasso Adapting Art to Viewers: More on Cabinet Design, Blog #6

PiCasso Adapting Art to Viewers:  New Art, Blog #7

PiCasso Adapting Art to Viewers:  Mechanical Complete, Blog #8

PiCasso Adapting Art to Viewers:  Displaying Art, Blog #9

PiCasso Adapting Art to Viewers:  Demonstration, Blog #10

  • Sign in to reply

Top Comments

  • gecoz
    gecoz over 7 years ago +5
    Hi Frank, Excellent work! It would make as great intelligent photo frame as well, displaying photo albums according to the person facing the frame. As for improving the recognition accuracy, even when…
  • ralphjy
    ralphjy over 7 years ago +4
    Great to see it all working. That must have been worth a few beers
  • dubbie
    dubbie over 7 years ago +4
    Frank, A great all round project. It looks good and it works. I'm impressed with the tidy wires. I'm having an untidy wire situation at the present so any ideas on how to move to a tidy wire situation…
Parents
  • ralphjy
    ralphjy over 7 years ago

    Great to see it all working.  That must have been worth a few beersimage

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to ralphjy

    Yes, a beer was in order image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago in reply to ralphjy

    Yes, a beer was in order image