• Products and Partners
    Products and Partners
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
Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Smart Range Hood - Blog Post #3 - Mechanical design complete!
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
  • Author Author: aspork42
  • Date Created: 4 Feb 2018 6:57 AM Date Created
  • Views 3003 views
  • Likes 8 likes
  • Comments 12 comments
  • home automation
  • pi chef design challenge
  • pi chef
Related
Recommended

Smart Range Hood - Blog Post #3 - Mechanical design complete!

aspork42
aspork42
4 Feb 2018

Greetings!

Goal: a smart, connected range hood to send images of what's cooking and to alert the user if something doesn't seem right.

First post and links to all of my other posts for this project - Smart Range Hood - Pi Chef Challenge Blog post #1

 

PDF, STP, STL, .ipt, and .iam files are all linked to this post for anyone brave enough to make their own image

 

I have completed my mechanical design for the range hood. This will consist of two pieces of sheet metal bent up by a local fabricator to meet my specifications. For many reasons, this feels like a major hurdle that I have crossed since it has been such a long time in the works.

 

This took many hours of measuring, remeasuring, remeasuring again, then all the CAD work - I spent a lot of time trying to get the "contour flange" to work properly in order for the front panel to lay out properly. Many hours of trying, reading tutorials, doing lessons, and watching videos on YouTube were required to achieve this finished portion of the project. I know that most the focus of this Newark Design Challenge will be related to the electrical architecture, controls, and wiring, but for my project the sheet metal represents a significant portion. This is doubly true since the goal will include the fact that this is a permanent fixture in our house and will outlive our tenure here - I need to make it good enough that when we sell our house it can stay. Granted that the RaspberryPi will be removed and the normal controls will be replaced; but the rest will be here for a long time to come. If for any reason the new hood can't arrive and be integrated in time, the doner hood will be used as a substitute. I can validate all features through using it as a stand-in.

 

But fear not, nerds! Most the rest of the blogs from here on out will focus on getting the electrons to bend to my will!!!  image

 

Autodesk Inventor Assembly steps -

I took a quick video which shows the actual steps taken to design the hood. The measurements were a combination taken from tape measure, caliper, and a mashup between the original hood and the doner hood parts. I had to make the fan box from the doner hood fit into a new enclosure which subsequently fit into a 40 year old built-in cabinet system in my house. One example is the power entry - the two hoods have this located in a slightly different spot. I need to use all the electronics of the new hood, but physically locate them where the old hood had them.

 

Overview video -

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This video explains the design constraints of adapting the doner hood to a new design which works in the old opening.

 

Autodesk Inventor is a 3D modeling program which serves as a successor to Autodesk AutoCAD. Inventor is designed from the ground up as a 3D modeling program; as opposed to AutoCAD which is a 2D drafting program adapted for the 3rd dimension. This means that many features of Inventor are more intuitive to the actual design and manufacturing process and doubly true that creating 3D assemblies of multiple components becomes much easier. Creating "joints" and "constraints" in an assembly of multiple individual components allows the user to easily check for fitment, tolerances, and interferences very easily. In my case, I had to ensure that the insert had adequate room for the spring clips and was still able to press in and press out easily. I was able to model the two major components individually, then create an assembly which contains them both. The two pieces were "constrained" to each other allowing mechanical movement only in certain directions across certain planes. I could then manipulate the assembly based on these joints and constraints - I could move the insert back and forth to measure the travel; then ensure that the spring clips would work properly and still allow the user to remove the insert.

 

Flange and contour flanges - here are some links to the textbook methods of creating them. They made 90% of the model that I needed.

Flange in Inventor -

https://knowledge.autodesk.com/support/inventor-products/learn-explore/caas/CloudHelp/cloudhelp/2014/ENU/Inventor/files/GUID-66E7956A-E269-4108-93F0-1A795A94BF6B-htm.html

 

Contour flange in Inventor -

https://knowledge.autodesk.com/support/inventor-products/learn-explore/caas/CloudHelp/cloudhelp/2016/ENU/Inventor-Help/f…

 

Most of what was done in Inventor started with a very basic sketch. They say if you're drawing more than rectangles and circles, you're over-thinking things. I started with a rectangle which was 40.25" x 12". Then I used the "flange" tool which makes a bend in the sheet metal, and dictated that it be ~5" tall to create the rear panel. Then another flange was created on one end of the rectangle for the right side of the hood. The process continued of creating flanges and bending the part usually at 90 degrees and that got me through most of the design process. I created the bolt patterns using a "point" then creating a "hole" with them. This allows precise placement, and the hole feature allows many useful features such as counterbores and chamfers.

 

I spent a lot of time in this design process thinking about how to make the sheet metal easy to manufacture. I am only planning to make a single piece, so want the fabricator to be able to easily create it. I need to know that they probably won't make a lot of money on a job like this, and if they make any mistakes and have to start over then they will likely lose money. If I was creating this commercially I could think about it much differently - the fabricator would probably make a nice jig and the could afford to waste a few pieces here and there across the 1000's or more units they build.

 

Probably very difficult to make "one" copy of:

image

Probably much easier to make "one" copy of:

image

 

Another area I spent a lot of time on is relative to the placement of the sensors - I officially have the following which require being able to "sense" the range top - GridEye IR sensor, Raspberry Pi 8mp camera, DHT22 Temperature/Humidity sensor, and a total of four "MQ" air sensors.

image

I was considering using a replaceable panel on the insert which could have custom holes or a 3D printed section to hold the sensors. I later changed this to just some slots. This would be quite incognito for the current iteration as it will hide all the sensors; plus later on wouldn't look strange when this becomes a normal "dumb" range hood.

 

 

Here are the actual assembly steps shown in Inventor -

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Final major mechanical components -

Here are the final components - I have attached the .iam, .ipt, .pdf, .stp, and .stl files for all of this to the post (archive.zip). If you want anything else, please let me know. I sent the PDFs and also created a .dxf file for the manufacturer. The PDFs attached to this post show all the major dims of this component.

image

 

 

image

 

More information / Use caution when doing a project such as this!!!

Please keep in mind that a project like this requires working with mains voltage. In the US this is 110 volts AC - that is more than enough to maime/injure/kill a person, or burn down their house while they sleep. Besides the obvious of crossing wires or forgetting to shut off mains when installing, improper grounding can cause a voltage between the hood and the stove which could kill someone. I do not recommend anyone else perform this modifications themselves unless they are or consult a licensed electrician. If you die or burn down your house, this is not my fault but your own.

Attachments:
imageHood7.pdf
imageBottomInsert2-1.pdf
Archive.zip
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 8 years ago +5
    On a side note... "...This is doubly true since the goal will include the fact that this is a permanent fixture in our house and will outlive our tenure here - I need to make it good enough that when we…
  • gecoz
    gecoz over 8 years ago +2
    Hi James, Very nice work you have done there with the design of the new hood. One thing that got me thinking was the positioning of all your sensors behind the cut-out slots at the very front, between…
  • beacon_dave
    beacon_dave over 8 years ago in reply to aspork42 +2
    This 32x24 Melexis sensor about to be released goes up to 300degrees for the object temperature, but the device itself is still is only rated at 85degrees operating temperature: https://www.melexis.com…
Parents
  • gecoz
    gecoz over 8 years ago

    Hi James,

    Very nice work you have done there with the design of the new hood.

    One thing that got me thinking was the positioning of all your sensors behind the cut-out slots at the very front, between the 2 spotlights. I'm not sure that will be an ideal position for the GridEye. Judging from the marks left on your mat, the 2 spotlights generate quite some heat. Those 2 heat emitting sources are mounted quite close to the GridEye, and will likely interfere with it when switched on.

    Another possible issue could be due to the proximity of the GridEye with the fan and the hobs: the aspiration system will probably cause an air flow to hit the sensor, and vapour/fumes/grease might end up on the sensor's lens. Protecting the lens is not a trivial task, as you need to find the right material that is transparent to the IR spectrum the GridEye is sensitive to (5 to 13μm - Far IR). I remember trying placing the GridEye behind a common glass pane during the 1-WireRegistered Grid-EYERegistered Sensor w/Arduino-Compatible PCB Roadtest, and it completely obscured the sensor.

    Perhaps, before finalising your desing and commit to its production, it is worth try testing the sensor, placing it in different spots and check its response during normal operation (i.e. while cooking on the hobs).

    Keep up the great work.

    Fabio.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 8 years ago in reply to gecoz

    I ran into the same issue when I did my Smart backsplash - https://youtu.be/M_df6y9scc4  - I wanted a PIR motion sensor hidden in the wall so it would provide pathway illumination. The glass tile blocks most IR light. I settled for just the capicitive touch sensors and a light sensor (Which ended up with greatly reduced sensing ability).

     

    The bigger elephant in the room is the sensing range of the GridEye which only goes up to 80 C so even a lot of boiling water will saturate the pixels. I am hoping this doesn’t damage the sensor. I am choosing to pursue using it anyways as a proof of concept and will keep in mind that the sensor isn’t exactly suited for the task. I will reach out to some friends who know optics and see if they have any recommendation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 8 years ago in reply to gecoz

    I ran into the same issue when I did my Smart backsplash - https://youtu.be/M_df6y9scc4  - I wanted a PIR motion sensor hidden in the wall so it would provide pathway illumination. The glass tile blocks most IR light. I settled for just the capicitive touch sensors and a light sensor (Which ended up with greatly reduced sensing ability).

     

    The bigger elephant in the room is the sensing range of the GridEye which only goes up to 80 C so even a lot of boiling water will saturate the pixels. I am hoping this doesn’t damage the sensor. I am choosing to pursue using it anyways as a proof of concept and will keep in mind that the sensor isn’t exactly suited for the task. I will reach out to some friends who know optics and see if they have any recommendation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 8 years ago in reply to aspork42

    This 32x24 Melexis sensor about to be released goes up to 300degrees for the object temperature, but the device itself is still is only rated at 85degrees operating temperature:

    https://www.melexis.com/en/product/MLX90640/Far-Infrared-Thermal-Sensor-Array

     

    There is a lower resolution 16x4 one which may already be shipping:

    https://www.melexis.com/en/product/MLX90621/Far-Infrared-Sensor-Array-High-Speed-Low-Noise

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gecoz
    gecoz over 8 years ago in reply to aspork42

    The GridEye operating range and temperature range of measuring object is 0C - 80C for the High Gain model, and -20C - 100C for the Low Gain one.

    Although the temperature at the hobs is going to be well over 80C, I think you can still operate the sensor safely, considering that it will be located some 60cm-80cm away from the source. When I did some testing with boiled water, from a distance of about a meter, the sensor would only read temperature of about 60C, so it is reasonable to assume that, as long as the sensor in not in close proximity to the heat source, no damage will be done.

    Again, I think the best way to go about it is to do some testing and verify what is the "safe" distance for the sensor.

    Fabio.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to gecoz

    Isn't it only the 'narrow angle' version that goes up to 100C for the object temperature ?

    https://industrial.panasonic.com/cdbs/www-data/pdf/ADI8000/ADI8000C65.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gecoz
    gecoz over 8 years ago in reply to beacon_dave

    I believe the AMG8854M01 model the datasheet refers to is a special model, with narrow viewing angle. The reduction of the angle is probably obtained by positioning the optical lens differently respect to the rest of the AMG88xx family. The difference between the High Gain and the Low Gain models is related to the accuracy, which decreases with the gain amplification, with all models keeping the same viewing angle of 60 degrees. The AMG88xx Series datasheet on Digikey shows the different models of the series.

    Fabio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 8 years ago in reply to beacon_dave

    Hi Dave,

    The MLX90640 doesn’t appear to be shipping yet. The 16x4 is for sale at about $42 but senses only up to 80-85C depending on exact model. They do have a better low end range down to -20c. I have the camera taking images now so will see what things look like. My use case for this is a simple On/Off detection so exact temperature is not important.