Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog Bees Monitor With Predators Repellent # 2 - Getting Started
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: guillengap
  • Date Created: 27 Feb 2023 12:47 AM Date Created
  • Views 1594 views
  • Likes 10 likes
  • Comments 6 comments
  • save the bees
  • savethebeesch
  • nicla vision
  • openmv
  • lora
  • edge impulse
  • mkr1310
  • arduino
Related
Recommended

Bees Monitor With Predators Repellent # 2 - Getting Started

guillengap
guillengap
27 Feb 2023
Bees Monitor With Predators Repellent # 2 - Getting Started

Table of Contents

  • Introduction
  • Getting Started
  • Edge Impulse
  • Improving Edge Impulse Model
  • Testing The Machine Learning Model With OpenMV
  • Adding The Water Sprayer System
  • Testing The Water Sprayer System
  • IoT Ambient Monitoring System | Part1
  • IoT Ambient Monitoring System | Part2
  • Summary

**********************************************************************************************************************

In this post I will show you the basic configuration of the Arduino Pro Nicla Vision and Arduino MKR WAN 1310 programming boards.

Nicla Vision Setup

The Arduino Nicla Vision board is a ready-to-use, standalone camera for analyzing and processing images on the edge. Thanks to its 2MP color camera, smart 6-axis motion sensor, integrated microphone and distance sensor, it is suitable for asset tracking, object recognition and predictive maintenance.

image

In my case I configure my board with Arduino IDE version 1.8; wow we need to navigate to Tools > Board > Board Manager.

image

This will open up a new window, with all available cores. Find the one named Arduino Mbed OS Nicla Boards and install it.

image

When it is finished, it should say  "INSTALLED"  under the title. Exit the board manager, and go to Tools > Board > Arduino Mbed OS Nicla Boards. Here you can see all the Mbed boards listed, where you can select the board you are using. You have now successfully installed the core.

image

On Nicla Vision you can test an example code. So when you have selected the USB connection port of your board, please use the File > Examples > Nicla_Sense_System > Blink_Nicla

In my case, I successfully tested the Proximity Detection with Arduino Nicla Vision example. Below I show you the code:

#include "VL53L1X.h"
VL53L1X proximity;

bool blinkState = false;
int reading = 0;
int timeStart = 0;
int blinkTime = 2000;

void setup() {
  Serial.begin(115200);
  Wire1.begin();
  Wire1.setClock(400000); // use 400 kHz I2C
  proximity.setBus(&Wire1);


  pinMode(LEDB, OUTPUT);
  digitalWrite(LEDB, blinkState);

  if (!proximity.init()) {
    Serial.println("Failed to detect and initialize sensor!");
    while (1);
  }

  proximity.setDistanceMode(VL53L1X::Long);
  proximity.setMeasurementTimingBudget(10000);
  proximity.startContinuous(10);
}

void loop() {
  reading = proximity.read();
  Serial.println(reading);

  if (millis() - timeStart >= reading) {
    digitalWrite(LEDB, blinkState);
    timeStart = millis();

    blinkState = !blinkState;
  }
}

Here the VL53L1X library for Arduino

In my case the connection was via USB 2.0 through the COM12 port

image

You can see the demonstration in the video below:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Using the Nicla Vision Camera

Finally, we will test the camera of the Nicla Vision board. First we download the OpenMV IDE application here: https://openmv.io/pages/download

image

This software has many resources to program with python and examples like snapshot, machine learning, image processing, etc. In my case I took a snapshot. which I show below.

image

Nicla vision module is working well. If you are looking for more details of what I just did, then here is a link: https://docs.arduino.cc/tutorials/nicla-vision/getting-started

Arduino MKR WAN 1310 Setup

The Arduino MKR WAN 1310 provides a practical and cost effective solution to add LoRa connectivity to projects requiring low power. This open source board can connect to the Arduino IoT Cloud, your own LoRa network using the Arduino LoRa PRO Gateway, existing LoRaWAN® infrastructure like The Things Network, or even other boards using the direct connectivity mode.

image

Here we need to navigate to Tools > Board > Board Manager.

This will open up a new window, with all available cores. Type in "samd"  in the search field, and install the Arduino SAMD Boards (32-bits ARM Cortex-M0+) core.

image

In my case update the library to version 1.8.13

 When it is finished, it should say "INSTALLED"  under the title.

Exit the board manager, and go to Tools > Board > Arduino SAMD Boards (32-bits ARM Cortex-M0+). Here you can see all the SAMD boards listed, where you can select the MKR board you are using. You have now successfully installed the core.

image

When you have selected the USB connection port of your board, you are now ready to start using your board! The easiest way to check that everything is working, is to upload just a simple blink example to your board. This is done by navigating to File > Examples > 01.Basics > Blink.

Conclusion

Both configurations of the Arduino Pro Nicla Visión and Arduino MKR WAN 1310 boards were successful. Now the next step is to implement Machine Learning with Edge Impulse.

 

  • Sign in to reply
  • robogary
    robogary over 3 years ago

    You make it look so easy ! How is the nicla connected to the arduino ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<