Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Sci Fi Your Pi: PiDesk - Project Update #4
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 6 May 2015 10:50 AM Date Created
  • Views 1824 views
  • Likes 3 likes
  • Comments 8 comments
  • design_challenge
  • touch_motion_controls
  • touch_motion_control
  • sci_fi_your_pi
Related
Recommended

Sci Fi Your Pi: PiDesk - Project Update #4

fvan
fvan
6 May 2015

Previous posts for this project:

  • Sci Fi Your Pi: PiDesk - Project Description
  • Sci Fi Your Pi: PiDesk - Project Update #1
  • Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2
  • Sci Fi Your Pi: PiDesk - Project Update #2
  • Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board
  • Sci Fi Your Pi: PiDesk - Project Update #3
  • Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot

 

  • Project Update

 

Project Update

 

Had some fun with stepper motors today! I've been setting up the Gertbot and building a first prototype for the screen lift mechanism.


The Gertbot is really easy to use, it was up and running in a matter of minutes. To know how, check out this post: Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot

 

The first prototype of the screen lift makes use of two stepper motors and threaded rods, as described in my application. The end result will be different in the sense that the mechanism should be completely hidden and only the screen should come out. The current prototype has threaded rods all the way to the top side of the screen, which should not be the case in the final mechanism. mcb1 suggested using a car window mechanism (thanks Mark!). I'll be running that track in parallel, figuring out where to get the parts first.

 

Another thing is that the current prototype is rather slow, requiring about 20 seconds to bring the screen up. An idea to increase the speed without having to change the electronics is to use threaded rods with a bigger pitch. The rods I'm using now have a 1mm pitch. I suppose that using rods with let's say a 1.5mm pitch, would reduce the lift time by a third. Does that sound right ?

 

In case you haven't checked out the other post, here's the lift prototype as it is now:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Until next update!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +2
    I suppose that using rods with let's say a 1.5mm pitch, would reduce the lift time by a third That may well be the case, but you need to go to M10 http://www.engineeringtoolbox.com/metric-threads-d_777…
  • mcb1
    mcb1 over 11 years ago in reply to fvan +1
    A leadscrew is perfect ... It tends to have a squared off top so that just the sides do the work. Yes the nuts would be an issue .... The M10 thread is easy to find at most hardware stores, and for what…
  • fvan
    fvan over 11 years ago in reply to balearicdynamics +1
    Thanks Enrico, on to the second (and improved) version!
Parents
  • mcb1
    mcb1 over 11 years ago

    I suppose that using rods with let's say a 1.5mm pitch, would reduce the lift time by a third

    That may well be the case, but you need to go to M10

    http://www.engineeringtoolbox.com/metric-threads-d_777.html

    image

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to mcb1

    I came across this while searching, with a 8mm diameter and 1.5mm pitch: http://www.benl.ebay.be/itm/Trapezoidal-Acme-Leadscrew-Spindle-8mm-x-1-5mm-Pitch-TR8x1-5DX500mm-CNC-3D-/161455405420?pt=LH_DefaultDomain_123&hash=item25977df96c

     

    Of course, the matching nuts are required, but would allow me to stay at 8mm, avoiding to have to replace the couplings etc ... Thoughts (besides the fact that it seems to be totally overpriced) ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to fvan

    A leadscrew is perfect ...

    It tends to have a squared off top so that just the sides do the work.

    Yes the nuts would be an issue ....

     

    The M10 thread is easy to find at most hardware stores, and for what you are doing a very quick sand/file while being rotated by a drill would allow some of the 'peak' to be removed.

     

    image

     

    You may well be able to find couplers, or drill out one.

    The other option is check what the 3D printer boys use ... some may have the exact parts.

     

    Failing that the local car wrecker is looking like a good weekend trip.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago in reply to fvan

    A leadscrew is perfect ...

    It tends to have a squared off top so that just the sides do the work.

    Yes the nuts would be an issue ....

     

    The M10 thread is easy to find at most hardware stores, and for what you are doing a very quick sand/file while being rotated by a drill would allow some of the 'peak' to be removed.

     

    image

     

    You may well be able to find couplers, or drill out one.

    The other option is check what the 3D printer boys use ... some may have the exact parts.

     

    Failing that the local car wrecker is looking like a good weekend trip.

     

    Mark