Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Measure Climate Change with Hydroponic System Blog #2 | XMC4200 Bring-up and Hydroponic System
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
  • Author Author: kurama007
  • Date Created: 4 Aug 2020 5:13 AM Date Created
  • Views 1862 views
  • Likes 4 likes
  • Comments 6 comments
  • xmc4200
  • sustain the world
Related
Recommended

Measure Climate Change with Hydroponic System Blog #2 | XMC4200 Bring-up and Hydroponic System

kurama007
kurama007
4 Aug 2020

Blog Posts ...

Blog #1: Measure Climate Change with Hydroponic System Blog #1 | Concept Design and Plans
Blog #2: Measure Climate Change with Hydroponic System Blog #2 | XMC4200 Bring-up and Hydroponic System

Blog #3: Measure Climate Change with Hydroponic System Blog #3 | XMC4700 + DC Motor Shield with Hydroponic System

Blog #4: Measure Climate Change with Hydroponic System Blog #4 | Sunlight Sensor and Water Purity

Blog #5: Measure Climate Change with Hydroponic System Blog #5 | Air Flow and CO2 Measurement

Blog #6: Measure Climate Change with Hydroponic System Blog #6 | Tomato Hydroponic Systems and Environmental Change Alert

Blog #7: Measure Climate Change with Hydroponic System Blog #7 | Hydroponic Nutrient and Water Measurements

 

Highlight

All components have arrived and I am very excited to try out the Infineon components because this is my first time to try them image

 

The plans for this week are summarized like this.

1. Get familiar with Infineon DAVE IDE image

2. Turn on/off/toggle LED image

3. UART communication between a XMC4200 microcontroller and computer image

4. Develop a small application involving UART and LED image

5. Hydroponic System image

 

Here is a video of my hydroponic system called YOSO (You Only Set-up Once) !

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Indoor Hydroponic System Videos are here at this website: https://green-scientist.com/indoor-gardening/

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Here are pictures that show the actual setup and software development progress.

image

Software Environment: From UART (TeraTerm), a user can type 0, 1, or 2 to turn off LED, turn on LED, or toggle LED (on--> off or off --> on).

image

 

 

Details

1. Get familiar with Infineon DAVE IDE

 

This is my first time to use Infineon microcontrollers. So, I didn't know where to start. Fortunately, the XMC4200 product website has nice documentation. So, I was able to follow the instructions. The software development kit was a bit confusing at the beginning as it says the Arduino compatible. However, XMC4200 is still a new product and Arduino IDE and Platform IO are not supported yet as of August 3, 2020. The only pins are compatible with Arduino Uno. So, I tried using Infineon DAVE IDE based on Eclipse. The experience so far is very good. There are two USB ports on XMC4200, and I only use the one on "Debug" side, so I can use the DAVE debugger flawlessly.

 

The notes are summarized here (still work in progress image) https://green-scientist.com/2020/07/26/infineon-mcu-xmc4200-guide/

2. Turn on/off/toggle LED

 

Usually, the first software application is either a Hello World or blink a LED with an embedded system. I tried a LED application for the first time. The LED configuration requires a DAVE UART application. The XMC 4200 Platform2Go comes with an on-board LED as part of Digital IO, which is assigned as P0.1 as a pin name.

 

Here are Digital IO commands that I used.

  • DIGITAL_IO_SetOutputLow(&LED0);
  • DIGITAL_IO_SetOutputHigh(&LED0);
  • DIGITAL_IO_ToggleOutput(&LED0);

This is a DAVE app block diagram.

image

 

3. UART communication between a XMC4200 microcontroller and computer

 

    To control the microcontroller and sensors later, I would like to have a debug UART console. Inside DAVE, we can enable UART and I have a USB-to-UART cable which can be connected to P2.14 an P2.15 pins. So, I connected the USB-to-UART cable with three wires like the picture below. This cable came with a FTDI FT232RL chip.

image

 

 

4. Develop a small application involving UART and LED

 

The small application starts with initializing the UART communication between a PC and XMC4200 microcontroller. Then, depending on the user input (ex: 0, 1, or 2) , XMC4200 takes action on the LED.

Code Snippet

image

 

5. Hydroponic System

Here is the simple hydroponic system that I built. The building instruction is summarized in my website here. https://green-scientist.com/2020/05/16/diy-hydroponics-under-10-mins-with-basil/

image

Next Steps

 

I would like to get familiar with the Infineon motor controller and high current PROFET shield to control the air pump by the XMC4200 and UART console. More fun to come image

  • Sign in to reply

Top Comments

  • m.ratcliffe
    m.ratcliffe over 6 years ago in reply to DAB +2
    It gets a bit tricky when measuring the resistance of nutrient water solutions as they polarise relatively quickly, making it challenging to get a true resistance. The grove TDS sensor board gets around…
  • stefan.mitocaru
    stefan.mitocaru over 6 years ago +1
    Impressive project! I am excited to see more
  • DAB
    DAB over 6 years ago in reply to kurama007 +1
    You could try a simple resistance measurement with an opamp and A/D. Clear water would be high resistance. As the plants use nutrients, they create salts, which lower the resistance. If you do a little…
Parents
  • DAB
    DAB over 6 years ago

    Good start.

     

    Are you monitoring the fluid content to measure how much nutrients the plants use?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kurama007
    kurama007 over 6 years ago in reply to DAB

    That's a good question. At least, I bought a Grove TDS Sensor to check the quality of water. I am still learning how to measure nutrients that the plants use over time. Please let me know if you have ideas about measuring the fluid content.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago in reply to kurama007

    You could try a simple resistance measurement with an opamp and A/D.

    Clear water would be high resistance.

    As the plants use nutrients, they create salts, which lower the resistance.

    If you do a little web search, you can find out the Ph levels that correspond to the percentage of salt in the water.

    It might take you some trial and error to establish what is a healthy level for the plants you are growing. It will change depending upon the plant.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 6 years ago in reply to DAB

    It gets a bit tricky when measuring the resistance of nutrient water solutions as they polarise relatively quickly, making it challenging to get a true resistance. The grove TDS sensor board gets around this by measuring resistance using an AC input between the probe faces. A DC measurement works if you take it quickly and have a low/long duty cycle:

    Automated Green House Blog:10 - Three Dollar EC PPM Meter for MCU 

     

    There was a vertical farming competition a good few years ago here on E14, its old but might make good reading for the OP.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kurama007
    kurama007 over 6 years ago in reply to m.ratcliffe

    Thank you DAB and Michael for the recommendations. This is very interesting. I will give it a try and hopefully report it out in a couple of weeks image --Satoshi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kurama007
    kurama007 over 6 years ago in reply to m.ratcliffe

    Thank you DAB and Michael for the recommendations. This is very interesting. I will give it a try and hopefully report it out in a couple of weeks image --Satoshi