Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound - Cell Phone Shield Test - blog 19
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
  • Author Author: dougw
  • Date Created: 12 Jun 2017 12:32 AM Date Created
  • Views 1456 views
  • Likes 10 likes
  • Comments 5 comments
  • safe and sound
  • doug wong
  • safe and sound design challenge
  • hazardous_environmental_factors
  • invisible_hazards
  • safe & sound
  • wearable technology
  • Wearables
  • cell phone shielding
  • safe&sound
Related
Recommended

Safe and Sound - Cell Phone Shield Test - blog 19

dougw
dougw
12 Jun 2017

The deadline for this challenge has been extended again, so I can squeeze in a few more blogs. Perhaps some real applications of all this instrumentation I have put together.

This blog shows some quick tests I did to see if shielding makes a difference to cell phone radiation. These tests are a follow up to an earlier blog on microwave radiation.

To set up for the test, I made a shield from two 3D printed shells sandwiching a layer of aluminum foil between them.

The shell and foil covered 5 of the 6 sides of the phone - about 1mm from the back of the phone and about 2mm from the sides.

image

I ran some tests with and without the shield to see if it made a difference - and it definitely did. I was a bit surprised by the results.

The main scenario that I am interested in is the case where the phone is in a pants pocket as studies show this results in lower testosterone and lower sperm count. So I placed the phone and meter in appropriate locations on a Hybrid III crash test dummy and took some readings. These particular dummies have seen some major trauma (explosions) and you can see they look a bit charred, but the geometry is still good - this is a 50th percentile male.

imageimage

These readings are the maximums I saw in this geometry. The shielded maximum was a rare spike, it spent most of its communication time at about 1 mW/m2.

The unshielded maximum is closer to its normal value ~ 150 mW/m2.

In this experiment the shielded case yielded 10 to 100 times less radiation density at the location of interest.

This is not a particularly scientific experiment, but the results do suggest it might be worth investigating shielding in a more scientific way.

I did not check to see how cell phone performance was impacted by the shield - I imagine the shield didn't help communications ...

To get a bit more of a feel for what the readings look like in real time, I made a video of typical readings. Viewers can decide if the readings are meaningful for themselves.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The other geometry of interest is holding the phone at your ear.

Here are some images showing a reading with the meter where an ear might be and what happens if a metal plate is inserted between the phone and the meter.

imageimage

Note the units change in these images - one is mW the other is uW, so the last image is 4.6 mW/m2

One observation is that the field strength seems to be lower at the face of the phone compared to the sides - by about 50%.

The other observation is that the metal plate cuts the field strength by more than a factor of 100. Again, I did not determine how this plate impacts cell phone communications performance.

 

These experiments are not trying to determine what level of radiation is safe, just trying to get a feel for whether partial shielding can reduce radiation exposure.

 

All links to blogs related to this project can be found in the first blog here:

Safe and Sound - Invisible Hazardous Environmental Factors Monitoring System - blog 1

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +4
    Another great blog and good demo. I do question if you don't have conflicting interests with protection vs functionality of the phone though. Perhaps you might do better to shield the sensitive area as…
  • dougw
    dougw over 9 years ago in reply to jw0752 +4
    Yes, the phone transmitter might even see extra stress by putting shielding nearby, in addition to the possibility of having communication difficulties. These experiments aren't recommendations, they are…
  • dwinhold
    dwinhold over 9 years ago +3
    Great blog!! Yet again your project shows you have outdone yourself (and the rest of us.. In my opinion) A couple of notes: 1) Cell phones in your pants isn't a good birth control. 2) Did you get the dummies…
Parents
  • dwinhold
    dwinhold over 9 years ago

    Great blog!! Yet again your project shows you have outdone yourself (and the rest of us.. In my opinion)

     

    A couple of notes:

    1) Cell phones in your pants isn't a good birth control.

    2) Did you get the dummies to sign a waiver before they agreed to the test?

     

    Dale W

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to dwinhold

    The dummies were happy to participate - it was a pleasant change from getting blown up.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 9 years ago in reply to dwinhold

    The dummies were happy to participate - it was a pleasant change from getting blown up.

    • Cancel
    • Vote Up +3 Vote Down