Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound - The Companion IoT Jacket #13: The Wearable Demonstration
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
  • Author Author: ipv1
  • Date Created: 9 Jul 2017 9:03 AM Date Created
  • Views 1123 views
  • Likes 3 likes
  • Comments 3 comments
  • ip_iot
  • safe & sound
  • safety_jacket
Related
Recommended

Safe & Sound - The Companion IoT Jacket #13: The Wearable Demonstration

ipv1
ipv1
9 Jul 2017

  • The Complete Design Review
  • One More TI Part
  • The Wearable Electronics
  • The Final Product
    • The Video Demonstration
  • The GitHub Repo and PinShapes
  • Conclusion

 

Here is the progress so far

Safe & Sound - Safety Jacket for the Tolling Industry #1: Introduction to ProjectSafe & Sound - Safety Jacket for the Tolling Industry #2: Filling up the space with CC110L Tutorial
Safe & Sound - Safety Jacket for the Tolling Industry #3: TI RTOS and POSIX with the CC1310 LaunchpadSafe & Sound - Safety Jacket for the Tolling Industry #4: Unboxing and a relaunchpad
Safe & Sound - Safety Jacket for the Tolling Industry #5: Writing your own protocolSafe & Sound - Safety Jacket for the Tolling Industry #6: Writing your own protocol - part 2
Safe & Sound - Safety Jacket for the Tolling Industry #7: Cloud CCS and Sample Code IssuesSafe & Sound - Safety Jacket for the Tolling Industry #8: Energy Harvesting
Safe & Sound - Safety Jacket for the Tolling Industry #9: Keeping the Launchpads SafeSafe & Sound - The Companion IoT Jacket #10: MSP432, BLE and 3D Printing module one
Safe & Sound - The Companion IoT Jacket #11: An Energy Harvesting DisplaySafe & Sound - The Companion IoT Jacket #12: Qi Charging with Element14, Texas Instruments and Wurth Electronics

 

In this post, I present the final wearable and submission. It is important to package the contents into an ergonomic wearable and make it serviceable. The final challenge is to create something presentable and usable.

 

The Complete Design Review

image

The four modules were segregated for design reuse and I designed and printed all enclosure using Fusion 360 and a Cel Robox. The idea is to create a wearable meant for safety and one that uses all Texas Instruments parts. The MSP432 is the hero of our design and runs TI-RTOS and a number of tasks for all the functions. BLE communication is handled by the TI CC2650 which reduces the BOM and power consumption. The BQ25570EVM is used in conjunction with a solar panel and a SuperCap to power an MSP430 and Sharp96 Booster Pack from TI. Information is relayed via serial communications to provide a visual indication of status and data display. The Qi Charging Power Pack is designed around the E14 and TI Fuel Tank Booster Pack and WE and TI Wireless Charging Kit to provide power to the main components.

 

All the above components are mounted in a jacket as explained in the proceeding sections.

 

One More TI Part

Since we are using BLE and it's a wearable, I decided to put in one more part. I had a CC2640 LED module from a previous challenge and design an enclosure around it. It is powered from another Fuel Tank adhering to my policy of using all TI parts.

image

This module adds another layer of visual indications that can work directly with the BLE app.

 

The Wearable Electronics

Creating an ergonomic wearable was a challenge that was taken up by my better half. Using ribbons, thread, and other accessories, she assembled all the parts into the final wearable.

 

{gallery} My Gallery Title

image

Appearance: Adding ribbons to the enclosure to make it blend in with the jacket

image

Exposing Headers: Exposing the headers to be able to connect with the power pack

image

Sensors Badge: Adding the sensors booster Pack so as to use the IR Temp sensor.

image

Concealed Cabled: Hiding the cables is a task on its own.

image

Cable Cleanup: All the cables run the underside in a concealedmanner.

image

A:A

image

image

Display : The display is embedded on the front.

image

Exposed Headers: The headers are first exposed and then stitched in place to provide a clean place to dock the Power Pack

 

The Final Product

My better half has done an excellent job in creating the final product.

image

image

The solar panel sits comfortably at the back exposed to light sources and the Sensors Booster Badge is mounted on the front along with the LCD. The LED light is converted into the badge with it's power source in the adjacent pocket. All the wiring is hidden inside going towards the Core module which is in the left pocket. The exposed headers under the jacket allow for mouting of the power pack with ease.

The Video Demonstration

A picture is worth a thousand words and in this case, I needed lots to explain the functioning.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The GitHub Repo and PinShapes

I promised a code upload and to download the code please visit https://github.com/inderpreet/Project-SafetyJacket

The 3D models can be downloaded from https://pinshape.com/users/29645-inderpreet-singh-ip

 

Conclusion

I managed to stick to my original plan and created a working Wearable with all TI parts. I am happy with the result and though I am not an Android Programmer, I have started the process of working with Java. The project works and can be expanded depending upon requirement. The intent was to be able to have two way communication and the proof of concept is presented thought the software part is still a bit rough. Hopefully this is an incentive for me to work on other skills.

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +2
    Really well done. Complete and with the attached material in the right place Enrico
  • DAB
    DAB over 9 years ago +1
    Great job of integrating the system into an easy to wear garment. DAB
Parents
  • DAB
    DAB over 9 years ago

    Great job of integrating the system into an easy to wear garment.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Great job of integrating the system into an easy to wear garment.

     

    DAB