Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound @ E14-CLEWE @ #1_Introduction: "A word."
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
  • Author Author: jkutzsch
  • Date Created: 20 Feb 2017 12:33 AM Date Created
  • Views 1230 views
  • Likes 3 likes
  • Comments 5 comments
  • safe and sound design challenge
Related
Recommended

Safe & Sound @ E14-CLEWE @ #1_Introduction: "A word."

jkutzsch
jkutzsch
20 Feb 2017

E14-C.L.E.W.E. INDEX:

#1_”The word.”

#6_Energia!

#2_”The Science.”

#7_Blog7

#3_"GPS decisions."

#8_GPS_Issues

#4_"GPS arrives!"

#5_"The box, the box!"

                                                                             image

In the beginning (at least of this project), there was, a word.

 

That word provides to our Modern day readers of Element 14 a clue.  To truly understand what this word is and how it pertains to this Safe & Sound Design Challenge project, we need to better understand the history and meaning of clue.

 

Referencing Merriam-Webster.com we find the current accepted definition of CLUE:

 

 

"1 :  something that guides through an intricate procedure or maze of difficulties; specifically :  a piece of evidence that leads one toward the solution of a problem

2 :  idea, notion<had no clue what he meant>"

 

 

They are even so kind as to provide some additional tidbits of information:

 

”Did You Know?

The word clue was originally a variant spelling of clew, meaning “ball of thread or yarn.” Our modern sense of clue, “guide to the solution of a mystery,” grows out of a motif in myth and folklore, the ball of thread that helps in finding one’s way out of a maze. Of these stories the best known is the myth of Theseus and the Minotaur. In the myth, Theseus unravels a ball of thread as he searches for the monstrous Minotaur in the Labyrinth. After killing the Minotaur, he retraces his steps out of the maze by rewinding the thread.

Origin and Etymology of clue

alteration of clew

First Known Use: circa 1665”

 

 

So now we see that our clue has the interesting heritage of coming from clew and can be traced back to the myth of Theseus and the Minotaur.  Not mentioned above is the fact that the clew that was given to Theseus was provided by Princess Ariadne, and has even more intriguing details.  Some of our readers may have heard of The Ariadne’s Clew algorithm, while well beyond the scope of this project it is interesting!

Out of curiosity, what more can be learned from Merriam-Webster.com about clew?

 

“Origin and Etymology of clew

Middle English clewe, from Old English cliewen; akin to Old High German kliuwa ball, Sanskrit glauḥ lump”

 

 

So today’s clue comes from the Middle English clewe.  The idea behind clewe is that when Theseus had to navigate the Minotaur’s maze, Princess Ariadne, who was quite taken by Theseus, offered to assist him if he would take her away and marry her.  She gave him a red ball of thread that he was able to use to mark his path through the maze and safely return.

This ball of thread provided an alternate solution to the maze aside from actually knowing the paths. 

Interestingly enough wikipedia has an entry on Ariadne’s Thread (logic):

 

 

“Ariadne's thread, named for the legend of Ariadne, is the solving of a problem with multiple apparent means of proceeding - such as a physical maze, a logic puzzle, or an ethical dilemma - through an exhaustive application of logic to all available routes.”

 

 

Following this thread of definitions/thoughts, I present the idea for the E14-C.L.E.W.E:  A wrist mounted explorer utility that provides GPS logging as well as other navigation functions and utilities.  A digital ball of thread that can be used to find your way!   

Element 14 – Custom Logging Explorer Wrist Equipped

      image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago in reply to jkutzsch +2
    Yes, the mention system does not like my simple user name. It has been an issue for a number of years now, but I do not plan to change because I am not big on point accumulation, plus it keeps the issue…
  • DAB
    DAB over 9 years ago +1
    Well I have seen worse acronyms. The project does have some interesting aspects, so I am interested in seeing it develop. DAB
  • jkutzsch
    jkutzsch over 9 years ago in reply to DAB

    Good to know it is not a new issue then.  Wasn't sure if it was tied to the email weirdness.  :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to jkutzsch

    Yes, the mention system does not like my simple user name.

    It has been an issue for a number of years now, but I do not plan to change because I am not big on point accumulation, plus it keeps the issue on the todo list.

    I mean really, how hard is it to fix?

    Isn't software easy?

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch

    For some reason it won't find you when I try to Mention you.

    Correct.

    DAB needs to change his username because it gets all confused.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to DAB

    @DAB I think you will enjoy my next blog where it references the acronyms from the Air Force and Army.  For some reason it won't find you when I try to Mention you. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Well I have seen worse acronyms.

     

    The project does have some interesting aspects, so I am interested in seeing it develop.

     

    DAB