Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog PDU #8 - Different Direction [Upcycle It]
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
  • Author Author: jasonwier92
  • Date Created: 15 May 2017 12:03 PM Date Created
  • Views 1663 views
  • Likes 6 likes
  • Comments 7 comments
  • upcycled_pdu
Related
Recommended

PDU #8 - Different Direction [Upcycle It]

jasonwier92
jasonwier92
15 May 2017

Change Never Changes

 

I have lots of ideas, but I need to get this project moving along, so I have started down the final path, but started more fresh than before.  I have decided to use the other Edison and the mini-board since I am putting all of this in a 1U enclosure.  Here are my hardware plans going down the stretch.

 

Outlet Switching

 

I am going to use an eight port version of the relay module posted right below. I have the module, but it is wired up currently for testing as I have just finished testing my circuit I am going to build to control this set of relays.

 

image

 

Now with these Opto-isolated relay modules, the pins need to be floating or tied to 5V to be off and connected to ground to be in a on state.  For this I have wired up a simple inverter circuit that helps me with another problem with the mini and that is 1.8V.

 

image

 

This is one of eight I will use to control the 8 relays on the board for the 8 outlets.  The LEDs will go the front of the unit it display power status to each outlet. I plan on making this control board to plug into the relay circuit to keep the wire count to a minimal.

 

Edison Mini-board

 

I have added a header to the bottom of the Mini-board and that will plug into another board for power and GPIO. That other board will be mounted inside the PDU, so that the Edison is easily removed if need be.

image

 

Only other thing I need to control is the LCD that will be mounted in the PDU. I will use the Adafruit 4-Bit Level Converter for to bring the I2C 1.8V to 5V fro the LCD.

 

image

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +3
    The header on the bottom of the mini-board is a brilliant idea!
  • gpolder
    gpolder over 9 years ago +3
    I'm using a Sparkfun level converter, Looks like its circuit is the same as the Adafruit, featuring the BSS138 FETs. Only the color of the board is different. In my case the Sparkfun works like a charm…
  • jasonwier92
    jasonwier92 over 9 years ago in reply to Workshopshed +2
    Thank you! I have seen partial headers and I have seen male headers, but I wanted female so the pins do not get bent on the part I do not want to solder often.
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    The header on the bottom of the mini-board is a brilliant idea!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jasonwier92
    jasonwier92 over 9 years ago in reply to Workshopshed

    Thank you!  I have seen partial headers and I have seen male headers, but I wanted female so the pins do not get bent on the part I do not want to solder often.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jasonwier92
    jasonwier92 over 9 years ago in reply to Workshopshed

    Thank you!  I have seen partial headers and I have seen male headers, but I wanted female so the pins do not get bent on the part I do not want to solder often.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • carmelito
    carmelito over 9 years ago in reply to jasonwier92

    Nice Idea, look like I am going to have to solder some female header to the mini-board,I think I have a level converters. Thanks for posting a picture..