Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Hotrodding the Edison
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
  • Author Author: Workshopshed
  • Date Created: 11 May 2017 8:24 AM Date Created
  • Views 3599 views
  • Likes 8 likes
  • Comments 21 comments
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Hotrodding the Edison

Workshopshed
Workshopshed
11 May 2017

The observant amongst you will have spotted that there was an item in the  [Upcycle It] Interactive Race Car Driver - 3D Printed Parts article that did not relate to any of the things I was printing. That was because I did not know if it was going to print ok or not. The part is some "exhaust pipes" to add to the Edison to turn my "engine" into a hotrod.

imageimage

Because I was concerned about the exhausts wobbling about when printing I added some 1mm horizontal supports to the model which were then cut off using a knife following the print. The print went well until layer 165 of 168 at which point it came detached from the print bed. As I was printing at 100% fill this did not actually matter and I've gone with fractionally shorter pipes by 0.9mm. If I was going to print it again I'd likely use a brim around the base to give it a bit more grip.

image

You can find all the models at https://github.com/Workshopshed/UpcyclingDesignChallenge/tree/master/3DModels

 

I don't think my modification will make any difference to the Edison's performance but I do think it looks cool. Hopefully, I'll have time to give it a coat of silver paint so it looks more like exhaust pipes.

 

Previous Posts

Upcycle It Blogs tagged with upcycled_interactiveracecardriver

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 9 years ago in reply to mcb1 +4
  • dougw
    dougw over 9 years ago +3
    Superb - those pipes are absolutely iconic. Of course if you printed a "blower" for the air intake it would be spectacular if you could squeeze in a real fan. Not trying to mess up your already impressive…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to mcb1 +2
    Mark, it seems there is not sufficient space to fit the Edison Enrico
Parents
  • DAB
    DAB over 9 years ago

    Nice update Andy.

     

    I am surprised that you did not do a heat sink mod for this part so that it was functional as well as cool!

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to DAB

    With a bit of fine tuning you could give the model better thermal bonding to the Edison then you could sent it off to one of those 3D printing firms they can print it in metal.

     

    Has anyone run the Edison for a long period, I've not actually noticed it getting hot?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Has anyone run the Edison for a long period

    Not really. I did notice it got relatively warm with no real loading, and I haven't been game to make it work hard just to see it melt.

     

    then you could sent it off to one of those 3D printing firms they can print it in metal

    You could, but the design you have infringes on the area Intel say to keep clear because of the wireless/BT aerial.

     

    I'm sure you could print off a metallic blower to attach to the metal part of the Edison though ... image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Has anyone run the Edison for a long period

    Not really. I did notice it got relatively warm with no real loading, and I haven't been game to make it work hard just to see it melt.

     

    then you could sent it off to one of those 3D printing firms they can print it in metal

    You could, but the design you have infringes on the area Intel say to keep clear because of the wireless/BT aerial.

     

    I'm sure you could print off a metallic blower to attach to the metal part of the Edison though ... image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1

    >You could, but the design you have infringes on the area Intel say to keep clear because of the wireless/BT aerial.

    Good point image