Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - No more printing
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
  • Author Author: Workshopshed
  • Date Created: 28 May 2017 2:54 PM Date Created
  • Views 2470 views
  • Likes 8 likes
  • Comments 18 comments
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - No more printing

Workshopshed
Workshopshed
28 May 2017

So this was supposed to be a joyful post about how I'd printed the redesigned backlight bracket and a base for the Furby to hold the Edison and other parts.

imageimage

However, before printing, I got a warning message on the printer and the printer refused to print. When I took the head off I realised why as there was a load of blue PET behind the print head.

imageimage

Despite various attempts to remove the plastic from using the purge cycle to heat the head and tweezers to using a soldering iron to carve through the plastic, I could not remove it. I fact I think I've made the problem worse and narrowly avoided setting the smoke alarm off.

 

I don't think there will be any more prints this week and I'll likely need to save up for a new head.

 

Updated - Wood and glue save the day

Dolls house offcuts

When I assembled a dolls house kit the other year, I kept all of the 3mm ply that formed the frame where the parts were pushed out. None of the parts were particularly large but I thought they might come in handy for models and the like.

 

So I cut some squares and some blocks and glued up some piles to support the Edison, it's not elegant and is taller than I wanted but will do the job till I can print a replacement for the platform I was going to make.

imageimage

Reference

RBX01-S2 - Single Material Dual Nozzle Head- Version 2 - Replacement and spare parts - Robox

Woodcraft Dolls House Kit

 

Previous Posts

Upcycle It Blogs tagged with upcycled_interactiveracecardriver

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +3
    I once had some kind of blown seal in my Robox head and filament was coming out in places it shouldn't. It was not obvious what was happening because by the time I realized something was wrong, there was…
  • jasonwier92
    jasonwier92 over 9 years ago +3
    Way to work plan B and get it done. I like saving scraps from a project. Never know when you have to do plan B, but the perfect material was in the landfill.
  • mcb1
    mcb1 over 9 years ago +3
    I only got one word to say. https://www.youtube.com/watch?v=cbBx4Ql6Umo
  • Workshopshed
    Workshopshed over 9 years ago in reply to DAB

    Not a good afternoon but a work around is in place (see above) and I can get back to the electronics and code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago

    As hideous as those nozzles look those are not the problem. They did print ok at one point this afternoon. The issues is that there is a LOT of plastic behind the heads where the mechanism is to switch the nozzles. This stops the mechanism moving and hence selecting a nozzle, hence the message.

     

    Here's some stock photos of a variations of this head, it's that space between the stepper and the nozzles that is full of plastic.

    imageimage

     

    I don't believe a seal was blown as it was printing ABS quite happily for a couple of hours after it was printing the PET. There was also no black ABS in the plastic I was removing. The problem must have started when it cooled down after that session and the PET set hard. The print head is 2.5 years old so I'd suspect beyond any warrantee.

     

    The smoke and flickering light before the temperature sensor stopped working were a really bad sign. I'm not saying that it's a complete right-off but it's not going to be running this week. Perhaps parts for my next upcycling project?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Yes, there is nothing sadder than being ready to do some making and have your primary tool fail.

     

    It kind of kills the mood.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to rachaelp

    Workshopshed I had to use "a lot" of heat the one time I successfully cleared a stubborn blockage. We are talking 900 degree hot air gun. I'm not recommending it - it was a desperate and scary procedure, but it did work.image

    For hot tip applications other than soldering, I use old tips that are no longer good for soldering.

    If you turn the temperature down, you can use them for sculpting hot glue and possibly 3D printer parts. (I've had mixed success)

    With some materials you will want good ventilation....image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago

    Despite various attempts to remove the plastic from using the purge cycle to heat the head and tweezers to using a soldering iron to carve through the plastic, I could not remove it.

    I hope you haven't wrecked the tip of your soldering iron doing that.... burned plastic usually leaves a horrid black surface which is very difficult to clean up and makes solder not stay on the tip.... I had a contractor who I employed once do something like that to a Pace soldering iron we had and I had to buy new tips as I just couldn't get the surface cleaned well enough to solder properly....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>