Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - No more printing
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
  • Author Author: Workshopshed
  • Date Created: 28 May 2017 2:54 PM Date Created
  • Views 2384 views
  • Likes 8 likes
  • Comments 18 comments
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - No more printing

Workshopshed
Workshopshed
28 May 2017

So this was supposed to be a joyful post about how I'd printed the redesigned backlight bracket and a base for the Furby to hold the Edison and other parts.

imageimage

However, before printing, I got a warning message on the printer and the printer refused to print. When I took the head off I realised why as there was a load of blue PET behind the print head.

imageimage

Despite various attempts to remove the plastic from using the purge cycle to heat the head and tweezers to using a soldering iron to carve through the plastic, I could not remove it. I fact I think I've made the problem worse and narrowly avoided setting the smoke alarm off.

 

I don't think there will be any more prints this week and I'll likely need to save up for a new head.

 

Updated - Wood and glue save the day

Dolls house offcuts

When I assembled a dolls house kit the other year, I kept all of the 3mm ply that formed the frame where the parts were pushed out. None of the parts were particularly large but I thought they might come in handy for models and the like.

 

So I cut some squares and some blocks and glued up some piles to support the Edison, it's not elegant and is taller than I wanted but will do the job till I can print a replacement for the platform I was going to make.

imageimage

Reference

RBX01-S2 - Single Material Dual Nozzle Head- Version 2 - Replacement and spare parts - Robox

Woodcraft Dolls House Kit

 

Previous Posts

Upcycle It Blogs tagged with upcycled_interactiveracecardriver

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +3
    I once had some kind of blown seal in my Robox head and filament was coming out in places it shouldn't. It was not obvious what was happening because by the time I realized something was wrong, there was…
  • jasonwier92
    jasonwier92 over 9 years ago +3
    Way to work plan B and get it done. I like saving scraps from a project. Never know when you have to do plan B, but the perfect material was in the landfill.
  • mcb1
    mcb1 over 9 years ago +3
    I only got one word to say. https://www.youtube.com/watch?v=cbBx4Ql6Umo
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to dougw

    Keep me informed image I am curious

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago

    I once had some kind of blown seal in my Robox head and filament was coming out in places it shouldn't. It was not obvious what was happening because by the time I realized something was wrong, there was too much plastic to see where the problem was. The manufacturer replaced the whole head for free and it has been fine since. Thanks CEL.image

    ..... So check with CEL ....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago

    As far as I know, these are just the nozzles to be replaced. No need an entire printing head...

    If you can unlock at least one, just check the thickness and you can ket sets of 5 new one for very few dollars from Amazon (I always have some in my boxes). A key M3 if I am not wrong should be used to unlock. When the nozzle are locked due the fused filament (out of place) I suggest to use the hot air of the soldering unit set at the proper temperature (about 120 C for PLA and 210 C for ABS). As you see that the plastic start fusing, stay ready with the key or a clamp to unlock the nozzles. then at least you have a better vision of what's inside. It is rare that the head is totally broken.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<