Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] WiFi Connected Smoke Detector #2: Hello, Edison!
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
  • Author Author: vlasov01
  • Date Created: 1 Apr 2017 7:14 PM Date Created
  • Views 1729 views
  • Likes 2 likes
  • Comments 5 comments
  • mqtt
  • intel edison
Related
Recommended

[Upcycle It] WiFi Connected Smoke Detector #2: Hello, Edison!

vlasov01
vlasov01
1 Apr 2017

<< Previous

Project Index

Next >>

 

Initial setup of Edison boards

The setup process completed successfully. I was able to setup and flash both boards. But the initial setup consumed much more time then I've anticipated.

Here are some thoughts about initial configuration of Edison:

  1. The reset button is located on the board and must be used as part of the flashing process. It was not very clear for me from the documentation. A simple picture may help a lot.
  2. I think the setup process may be simplified if only one USB cable and one USB port have been used during setup/flashing.
  3. It seems it is not possible to connect two Edison boards over USB Serial connection at the same time on my PC, as only one connection works at a time. But it is not an issue once WiFi connection is on.
  4. It will be great if the documentation had a troubleshooting section. Specifically, I spent most of the time googling around to resolve a serial connection:

image

 

 

MQTT on Edison

I've flashed my Edison boards with Yocto 1.7.3 Linux. In this release Yocto comes with Really Small Message Broker (RSMB). Mosquitto broker version 1.3.4. The process is live from the start.

root@node1:~# netstat -tunl | grep 1883
tcp        0      0 0.0.0.0:1883            0.0.0.0:*               LISTEN
tcp6       0      0 :::1883                 :::*                    LISTEN

 

It seems there is no MQTT client with Yocto, so I've used Paho MQTT client on my PC to test MQTT broker.

I was able connect to both MQTT nodes and publish test messages from Paho.

image

Next Steps

  1. Decide to keep RSMB (it is free, but not OSS, not a lot of documentation) or switch to Mosquitto broker.
  2. Build MQTT client (and may be broker) for Yocto for my project.
  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago in reply to jasonwier92 +1
    If Mosquitto is there by default it makes sense to use that. I've been using Mosca for my testing, that runs on top of Node so should run on any platform that supports Node if you can't find an alternative…
  • vlasov01
    vlasov01 over 9 years ago in reply to DAB +1
    Thank you for the feedback. I may be able to help a bit if you run into issues with Linux. Sergey
Parents
  • DAB
    DAB over 9 years ago

    Nice post.

     

    I will be following your progress, though my Linux skills are very limited.

     

    So I am looking to see what tips I can pick up.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Nice post.

     

    I will be following your progress, though my Linux skills are very limited.

     

    So I am looking to see what tips I can pick up.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vlasov01
    vlasov01 over 9 years ago in reply to DAB

    Thank you for the feedback. I may be able to help a bit if you run into issues with Linux.

     

    Sergey