element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Episode 607 Reboot request
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 140 subscribers
  • Views 8874 views
  • Users 0 members are here
Related

Episode 607 Reboot request

Mikeatencio
Mikeatencio over 1 year ago

/challenges-projects/element14-presents/project-videos/w/documents/28198/from-strava-to-motion-creating-an-arduino-powered-arcade-game-with-running-data----episode-607

I included the episode for context. Can someone please recreate this project for horse racing like the carnival arcades instead of the STAVA Lorraine created? I would truly enjoy making this now that I am retired. Thanks

Mike 

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +3
    I recall colporteur created a project 14 entry based on PWM locomotive motor control about 3 years ago as part of the world in motion competition and won a prize. I think it will have some similarities…
  • beacon_dave
    beacon_dave over 1 year ago +2
    You may need to start by sharing some pictures of the version of the game that you are after creating, as they vary quite a bit. Over here in my youth it was known as the 'Donkey Derby' but that I believe…
  • beacon_dave
    beacon_dave over 1 year ago +2
    If you still want to use a pinball mechanism, then perhaps look at the Ben Heck Show episode archive, as he built a number of pinball machines from scratch.
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +2
    Well that was a quick and easy decision... You can get GPIO expanders if you run out or you can just add another microcontroller, like has been done here where 200 buttons are being used: https://www…
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave +1
    I recall that some were based on linear tracks like Lorrainbow's Strava version whereas some were based on oval tracks. Size varied a lot as well from the large arcade versions like this Blackpool Pier…
  • michaelkellett
    michaelkellett over 1 year ago in reply to Mikeatencio +1
    I would have had a look but you can't see much at all without signing in an creating an account - but they want you to pay before you can access the 14 day free account. I won't pay money to a supplier…
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave +1
    I recall SparkFun did a corn hole board game with a LED light strip in the hole the corn bag drops through Sketch Up SparkFun Corn Hole Lorrainbow also did a BasketBall hoop using a colour sensor …
  • michaelkellett
    michaelkellett over 1 year ago in reply to Mikeatencio +1
    No need to apologise - it's not you being a muppet ! MK
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +1
    Mikeatencio said: 6 foot long. For 12 players then a 6' long track might be a bit on the short side. If you have 6 players either side then that only leaves 1' per player. Might be worth considering…
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +1
    I think you are going to be around 2' shoulder width, then you need extra for the elbow movement when picking and rolling the balls. One way to maximize space may be to make it dodecagonal as that way…
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    In the final design, you may want to make the play surface a replaceable element so as you can easily swap it out for a different design.

    I suspect that over time you may want to refine it a bit as you get more confident with the different aspects of the build.  

    You could have swappable themed designs for different seasons or events. Or you could perhaps swap a roll a ball for a pinball design.

    Perhaps keep an eye out for some of the DIY pinball machine forums as they are likely to have some tips on how to make interactive features that work reliably.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    I like that idea. Thank you Blush 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    Some educational constructor kits might be worth a look for ideas/prototyping.

    Build your own game: Quick building success and great fun for the whole family!

    The rotating deflectors looked interesting as they perhaps could be attached to rotary sensors to generate points and flash lights. The rubber band shooting balls through a narrow opening looks like another simple but effective option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    The sensor arrangement on the Elton Derby game can be seen here:

       https://rollaball.co.uk/product/score-tray-optical-sensor-v4/

    in the spares section.

    Looks like 3 pairs of optical break beam sensors with the chutes directing balls from certain pockets through the different sensors.

    According to a comment here:

       https://forum.arduino.cc/t/roll-a-ball-horse-race-game/417850

    apparently in 2017, the game cost £18,000.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    I love the mouse on the bus game. The camel racing was great too. 18,000 must include everything.  I like the scoring system.  It would be easy to replicate. Thank you for the links. I'm guessing, but I imagine there's a chain driven system using NEMA 23 step motors. These are similar to this episode project.  It's exactly what I wanted,  just bigger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio
    Mikeatencio said:
    I'm guessing, but I imagine there's a chain driven system using NEMA 23 step motors.

    The original carnival versions were more like Scalextric sets with a powered track and motors on the horse carriage

    image

    https://rollaball.co.uk/product/model-motor/

    The horses also had linkages to animate their heads and tails and rider as they moved along the track

    image

    You have a choice of sticking with this method or going with a belt type drive with a static motor.

    A static motor would perhaps be easier for determining carriage position but perhaps more fiddly if you wanted to add in an extra 6' of race track, as you would need to change the length of the 12 belts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    You may find some of these construction tips videos by Tim Hunkin useful:

       https://www.youtube.com/playlist?list=PLtaR0lZhSyANYB0Xxb9OSp47pHuQmj3Ol

    He has spent a lifetime building electromechanical arcade machines.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    I absolutely am chuffed.  Thank you so much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave

    Scalextric style power perhaps has the advantage that it supplies power to the carriage as it is being driven so you have the option for powering other stuff on the carriage as well as the motor.

    Although these days you could use rechargeable batteries with a belt drive system.

    Depends if you ever see yourself wanting to get creative with the carriages. At Xmas you could be racing Xmas trees and want them to light up as they move down the track or have the reindeer noses and Santa's sleigh light up.

    If you are going to be putting a fair bit of time and effort into building this, then you perhaps want to try keep your options open for enhancing it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    Hmmm. Interesting. Similar to the old automatons from the 18th and 19th centuries. Do you think this is like a slot car track underneath? Two brushes? How would I send a signal without using stepper motors? A timer? This is very simple, yet my brain is more advanced. This is a case of TMI with newer technologies (sadly). I believe a simple design is the best and most effective plan. This falls into that category, but I'm not sure how. The horses can be 3D printed along with the jockey and levers, and even the chassis. Getting voltage to the motor isn't a problem. It's telling the motor how many revolutions ---> distance to go for each point scored. And provide a beam breaker to identify the winner at the end. I found the company that makes this: https://eltonamusements.com/derby-games/  

    Which would you create with what we've both researched? I'm no engineer. I'm a guy who tears everything apart to figure out how it was built and reassemble it, and think about how it works in other applications. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>