Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Mar 2023 2:01 AM Date Created
  • Last Updated Last Updated: 17 Mar 2023 8:24 AM
  • Views 24989 views
  • Likes 10 likes
  • Comments 46 comments

Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594

I’ve got a studio light which has suddenly become faulty, how hard could it be to fix it rather than replace? In today’s episode I try and fault find the PCB to see if its a fault I can fix.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
8 bit MCU, STM8S003F3P6TR STMICROELECTRONICS 1 Buy Now
Fixed LDO Voltage Regulator HOLTEK 1 Buy Now
Pluggable Terminal Block WAGO 3 Buy Now
 

Additional Parts:

Fault studio light

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • fault finding
  • e14p_KD
  • neewar
  • Pluggable Voltage Regulator
  • 8 bit mcu
  • Fixed LDO Voltage Regulator
  • Studio Light
  • st
  • friday_release
  • led panel repair
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 3 years ago in reply to RichG +3
    I'm quite tempted to go completely away from the original design and do a 555 based controller, the main operation of the micro was to take the potentiometer input and turn it in to a PWM to the LED driver…
  • RichG
    RichG over 3 years ago +1
    Yes a new project with a microcontroller.
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to hifromkatie

      hifromkatie You are building a bigger box, for no reason. As an Integration & Sustaining Engineer, I used to work on all sorts of stuff,   And I had a problem, which you seem to have. STOP BUILDING BIGGER BOXES! It's a disease. please refer to Occam's razor. Where the simplest solution is most likely the best.  You started to build the bigger box:
         "I'm tempted to challenge myself and replace it with a 555-based circuit though, to output the PWM signal based on the pots to the LED drivers,              potentially still using the existing drivers, but if I redo them, I can get a single drop-in replacement PCB made with the 555s(/556), LED drivers and        power produced, which I think would be a pretty neat solution, just a little more time-consuming." 
    I hope you don't. do easier things like wire a new CPU to the board, maybe something different if you have the toolset. You just need to get the I/O of the new CPU to the old CPU and start to program it. AND get rid of the LDO in favor of a better device like an LM780x but with one more component a Zener Diode across the input side of the regulator and you want it about .5vdc above the input voltage. This way a transient from the wall wart, will not do any damage, as when the voltage rises it will be directed to the ground. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to DAB

    Thanks, I think a rebuild will be the most fun option. Currently looking at a 555 based control to replace the micro, as think that'd be a different way to solve it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to dougw

    Smell tests, yes thats usually an obvious one, along with heat. Years ago I was fault finding regularly for work (thankfully with circuit diagrams and parts lists), and a very infrequently we'd get really stuck, and the last resort was to just power it up without a current limit and see if anywhere went pop, got hot, started to smoke etc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to michaelkellett

    Yes, something to consider in a future redesign. I have many different barrel plugs lying around my workshop, with various voltages, they are all labelled up with what they should be connected to, but I can't for certain say that something didn't get plugged in incorrectly, or just that there wasn't some sort of power fluctuation at some point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to phoenixcomm

    I immediately thought I'd just replace the microcontroller with a replacement, and write my own code, especially as the programming header is on the PCB and easy to connect in to.
    I'm tempted to challenge myself and replace it with a 555 based circuit though, to output the PWM signal based on the pots to the LED drivers, potentially still using the existing drivers, but if I re do them, I can get a single drop in replacement PCB made with the 555s(/556), LED drivers and power produced, which I think would be a pretty neat solution, just a little more time consuming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to scottiebabe

    It seems to MCU was providing a PWM to the LED drivers circuit, so think it'd be fairly easy to use a 555 to replace this PWM control. A quick power up directly on the LED panel and it seems that is still working correctly, so I think it's just a case of build a new control circuit and new LED constant currant driver on a PCB that can be dropped into the case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to jc2048

    As beacon_dave says below there are 2 separate controls, which the micro converts into 2 seperate PWM outputs to LED drivers, 1 for yellow(ish) LEDs and the other for bright white LEDs, so you can adjust the brightness of each and therefore the colour temperature of the light output.

    In hindsight removing the caps was unlikely to help, but I have had an occurrence where a ceramic cap had hairline cracked through it due to an impact, and I wondered if that had happened again.

    My current idea is to use a 555 for control and avoid using a micro for a replacement control board, not really any reason other than to challenge myself to not use one in it's repair.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to phoenixcomm

    I sort of found the regulator and jumped straight in to that being the problem, I should have checked further along before assuming that was the problem. There was quite a bit of troubleshooting that got cut, as we almost had a 1 hour video of the highlights, unfortunately because I spent a while poking at it, there was also times I just wasn't recording.
    My plan is to build a replacement controller, but will probably skip the micro and use a 555 to produce the PWM control for the LED drivers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to beacon_dave

    Oh also no battery charging, just the ability to power from them, I don't have any of the compatible Sony battery packs though so have never used those connectors

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to beacon_dave

    Lots of interesting ideas, in fact the replacement I got for this one is a new "upgraded" version which has a small LCD screen for displaying the brightness and colour temp, and is wirelessly controlled by a remote either individually or you can change all of them in a room at the same time!

    The LED side works perfectly, I checked that, but I don't think it made the cut for the video, we almost ended up with a 1hour long video of the highlights!
    Definitely will be reusing the external casing, barn doors, LED panel (It's a single PCB).
    The pots are analogue inputs to the micro which is then PWM control to the LED drivers, I'm tempted to simplify the circuit and make a drop in replacement PCB which will line up with the holes for the pots, but these will be fed into a 555  (or 556, as theres 2 to control) and output a PWM to the LED drivers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>