Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Raspberry Pi 4 Experimental Resin 3D Printer -- Episode 414
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 30 Sep 2019 8:47 PM Date Created
  • Last Updated Last Updated: 4 Oct 2019 7:24 AM
  • Views 10589 views
  • Likes 17 likes
  • Comments 27 comments

Raspberry Pi 4 Experimental Resin 3D Printer -- Episode 414

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
 

Tiny resin based 3D printers may be all the rage now, but size matter sometimes, and how these printers operate does not scale up well. Clem has an Idea to circumvent these technical limitations with a ground breaking giant 4k Resin 3D printer! Utilizing 2 Raspberry Pis (4 & 3B+) he sets out to prove that FEP foil can be replaced with a specialized liquid, making the LCD-masking technique viable for large format 3D printers!

Supplemental Content:

  • A lot of parts for the mechanics were salvaged from this project: Episode 359: Make Your Own CNC Pyrography Wood Burner
  • The heatsinks were covered in-depth in this video:  Episode 399: Candle-Powered Robot
  • The main board for the giant 3D printer is the MAYER MOVES Dev Kit showcased in this episode: Episode 410: MacPro G5 Cheese Grater with Raspberry Pi 4
  • Click here to get the complete MAYER MOVES Motor Control Dev Kit

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Raspberry pi 4B Raspberry-PI 1 Buy Now
Raspberry p3B /3B+ Raspberry-PI 1 Buy Now
PRO SIGNAL Audio / Video Cable Assembly, HDMI A Plug to Micro HDMI D Plug, 6.6 ft, 2 m, Black PRO SIGNAL 1 Buy Now
CARLO GAVAZZI Solid State Relay, SPST-NO, 25 A, 280 VAC, Panel, Screw, Zero Crossing CARLO GAVAZZI 1 Buy Now
RASPBERRY-PI Daughter Board, Raspberry Pi 7" Touch Screen Display, 10 Finger Capacitive Touch RASPBERRY-PI 1 Buy Now
MEAN WELL AC/DC Enclosed Power Supply (PSU), ITE, 1 Outputs, 100.8 W, 36 V, 2.8 A MEAN WELL 1 Buy Now
MEAN WELL AC/DC Enclosed Power Supply (PSU), ITE, 1 Outputs, 50.4 W, 12 V, 4.2 A MEAN WELL 1 Buy Now
MULTICOMP Axial Fan, 12 V, DC, 60 mm, 33.05 dBA, 18.84 cu.ft/min MULTICOMP 3 Buy Now
MEAN WELL AC/DC Enclosed Power Supply (PSU), ITE, 1 Outputs, 15 W, 5 V, 3 A MEAN WELL 2 Buy Now
TRINAMIC Evaluation Board, TMC2209 SilentStepStick, 2-Phase Motor Driver TRINAMIC 1 Buy Now
NANOTEC Stepper Motor, High Torque, DC, 0.5 N-m, 1.8 A, Two Phase, 1.75 ohm, 3.3 mH NANOTEC 1 Buy Now
OMRON Microswitch, Snap Action, Hinge Roller Lever, SPDT, Solder, 5 A OMRON 1 Buy Now

 

Additional Parts:

Product Name

4k instore Display Monitor 28“

Aluminium Extrusion for the Frame

PMMA-XT for the Vat

PMMA/Acrylic for the Case

3D printing filament for all the printed parts

UV LEDs  and heatsinks

Attachments:
ResinPrinter_Resources.zip
image
Rasperry Pi4 Resin 3d Experimental Printer

element14 Presents  |  About Clem  |  Project Videos

  • 3d printer
  • formlabs
  • large 3d printer
  • clem
  • 4k 3d printer
  • nonotec
  • solid state relay
  • e14presents
  • trinamic
  • anycubic photon
  • omron
  • resin printer upgrade
  • e14presents_mayermakes
  • resin printer
  • big 3d printer
  • elegoo mars
  • large resin printer
  • raspberry pi 4
  • giant 3d printer
  • 2-phase motor
  • Raspberry Pi Touchscreen
  • fom1
  • diy 3d printer
  • multicomp
  • form2
  • pro signal
  • friday_release
  • 4k resin printer
  • mayermakes
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 7 years ago +5
    If you have any questions I'll be happy to answer them here. Clarification on the Firmware: NanoDLP is FREE(as in cost) , but it is not open source. You can use share and distribute it freely even comercially…
  • pumpernickel
    pumpernickel over 7 years ago +3
    Hello! I wrote some ideas about a large format MSLA printer in the youtube comments and was asked to post em here. I've thought about three ways, each with their advantages and disadvantages: 1. Easiest…
  • deadbe3f
    deadbe3f over 6 years ago +3
    Hi Clem, I found your youtube video very interesting, I am wondering why not use the low refractive index substrate with a silicone applied coating? lots of laser resin folks are using acrylic like vats…
Parents
  • kk6vxx
    kk6vxx over 6 years ago

    Hello! retyping my thoughts from my youtube comment:

    I recommend you make a build tank out of solvent welded acrylic, and a base of thin plastic film. This will allow you to see how thick your gap liquid layer is from the side of the tank. a tub with rounded edges makes this impossible and has too thick a base. You want as little distance from pixels-to-resin as possible which means the gap liquid+plastic film needs to be as thin as possible.

    As for bubbles, I pour the resin in the tank and then give it like 10 minutes to settle, then i use the build plate motor to stir it up and down but under the surface so you don't introduce further bubbles. maybe add the gap liquid only after the resin is well stirred & de-bubbled.

    It seems like for this method to work you really have to avoid agitating the gap liquid which probably means running the thing super slow. as the build plate moves up there will be a strong suction force inward which will disturb the uniformity of the gap liquid. perforating the build plate should reduce this force in the early layers. also using a physically smaller build plate, like just the size of one benchy for starters, because the smaller the build plate the less it disturbs the fluid.

    It will maybe also be necessary to glue down the plastic sheet to the display surface (like with a light dusting of contact adhesive like super77) to prevent it from pulling away from the display under the forces.

    I'm not a chemist, I'd love to hear from one on how to increase the separating forces between the liquids, like maybe if the resin is less dense and gap liquid more dense then they will want to more strongly separate. If density is part of what makes the gap liquid fall and the resin float, then you should measure the densities of various resins and use the lightest one, and figure out how to increase the density of the gap liquid. I think i'm talking about the buoyant forces like what makes oil float on water.

    Another maybe useful idea is to put a sort of plastic mesh or fine netting material against the display and putting enough gap liquid to *just* cover up the mesh material. it'd act as a baffle keeping the gap liquid mostly in place, in the case where the suction forces are disturbing the interface too strongly.

    alright, that's all I can think of right now. Cant wait to see more experiments image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 6 years ago in reply to kk6vxx

    Hi, thanks for sharing your ideas here. I will add some of them for the Q&A when I finally get to the second iteration.
    O nthe separation forces: density of course is a factor, but the resin does not seem to be always at the same density from batch to batch and also behaves differently at different temperatures, over the course of a print it warms up a bit. For floating it was crucial to have unbroken surface tension. so I increased the density of the liquid but also had to make sure the surface would not get broken. which made removing air bubles areal pain.

     

    to avoid having to deal with it the current plan for C.L.E.M. iteration 2 is to put it on its head and have avery deep floating liquid that supports a bigger amount of resin and the topmost layer wil lget cured not the layer at the seperation zone of the two liquids.
    this avoids having to make sure for a perfectly clean separation and only needs it to be a uniform layer of resin that levels itself by gravity.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 6 years ago in reply to kk6vxx

    Hi, thanks for sharing your ideas here. I will add some of them for the Q&A when I finally get to the second iteration.
    O nthe separation forces: density of course is a factor, but the resin does not seem to be always at the same density from batch to batch and also behaves differently at different temperatures, over the course of a print it warms up a bit. For floating it was crucial to have unbroken surface tension. so I increased the density of the liquid but also had to make sure the surface would not get broken. which made removing air bubles areal pain.

     

    to avoid having to deal with it the current plan for C.L.E.M. iteration 2 is to put it on its head and have avery deep floating liquid that supports a bigger amount of resin and the topmost layer wil lget cured not the layer at the seperation zone of the two liquids.
    this avoids having to make sure for a perfectly clean separation and only needs it to be a uniform layer of resin that levels itself by gravity.