Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Arduino Helicopter Collective Joystick Control -- Episode 440
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 1 Apr 2020 8:47 PM Date Created
  • Last Updated Last Updated: 3 Apr 2020 7:24 AM
  • Views 35800 views
  • Likes 15 likes
  • Comments 139 comments

DIY Arduino Helicopter Collective Joystick Control -- Episode 440

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
 

I love to fly in simulators, especially helicopters. But, there is just not an affordable collective control that I have found, so I decided to make one for myself! I am going to build a joystick using an Arduino Micro, with a bunch of buttons for assignable controls and a high quality encoder for the collective axis.

Supplemental Content:

  • Download Code from Github
  • View Model and download 3d Cad files

 

Also you can watch the live Twitch recording about this build: element14 Presents Live Twitch Stream: DIY Arduino Helicopter Collective Joystick Control

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
BOURNS Absolute Rotary Encoder, 120 rpm, 128 PPR, EAW Series BOURNS 1 Buy Now
ARDUINO Development Board, Arduino Micro, ATmega32U4 MCU, 20 3.3V I/O, 12 Analogue Inputs, ISCP Header ARDUINO 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Square ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Square ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Round ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Round ITW SWITCHES 1 Buy Now
C & K COMPONENTS SWITCH, SPDT, 5A, 120VAC C & K COMPONENTS 3 Buy Now
BOURNS Incremental Rotary Encoder, Pro Audio, Continuous. 24 Detents, 24 Pulses, Quadrature Output BOURNS 1 Buy Now

 

Additional Parts:

 

Product Name

5 Way Momentary Square SMD Tactitle Switch

M3x5x2 Square Nuts

8mm Bore Diameter ball mounted pillow blocks

T6 Seamless Aluminum Round Straight Tubing 16 Gauge 1-3/8" OD

Attachments:
HelicopterCollective_Resources.zip
image
DIY Arduino Helicopter Collective Joystick Control

element14 presents  |  About Kaleb |  Project Videos

  • kaleb
  • e14presents_kalebclark
  • itw
  • arduino micro
  • rotary encoder
  • friday release
  • diy arduino helicopter collective joystick control
  • bourns
  • arduino
  • e14p_KC
  • helicopter
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • benaim
    benaim over 6 years ago +5
    One good project, it's one project that you can modify So I changed my mind, I use now one hall sensor AS5048a with 14-bit resolution ( Best resolution and linerality ) I changed too, the place of friction…
  • benaim
    benaim over 6 years ago in reply to benaim +4
    Pictures coming, better later than never So I used on SS495a, and to have one big range of value for "only" 45° of move, I done one adapter with 2 magnets. With this I have near 0 to 5 Volts on SS495a…
  • benaim
    benaim over 6 years ago in reply to KalebTheMaker +3
    Just received my two Bore Diameter ball So, now I can continue this project Kaleb, Thanks for sending a diagram to all followers I don't need because, I changed somethings, for example angle sensor and…
Parents
  • benaim
    benaim over 6 years ago

    Very nice I just ordered all that I need, but for elevation I will try another thing... image

     

    Why not use the Hall effect sensor for elevation instead of a big gear ? image

    I think is more precise, and less mechanical...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 6 years ago in reply to benaim

    It's just the route I took, Initial idea was to go with a timing belt for more precision, but... space.

     

    What hall effect sensor did you go with?

     

    -Kaleb

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dnl40
    dnl40 over 6 years ago in reply to benaim

    That is awsome Philippe, thanks. I am low on cash for now but in a couple of months I will be beginning to buy parts, (for now i am just doing the pricing). If during the construction phase i get stuck I hope is ok to give you a shout out with a question or two jejejeje. Thanks again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Charlienofun
    Charlienofun over 5 years ago in reply to benaim

    Hi Philippe - can you advise on the magnet sizes I should use? (first time using a hall sensor like this). I thought the potentiometer I had was having a short enough rotation but not in reality imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • benaim
    benaim over 5 years ago in reply to Charlienofun

    I use square magnet 5x5x5. 

    I make this choice because many round magnets are not polarised correctly, and too much sellers send bads magnets

    NB: now I use AS5048a it's more precise than SS495a, of course it's working now in SPI interface, not in analog.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Charlienofun
    Charlienofun over 5 years ago in reply to benaim

    Thanks, benaim, I will go for the bigger square magnets. Did you have to play with magnet distance a lot to get the full range from 45 degrees of rotation? Maybe I should make my mount adjustable instead of hard 45. Interesting you moved to AS5048a, I'm on a Pro micro (planning to fly a quadcopter) and the SPI pins are not used so I could try that as well (will check the datasheet and order one to experiment with as well). Thanks for the info!! Great project KalebTheMaker

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • benaim
    benaim over 5 years ago in reply to Charlienofun

    I can see on your second picture, the distance is good for AS5048a but for SS495a is not the good way, SS495a mesure the distance, not angle like AS5048a

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Charlienofun
    Charlienofun over 5 years ago in reply to benaim

    Thanks, benaim I see now the AS5048a is popular for brushless gimbal position. Many PCBs like this I could use in place of the one I have with the potentiometer now. Will pause on the linear sensor and look into this further. Seems like a better solution! Much appreciate the info!! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Charlienofun
    Charlienofun over 5 years ago in reply to Charlienofun

    I might try the AS5600 - lots of cheap kits with magnets and examples of it working on youtube.

     

    https://www.ebay.com/itm/AS5600-Magnetic-Encoder-Magnetic-Induction-Angle-Measurement-Sensor-IIC-Module/164243118854?_tr…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • benaim
    benaim over 5 years ago in reply to Charlienofun

    Yes I use this board (https://m.fr.aliexpress.com/item/1005001622340192.html) in SPI mode, not analog...

    In SPI is very accurate, in particular with low angles, for us only 45° maybe less.

     

    Don't forget, you need 4 pins for SPI ( SCLK / MISO /MOSI) but one more for control each SPI device, same if you have only one...

     

    I'm now on my smartphone, tomorrow, when I will be on my computer, I will send, here, the link of library that I use.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Charlienofun
    Charlienofun over 5 years ago in reply to benaim

    Ah, I will look at the lib when you get a chance to post it. No rush will be a while before I get a sensor board from China. I was planning to be lazy and try the analog mode of 5600, but first setting its range with i2c so it will have a full 0-5v from whatever rotation it can sense (I got the idea from this demo video from AMS) If that works I don't have to rewrite my existing code image Did you bother with trying this or just went straight to reading the angle over SPI?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • benaim
    benaim over 5 years ago in reply to Charlienofun

    The Lib SPI for AS5048a is here : https://github.com/eborghi10/AS5048A  image

     

    I to read the angle over SPI, it's more accurate image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • benaim
    benaim over 5 years ago in reply to Charlienofun

    The Lib SPI for AS5048a is here : https://github.com/eborghi10/AS5048A  image

     

    I to read the angle over SPI, it's more accurate image