Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Arduino Helicopter Collective Joystick Control -- Episode 440
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
EMI-Reduction-Techniques
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 1 Apr 2020 8:47 PM Date Created
  • Last Updated Last Updated: 3 Apr 2020 7:24 AM
  • Views 31682 views
  • Likes 15 likes
  • Comments 139 comments

DIY Arduino Helicopter Collective Joystick Control -- Episode 440

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
 

I love to fly in simulators, especially helicopters. But, there is just not an affordable collective control that I have found, so I decided to make one for myself! I am going to build a joystick using an Arduino Micro, with a bunch of buttons for assignable controls and a high quality encoder for the collective axis.

Supplemental Content:

  • Download Code from Github
  • View Model and download 3d Cad files

 

Also you can watch the live Twitch recording about this build: element14 Presents Live Twitch Stream: DIY Arduino Helicopter Collective Joystick Control

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
BOURNS Absolute Rotary Encoder, 120 rpm, 128 PPR, EAW Series BOURNS 1 Buy Now
ARDUINO Development Board, Arduino Micro, ATmega32U4 MCU, 20 3.3V I/O, 12 Analogue Inputs, ISCP Header ARDUINO 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Square ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Square ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Round ITW SWITCHES 1 Buy Now
ITW SWITCHES Pushbutton Switch, Industrial, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Round ITW SWITCHES 1 Buy Now
C & K COMPONENTS SWITCH, SPDT, 5A, 120VAC C & K COMPONENTS 3 Buy Now
BOURNS Incremental Rotary Encoder, Pro Audio, Continuous. 24 Detents, 24 Pulses, Quadrature Output BOURNS 1 Buy Now

 

Additional Parts:

 

Product Name

5 Way Momentary Square SMD Tactitle Switch

M3x5x2 Square Nuts

8mm Bore Diameter ball mounted pillow blocks

T6 Seamless Aluminum Round Straight Tubing 16 Gauge 1-3/8" OD

Attachments:
HelicopterCollective_Resources.zip
image
DIY Arduino Helicopter Collective Joystick Control

element14 presents  |  About Kaleb |  Project Videos

  • kaleb
  • e14presents_kalebclark
  • itw
  • arduino micro
  • rotary encoder
  • friday release
  • diy arduino helicopter collective joystick control
  • bourns
  • arduino
  • e14p_KC
  • helicopter
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • benaim
    benaim over 5 years ago +5
    One good project, it's one project that you can modify So I changed my mind, I use now one hall sensor AS5048a with 14-bit resolution ( Best resolution and linerality ) I changed too, the place of friction…
  • benaim
    benaim over 5 years ago in reply to benaim +4
    Pictures coming, better later than never So I used on SS495a, and to have one big range of value for "only" 45° of move, I done one adapter with 2 magnets. With this I have near 0 to 5 Volts on SS495a…
  • benaim
    benaim over 5 years ago in reply to KalebTheMaker +3
    Just received my two Bore Diameter ball So, now I can continue this project Kaleb, Thanks for sending a diagram to all followers I don't need because, I changed somethings, for example angle sensor and…
  • webitman
    webitman over 3 years ago in reply to beacon_dave

    Sorry beacon_dave I should of checked, thank you once again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to webitman

    If you look at the Adafruit example I linked to above, then they use this format to set the pin to an input with pullup:

    // configure button pin for input with pull up
    mcp.pinMode(BUTTON_PIN, INPUT_PULLUP);

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • webitman
    webitman over 3 years ago in reply to beacon_dave

    Yes I have already changed that to mcp_I2C and that was OK, but as it reached the mcp pinMode it passed  15, 14 ,13 but halted on pinMode 12 button 4

    with  "class adafruit_mcp23X17 has no member named pullup" I have checked that all 4 button pullups are writen exactly the same, and checked spelling for any changes, and all match.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to webitman

    You will likely need to change the mcp instance on the line below it as well, as per the Adafruit example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • webitman
    webitman over 3 years ago in reply to beacon_dave

    Thank you beacon_dave I will change the include and hopfully i will finaly finish these projects, thanks for your responce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to webitman

    Depends on the exact error message but looks like it can't find a file that is being referenced.

    Kaleb's CollectiveControl.ino references 'Adafruit_MCP23017.h'

    #include <Adafruit_MCP23017.h>

    but it looks like with the later Adafruit MCP23017 libraries this has changed to:

    #include <Adafruit_MCP23X17.h>

    https://learn.adafruit.com/adafruit-mcp23017-i2c-gpio-expander/arduino

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • webitman
    webitman over 3 years ago

    Hi Kaleb,

    I know these are old projects but I need your help if possible? at the moment I am persuing with two of your projects,

    this one and the MCP23017 and on both projects I cant get the Arduino code to upload?  on both codes its the same problem cant find MPC23017.h  file does not exists.

    I have installed the MPC23017 using the arduino file manager and also by using the Zip file from github still keeps failing with ( file does not exist ) do you have any ideal what the problem could be or how to get this to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fanavaran.company
    fanavaran.company over 3 years ago


    What simulator software does this joystick work on?
    In this case, if possible, give a full explanation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Steeple
    Steeple over 4 years ago in reply to benaim

    Busy printing and collecting parts. Would you mind sharing some dimensions of your friction mod or better still an stl file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jlaingen
    jlaingen over 4 years ago in reply to jlaingen

    Resolved the issue. There are multiple "joystick" libraries and not all are created equal. I located the correct library by searching for one with value the code called out as not defined, in this case "JOYSTICK_DEFAULT_REPORT_ID".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>