Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Designing an Arduino PID Controlled Micro Drone -- Episode 668
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: e14cstanton
  • Date Created: 3 Jun 2025 5:03 PM Date Created
  • Last Updated Last Updated: 5 Jun 2025 2:19 PM
  • Views 13357 views
  • Likes 5 likes
  • Comments 11 comments

Designing an Arduino PID Controlled Micro Drone -- Episode 668

In this video, Milos builds a fully custom micro drone from scratch using the Arduino Nicla Vision board—no off-the-shelf flight controllers, just custom PCBs, hand-written flight control code, and a lot of trial and error. He walks through the full process from hardware design to PID-based stabilization and joystick-controlled flight via Python. Watch the full build and flight test to see how it all came together.

Watch the Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

There aren’t many people who tried flying a drone and then didn’t like it! It’s incredibly fun to control something that you can look at soar through the air. In this video, Milos wanted to make a tiny drone from zero without relying on things like already tested flight controllers but do all of the electronics and code from scratch!

Building on a Previous Project

This isn’t the first drone Milos made, back in 2021, for a Project14 Competition called Attack of the Drones, Milos made a big Arduino based drone that he named the SRD1. It was based on 3 Arduino Nano boards, one for the flight controller, one for the radio receiver and one for the radio transmitted. If you’re interested in that big drone, look at these links:

  •  SRD-1 - 3D Printed Drone (Arduino + Raspberry) - June 11th Update - It Flies! 
  • https://github.com/MilosRasic98/SRD-1

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The drone he wanted to make this time was different. The size he was going for was two times smaller than the propeller of the original drone! He came onto this idea while working with the tiny Arduino Nicla vision board.

image

This little board packs a serious punch. It has a built-in camera, IMU, ToF sensor, Wifi, it has everything you need to make a drone! Milos decided to build a custom PCB that will work as a shield for the Arduino Nicla Vision and that will house the rest of the electronics to keep everything as compact as possible.

Schematics of Electronics

This is where the “fun” began for Milos as he explains in the video. For the first PCB he didn’t go thoroughly through the data sheet, and the pinout was wrong for the Nicla Vision, so while he was trying to make it work, he managed to burn the onboard battery regulator… This didn’t deter him, and he continued by designing a new PCB. While still not perfect, it was good enough for him to make it work! Here are the full schematics and the look of the final PCB.

image

image

image

image

imageimage

imageimage

The PCB was designed to be as small as possible with the Arduino taking the central position because of the IMU. Acting as a roll bar, he added a part of the PCB to stick out at the top, so it protects the delicate (and costly!) Arduino Nicla Vision in case of some crashes. This was also a perfect place for putting some LED-s that can be used to show the state the drone is in, for example, flashing green means it’s safe to touch, while flashing red means the drone is armed and could spin any of the motors up.

Practical and Mechanical Design

Mechanical design has taken a few attempts to get just right. He initially wanted to use small 717 motors, but they were too lacking in thrust, so he decided to instead go with the much more powerful 8520 motors, which are some motors used in the DJI Tello drone. These motors proved to be more than powerful enough for this drone. Nevertheless, Milos still tried keeping the drone as light as possible and he tried maximising that by designing the frame to be as tiny as possible while still being strong. Here are some of the designs he tried before settling on the final one.

image

image

image

image

For printing materials, he experimented both with PLA and PETG. PLA gives a stiffer frame but is more brittle and more likely to crack on impact. While PETG is a bit less stiff, it takes impacts incredibly well with less chance of something breaking. In the end, both materials proved to work rather well, so you can choose any, or experiment with something more exotic.

Coding the Software

With all the mechanical and electrical stuff figured out, the only thing left now is controlling the drone and software. For this, Milos decided to go on a route that he believes will be natural for most people, and that’s by using a joystick connected to a PC. He used a regular flight joystick stick for this, but you can use any joystick that connects over USB. A code in Python using the PyGame library captures all the inputs from the joystick and then sends them over UDP to the drone. Important thing to note here, the PC and the Drone must be on the same network for this work in this setup!

Since Milos wanted to do everything from zero and make this video as educational as possible, this included the flight controller software as well. There are a lot of open-source flight controllers that you can flash to an Arduino, such as MultiWii, but Milos wanted to try writing a bare bones controller from scratch. This meant he had to write 3 PID controllers for the Pitch, Roll & Yaw axis to stabilise the drone in flight. If you’re interested in more detail, he did a full explanation on how PID controllers work, and why they are necessary for the drone in the video.

image

After all of this, the only thing left to do was test the drone, but to find out how that went, you’ll need to check out the video above!

Supporting Links and Files

  •  SRD-1 - 3D Printed Drone (Arduino + Raspberry) - June 11th Update - It Flies! 
  •  Spying Under the Christmas Tree with an Arduino-powered Ornament -- Episode-633  
  •  Supporting Files for Episode 668 of element14 presents 

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Arduino Nicla Vision - ABX00051 ARDUINO 1 Buy Now
MCPAS03W4J0472T5E MULTICOMP PRO 2 Buy Now
GRT21BR60J476ME13L MURATA 5 Buy Now
DMN3065LW-7 DIODES INC 7 Buy Now
RBR3LAM40CTFTR ROHM 5 Buy Now
MC34152DG ONSEMI 2 Buy Now
GRM21BR61E226ME44L MURATA 6 Buy Now
C0603X104K8RACAUTO YAGEO 5 Buy Now
RCG060310R0FKEA VISHAY 4 Buy Now
TPS61085PWR TEXAS INSTRUMENTS 1 Buy Now
MSS7341-502NLB COILCRAFT 1 Buy Now
C0603C112J5GACTU YAGEO 1 Buy Now
RP0603BRD0730KL YAGEO 1 Buy Now
ERJP03F7502V PANASONIC 2 Buy Now
RC0603JR-07100KL YAGEO 4 Buy Now
ERA3VRB8201V PANASONIC 1 Buy Now
150066M153000 WURTH 2 Buy Now
ERJUP3J681V PANASONIC 6 Buy Now
CRCW06031K00JNEAIF VISHAY 3 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
2.54mm Pitch Male and Female Headers
8520 Motors with Propellers
PLA or PETG filament for 3D Printing
USB Joystick
Small 1S LION Battery

element14 presents

element14 presents  |  About Milos Rasic |  Project Videos

  • 8520 motors
  • diy drone
  • fpv drone build
  • drone flight controller
  • ardupilot
  • Arduino Nicla Vision
  • diy quadcopter
  • drone from scratch
  • Arduino drone
  • cutsom pcb drone
  • python drone control
  • joystick drone control
  • mini drone project
  • drone electronics
  • pid controller drone
  • micro drone
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 1 year ago in reply to beacon_dave +1
    Yep.
Parents
  • kmikemoo
    kmikemoo over 1 year ago

     milosrasic98 Bold project.  Great presentation.  Impressive on the detail.  Well done. Thumbsup  There is no way I'm trying this. Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to kmikemoo

    Thanks! I just wanted to see it off the ground in the end no matter what hahahaha. The project is fun to try if you by chance have a Nicla Vision laying around. If not I plan on doing a more stable (able to fly without hitting the wall) drone soon, just deciding how big to go with it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • milosrasic98
    milosrasic98 over 1 year ago in reply to kmikemoo

    Thanks! I just wanted to see it off the ground in the end no matter what hahahaha. The project is fun to try if you by chance have a Nicla Vision laying around. If not I plan on doing a more stable (able to fly without hitting the wall) drone soon, just deciding how big to go with it!