Hardware Hacking
  • Challenges & Projects
  • Project14
  • Hardware Hacking
  • More
  • Cancel
Hardware Hacking
Forum Hardware hacking an electric fan heater without burning the house down
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hardware Hacking to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 14 subscribers
  • Views 6591 views
  • Users 0 members are here
  • hardwarehackingch
Related

Hardware hacking an electric fan heater without burning the house down

BigG
BigG over 6 years ago

I recently purchased a 2kW electric fan heater for $12 (it was on sale). This was an offer too good to refuse, especially as the latest Project14 competition is hardware hacking.

 

image

 

These fan heaters, like any other personal heater, are great for the winter months.

 

However, as I have on the very odd occasion left an oil heater on over night (it is very easily done), I certainly wouldn't want to do the same with an electric fan heater.

 

So I want to add in some "smarts" or electronics to ensure that it can automatically turn off if I leave the room etc. and it would also be handy to remotely adjust heat and fan speed.

 

The nice thing about this particular fan heater is that it has a safety cut off switch, should it tip over. I thought that this would be my starting point for my project, as this part can be readily enhanced.

 

image

 

 

The part I am struggling with is how to or what electronic options could I use to hack the heater settings switch, which is mechanical. How could I do this electronically, bearing in mind we are dealing with mains voltage.

 

{gallery:autoplay=false} Heater Settings Switch

image

image

 

And the other question is what options are out there on how to hack the fan speed controller... this also is mains voltage, so I'm out of my depth in terms of using a digital potentiometer, for example.

 

image

 

Any suggestions / ideas would be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 6 years ago in reply to shabaz +1
    I am still unpacking and tearing it down myself to understand the wiring and the rest. I've yet to sketch out a wiring diagram and it's quite hard to capture the key elements in photos. It looks like two…
  • shabaz
    shabaz over 6 years ago in reply to BigG +1
    Hi Colin, I was looking at your photos earlier, and think that's a bimetallic strip (it bends when it gets hot, and self-disconnects). the rotary control just adjusts the point it occurs by moving it closer…
  • ralphjy
    ralphjy over 6 years ago +1
    Very interesting teardown. Always fun figuring out these electromechanical gadgets. You've almost inspired me to hack an old thermostatically controlled window fan but summer is here and I use it all the…
Parents
  • BigG
    BigG over 6 years ago

    The awesome thing about element14 is the wealth of expertise and the documented lessons learnt... Automatic Dough Shaper - Blog #10 More Magic Smoke

     

    Yes, I'm exploring triacs! Thankfully, I've ticked that off the list - i.e. know your power ratings etc. So I basically just want to use one triac for now to remotely turn the device on and off. I decided to place the triac above the microswitch as shown (will be snipping that red wire).

     

    image

     

    That's the plan anyway. I'm working through element14 as there are plenty links on triacs.

     

    Now when looking at my design process, I've zoomed straight onto snubber capacitors (I have a habit of doing that... zoning in on something that's probably not necessary but just want to understand).

     

    And, while searching online I came across these guys. They are reasonable price wise but are they appropriate... and if so, how do you choose.

    http://www.capacitorguide.com/mica-capacitor/

     

    Not sure what other bells and whistles are needed to look after the triac and the circuit for switching high loads. I'm basing my max load off 24A RMS (to cover the 6A + 16A).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to BigG

    image

    I've used this SSR to control AC with great success. The low voltage side is very compatible with a Pi. It has a large physical footprint probably not the size you are looking for then.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 6 years ago in reply to BigG

    image

    I've used this SSR to control AC with great success. The low voltage side is very compatible with a Pi. It has a large physical footprint probably not the size you are looking for then.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • BigG
    BigG over 6 years ago in reply to colporteur

    Thanks for this suggestion. I will certainly look at this option.