Radio Control
  • Challenges & Projects
  • Project14
  • Radio Control
  • More
  • Cancel
Radio Control
Blog FPGA: a quadrature oscillator with rotary encoder control
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Radio Control to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 20 Oct 2021 6:48 PM Date Created
  • Views 7132 views
  • Likes 1 like
  • Comments 15 comments
  • summer_of_fpgas
  • radiocontrolch
  • fpga
Related
Recommended

FPGA: a quadrature oscillator with rotary encoder control

Jan Cumps
Jan Cumps
20 Oct 2021

This design is a pure VHDL quadrature signal generator.

With variable frequency. The frequency can be controlled with a scroll wheel.

The purpose of this design is to build an alternative local oscilator for Shabaz' Software Defined Radio (SDR) Experiment Board.

 

image

 

I tried to make everything as standard as possible, so that it can be used on many FPGA makes and sizes.

I'm working on a Xilinx Spartan 6, with a 12 MHz clock (Xess XuLA2 kit).

 

image

 

The design has 4 inputs

  • rotary encoder pins A and B
  • clock  input
  • reset

and 5 outputs:

  • quadrature signals 0 -> 3
  • the variable clock based on the input clock and the encoder setting

 

image

 

The design is broken up in 3 components:

  • decoder to translate the movements of a scroll wheel into a numeric value.
  • variable clock that will stretch the input clock based on the value coming out of the decoder
  • quadrature signal generator will create 4 90° phase-shifted signals from that variable clock.

A wrapper glues the components together.

 

All this has been used before for my Pynq blog series and this Spartan 6 article: XuLA2 FPGA - Rotary Encoder and VHDL.

 

image

 

Because all the code has been documented before, I'm just putting the source here.

Check the link earlier in this post for explanations.

 

quad_decode_quad_osc.vhd

This code should be portable.

The external pins are defined in wrapper entity quad_decode_quad_osc.

 

-- ==============================================

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.NUMERIC_STD.ALL;

entity quadrature_decoder is
    Port ( QuadA : in  STD_LOGIC;
           QuadB : in  STD_LOGIC;
           Clk : in  STD_LOGIC;
           nReset : in STD_LOGIC;
           Position : out  unsigned (7 downto 0));
end quadrature_decoder;

architecture Behavioral of quadrature_decoder is

signal QuadA_Delayed: std_logic_vector(2 downto 0) := (others=>'0');
signal QuadB_Delayed: std_logic_vector(2 downto 0) := (others=>'0');

signal Count_Enable: STD_LOGIC;
signal Count_Direction: STD_LOGIC;

signal Count: unsigned(Position'length-1 downto 0) := (others=>'0');

begin

process (Clk, nReset)
begin
   if (nReset = '0') then
      Count <= (others=>'0');
      QuadA_Delayed <= (others=>'0');
      QuadB_Delayed <= (others=>'0');
   elsif rising_edge(Clk) then
      QuadA_Delayed <= (QuadA_Delayed(1), QuadA_Delayed(0), QuadA);
      QuadB_Delayed <= (QuadB_Delayed(1), QuadB_Delayed(0), QuadB);
      if Count_Enable='1' then
         if Count_Direction='1' then
            Count <= Count + 1;
            Position <= Count;
         else
            Count <= Count - 1;
            Position <= Count;
         end if;
      end if;
   end if;
end process;

Count_Enable <= QuadA_Delayed(1) xor QuadA_Delayed(2) xor QuadB_Delayed(1)
            xor QuadB_Delayed(2);
Count_Direction <= QuadA_Delayed(1) xor QuadB_Delayed(2);

end Behavioral;

-- ==============================================

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.NUMERIC_STD.ALL;

entity variable_clock is
    Port ( 
      clk_i    : in  STD_LOGIC;
      resetn_i : in  STD_LOGIC;
      ticks_i  : in  unsigned (7 downto 0);
      clk_o    : out STD_LOGIC
    );
end variable_clock;

architecture Behavioral of variable_clock is
  signal counter_s: natural range 0 to 2**ticks_i'length-1 := 0;
  signal clk_out_s: STD_LOGIC := '0';
begin

process (clk_i, resetn_i)

  procedure perform_reset is -- this procedure contains the reset action
  begin
      counter_s <= 0;
      clk_out_s <= '0';
  end procedure;

  procedure perform_action is -- this procedure contains the reset action
  begin
      if counter_s >= ticks_i then -- >= because the value can change
        counter_s <= 0;
        clk_out_s <= not clk_out_s;
      else
        counter_s <= counter_s + 1;
      end if;
  end procedure;

begin
  if rising_edge(clk_i) then
    if resetn_i = '0' then
      perform_reset;
    else
      perform_action;
    end if;
    clk_o <= clk_out_s;
  end if;
end process;  
  
end Behavioral;

-- ==============================================

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.NUMERIC_STD.ALL;

entity quadrature_oscillator is
  Port (
    clk_i     : in std_logic;
    resetn_i  : in std_logic;
    outputs_o : out std_logic_vector (3 downto 0)
   );
end quadrature_oscillator;

architecture Behavioral of quadrature_oscillator is
  signal pattern_s: std_logic_vector (6 downto 0) := "0011001";
  signal counter_s: natural range 0 to 3 := 0;

begin

process (clk_i, resetn_i)

  procedure perform_reset is -- this procedure contains the reset action
  begin
    counter_s <= 0;
  end procedure;

  procedure perform_action is -- this procedure contains the reset action
  begin
    if counter_s = 3 then 
      counter_s <= 0;
    else
      counter_s <= counter_s + 1;
    end if;
  end procedure;

begin
  if rising_edge(clk_i) then
    if resetn_i = '0' then
      perform_reset;
    else
      perform_action;
    end if;
    outputs_o(0) <= pattern_s(counter_s + 3); 
    outputs_o(1) <= pattern_s(counter_s + 2); 
    outputs_o(2) <= pattern_s(counter_s + 1); 
    outputs_o(3) <= pattern_s(counter_s + 0);
  end if;
end process;

end Behavioral;

-- ==============================================

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.NUMERIC_STD.ALL;

entity quad_decode_quad_osc is
    Port ( QuadA_in : in  STD_LOGIC;
           QuadB_in : in  STD_LOGIC;
           clk_in : in  STD_LOGIC;
           nReset_in : in  STD_LOGIC;
           oscillator_quad_out : out  STD_LOGIC_VECTOR (3 downto 0);
           clk_out : out  STD_LOGIC);
end quad_decode_quad_osc;

architecture Behavioral of quad_decode_quad_osc is

signal position_s : unsigned (7 downto 0);
signal clk_s : STD_LOGIC;

component quadrature_decoder is
    Port ( QuadA : in  STD_LOGIC;
           QuadB : in  STD_LOGIC;
           Clk : in  STD_LOGIC;
           nReset : in STD_LOGIC;
           Position : out  unsigned (7 downto 0));
end component quadrature_decoder;

component variable_clock is
    Port ( 
      clk_i    : in  STD_LOGIC;
      resetn_i : in  STD_LOGIC;
      ticks_i  : in  unsigned (7 downto 0);
      clk_o    : out STD_LOGIC
    );
end component variable_clock;

component quadrature_oscillator is
  Port (
    clk_i     : in std_logic;
    resetn_i  : in std_logic;
    outputs_o : out std_logic_vector (3 downto 0)
   );
end component quadrature_oscillator;

begin

quadrature_decoder_i: component quadrature_decoder
     port map (
   QuadA => QuadA_in,
   QuadB => QuadB_in,
   Clk => clk_in,
   nReset => nReset_in,
   Position (7 downto 0) => position_s (7 downto 0)
    );

variable_clock_i: component variable_clock
     port map (
   clk_i => clk_in,
   resetn_i => nReset_in,
   ticks_i (7 downto 0) => position_s (7 downto 0),
   clk_o => clk_s
    );

quadrature_oscillator_i: component quadrature_oscillator
     port map (
   clk_i => clk_s,
   resetn_i => nReset_in,
   outputs_o (3 downto 0) => oscillator_quad_out (3 downto 0)
    );

  clk_out <= clk_s;  

end Behavioral;

 

constraints.ucf

The external pins defined in quad_decode_quad_osc are mapped here.

I've mapped them for my specific board. Adapt for your FPGA/kit.

 

net clk_in                      loc=a9; # 12 MHz clock to FPGA.
net nReset_in                   loc=k15;


# PM1 connections for rotary encoder module.
net QuadA_in                    loc=r15;
net QuadB_in                    loc=m15;


# PM1 connections for the pwm outputs
net oscillator_quad_out[0]      loc=r7;
net oscillator_quad_out[1]      loc=r16;
net oscillator_quad_out[2]      loc=m16;
net oscillator_quad_out[3]      loc=k16;
net clk_out                     loc=t7;

 

Untested. I'll update if there are errors.

 

image

 

If used for Shabaz' SDR, pins [0]and [2] should go to the JFETS for one opamp. Pins [1] and [3] to the JFETS for the other. Because they are the 2 differential pairs.

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    It works

    image

     

    I had 1 error: the nReset pin was not in my constraint file. So it was always 0 and the circuit constantly in reset.

     

    I changed the constraint file (also moved the clk_out to a PMOD pin named clock)

    net nReset_in                   loc=k15;
    net clk_out                     loc=t7;

     

    and the image with the pins in the post above.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    With the 12 MHz clock:

    • the fastest quad is 1.5 MHz. period = 666 ns
    • Each click of the rotary adds 666 ns to the period of the signals.
    • After one click: period = 1333 ns = 750 kHz
    • After two clicks: period = 2 µS = 500 kHz, ...

     

    To have narrow steps at higher frequency, it helps to have a fast clock.

    On a Spartan 6, you can speed up with a clock manager:

     

    begin
    
       DCM_SP_inst : DCM_SP
       generic map (
          CLKFX_DIVIDE => 1,                     -- Divide value on CLKFX outputs - D - (1-32)
          CLKFX_MULTIPLY => 25                    -- Multiply value on CLKFX outputs - M - (2-32)
       )
       port map (
          CLKFX => clk_fast,    -- 1-bit output: Digital Frequency Synthesizer output (DFS)
          CLKIN => clk_i,       -- 1-bit input: Clock input
          RST => '0'            -- 1-bit input: Active high reset input
       );

     

    It's specific for this device, not portable.

     

    edit: tested it

     

    image

    20 ns per click of the encoder. It makes it more usable in low MHz range .

     

    Changes made to the source file:

    All in the very last object, quad_decode_quad_osc. Under the last -- ========================= divider.

     

    Added the custom Xilinx UNISIM lib for the clock manager primitive:

    library IEEE;
    use IEEE.STD_LOGIC_1164.ALL;
    use IEEE.NUMERIC_STD.ALL;
    library UNISIM;
    use UNISIM.VComponents.all;

     

    Created a signal to hold the fast clock generated by the primitive:

    signal position_s : unsigned (7 downto 0);
    signal clk_s : STD_LOGIC;
    signal clk_fast: STD_LOGIC;

     

    Put the primitive just after begin, wired input to the original 12 MHz clock, output to the new signal clk_fast

    begin
    
    DCM_SP_inst : DCM_SP
       generic map (
          CLKFX_DIVIDE => 1,                     -- Divide value on CLKFX outputs - D - (1-32)
          CLKFX_MULTIPLY => 25                    -- Multiply value on CLKFX outputs - M - (2-32)
       )
       port map (
          CLKFX => clk_fast,    -- 1-bit output: Digital Frequency Synthesizer output (DFS)
          CLKIN => clk_in,       -- 1-bit input: Clock input
          RST => '0'            -- 1-bit input: Active high reset input
       );
    
    quadrature_decoder_i: component quadrature_decoder

     

    Last step: used that clk_fast signal as input for the variable clock object:

    variable_clock_i: component variable_clock
         port map (
       clk_i => clk_fast,
       resetn_i => nReset_in,
    ticks_i => position_s,
    clk_o => clk_s
        );

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    With the 12 MHz clock:

    • the fastest quad is 1.5 MHz. period = 666 ns
    • Each click of the rotary adds 666 ns to the period of the signals.
    • After one click: period = 1333 ns = 750 kHz
    • After two clicks: period = 2 µS = 500 kHz, ...

     

    To have narrow steps at higher frequency, it helps to have a fast clock.

    On a Spartan 6, you can speed up with a clock manager:

     

    begin
    
       DCM_SP_inst : DCM_SP
       generic map (
          CLKFX_DIVIDE => 1,                     -- Divide value on CLKFX outputs - D - (1-32)
          CLKFX_MULTIPLY => 25                    -- Multiply value on CLKFX outputs - M - (2-32)
       )
       port map (
          CLKFX => clk_fast,    -- 1-bit output: Digital Frequency Synthesizer output (DFS)
          CLKIN => clk_i,       -- 1-bit input: Clock input
          RST => '0'            -- 1-bit input: Active high reset input
       );

     

    It's specific for this device, not portable.

     

    edit: tested it

     

    image

    20 ns per click of the encoder. It makes it more usable in low MHz range .

     

    Changes made to the source file:

    All in the very last object, quad_decode_quad_osc. Under the last -- ========================= divider.

     

    Added the custom Xilinx UNISIM lib for the clock manager primitive:

    library IEEE;
    use IEEE.STD_LOGIC_1164.ALL;
    use IEEE.NUMERIC_STD.ALL;
    library UNISIM;
    use UNISIM.VComponents.all;

     

    Created a signal to hold the fast clock generated by the primitive:

    signal position_s : unsigned (7 downto 0);
    signal clk_s : STD_LOGIC;
    signal clk_fast: STD_LOGIC;

     

    Put the primitive just after begin, wired input to the original 12 MHz clock, output to the new signal clk_fast

    begin
    
    DCM_SP_inst : DCM_SP
       generic map (
          CLKFX_DIVIDE => 1,                     -- Divide value on CLKFX outputs - D - (1-32)
          CLKFX_MULTIPLY => 25                    -- Multiply value on CLKFX outputs - M - (2-32)
       )
       port map (
          CLKFX => clk_fast,    -- 1-bit output: Digital Frequency Synthesizer output (DFS)
          CLKIN => clk_in,       -- 1-bit input: Clock input
          RST => '0'            -- 1-bit input: Active high reset input
       );
    
    quadrature_decoder_i: component quadrature_decoder

     

    Last step: used that clk_fast signal as input for the variable clock object:

    variable_clock_i: component variable_clock
         port map (
       clk_i => clk_fast,
       resetn_i => nReset_in,
    ticks_i => position_s,
    clk_o => clk_s
        );