Remote Monitoring & Control
  • Challenges & Projects
  • Project14
  • Remote Monitoring & Control
  • More
  • Cancel
Remote Monitoring & Control
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Remote Monitoring & Control to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • LoRa Experimental Environmental Sensors (LoRaXes) - Need to use a bigger case

    ralphjy
    ralphjy
    As we all experience with our projects - the Devil is in the details.  As I started to figure out how to mount all the components for the sensor in the case, I quickly realized that the case that I had chosen was too small.  One significant...
    • 21 Jul 2019
  • LoRa Experimental Environmental Sensors (LoRaXes) - Introduction

    ralphjy
    ralphjy
    I recently connected my Things Gateway to the Things Network and this Project14 challenge seemed like a good opportunity to do some experiments with the two MKR WAN 1300 boards that I received with the gateway.   I'd like to build a pair of por...
    • 17 Jul 2019
  • Big Petro Maker Magic:  $100 Datalogger That Can Save Millions

    Sean_Miller
    Sean_Miller
    This blog is in support of the Remote Monitoring & Control Project14 Challenge: "So that is my challenge - make a datalogger of 24 sensors logging data every one minute that could run without mains power or human intervention for 7 days with no...
    • 17 Jul 2019
  • CatDogFoxBot #4 : GridEye Sensor is Connected and Working

    dubbie
    dubbie
    I have now make the I2C connections between the GridEye sensor and the Nano. The specific GridEye sensor that I purchased did not seem to have any accompanying documentation, although it was claimed there was some on the suppliers website but I could...
    • 12 Jul 2019
  • Assaulting the cloud: uploading fitness data to IoT (part II)

    andyforeverest
    andyforeverest
    Remote Monitoring & ControlEnter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll Assaulting the cloud: uploading fi...
    • 11 Jul 2019
  • CatDogFoxBot #3 : The Step Motor Scanner is Working

    dubbie
    dubbie
    Having collected together all the parts I thought I needed to get started with my CatDogFoxBot Project14 effort for Remote Sensing and Control I happily sat down for a couple of hours using TinkerCAD to design some 3D printed parts to hold everythin...
    • 9 Jul 2019
  • CatDogFoxBot #2 : System Design and Gathering the Components

    dubbie
    dubbie
    Now that the Remote Monitoring and Control Project14 Challenge has started I have gathered together some of the components and PCBs that I am thinking of using, following on from my initial ideas (CatDogFoxBot #1 : My Initial Idea). The Grideye modu...
    • 8 Jul 2019
  • Smarthab: Remote Sensing and Control .iv  Software Design

    phoenixcomm
    phoenixcomm
    Ok, I have settled on the MSP-432 with the Kentec display. Out of the box the feature set is quite impressive:48MHz 32-bit ARM Cortex M4F with Floating Point Unit and DSP accelerationPower consumption: 95uA/MHz active, and 850nA RTC standby operation...
    • 4 Jul 2019
  • Smarthab: Remote Sensing and Control .iii  Sensors

    phoenixcomm
    phoenixcomm
    Lets say that my home has 2 bedrooms, 2.5 bathrooms, laundry, kitchen, Office, and a workroom(I like to tinker). So we are going to need six room controllers. So we will need several sensors in each of the rooms which in turn feed in the correspondin...
    • 3 Jul 2019
  • Assaulting the cloud: uploading fitness data to IoT

    andyforeverest
    andyforeverest
    Remote Monitoring & ControlEnter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll I have this Schwinn Airdyne AD-4 b...
    • 2 Jul 2019
  • Smarthab: Remote Sensing and Control .ii   Environmental Controls

    phoenixcomm
    phoenixcomm
    Ok, lets start what we mean by environmental control and what is it. Environmental control is what temperature, humidity, air quality.  Lets take theses one at a time so I don't loose you.Temperature:  This is the current temperature of...
    • 1 Jul 2019
  • Solar Panel Monitoring Using Particle Photon

    ruchir1674
    ruchir1674
    Remote Monitoring & ControlEnter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll      &nbs...
    • 23 Jun 2019
  • Air Quality Monitoring Using Particle Photon

    ruchir1674
    ruchir1674
    Remote Monitoring & ControlEnter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll      &nbs...
    • 22 Jun 2019
  • Smarthab: Remote Sensing and Control .I

    phoenixcomm
    phoenixcomm
    From the start, I have designed Smarthab with connectivity. Smarthab uses several forms of connectivity: Bluetooth, Zigbee,e WiFi, RFID, and Internet. And here is what they do:Zigbee - Interconnection of low-power devices in a mesh network such as m...
    • 19 Jun 2019
  • Combined homebrew and irrigation controller using Node Red

    lawsonkeith
    lawsonkeith
    Garage omni controller       For my control and automation project I have automated a couple of processes in the Garage.  Being a keen home brewer I've decided to upgrade my existing homebrew controller, the existing unit I had...
    • 19 Jun 2019
  • CatDogFoxBot #1 : My Initial Idea

    dubbie
    dubbie
    There are lots of good competitions and stuff going on at the moment and I am torn between which one or ones to get involved with. However, the Remote Monitoring and Control Project14 challenge is one I have been considering for some time. I am bless...
    • 18 Jun 2019
<