RFID or NFC
  • Challenges & Projects
  • Project14
  • RFID or NFC
  • More
  • Cancel
RFID or NFC
Project14: RFID or NFC Competition Low-Power NFC Thermometer
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RFID or NFC to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: misaz
  • Date Created: 19 Dec 2022 6:18 PM Date Created
  • Views 10030 views
  • Likes 10 likes
  • Comments 13 comments
  • rfidornfcch
  • tag
  • temperature
  • stm32
  • max31875
  • nfc
  • ST25
  • ST25DV64KC
Related
Recommended

Low-Power NFC Thermometer

misaz
misaz
19 Dec 2022
Low-Power NFC Thermometer

Hello everyone.

In this blog post I would like to describe my second project for a NFC or RFID Project14 Competition. In this project I utilized my own dynamic tag. This project tis about thermometer with output readable via NFC. Idea is that thermometer reads temperature at the background and saves output to the NFC tag. When you touch phone (or other NFC reader) to the tag, you can read the latest measured temperature.

Sample Sponsors

Experiments was also sponsored by ST. ST send me free samples of ST25DV64KC-IE6T3 NFC Tags. I ordered them in the time when shipping on their store was free, so I received them totally for free.

See it in the action!

On following video, you can see my final build in the action. Before recording I opened window. For this reason, ambient temperature decreased to about 16 °C. Then I touched thermometer by finger which increased temperature and after thermometer recorded new temperate (short green LED blink) I read new temperature with my phone again. Phone application is standard NFC reader app. It is designed for use without need to use project specific application.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Components

Devices integrates 4 components:

  • STMicroelectronics STM32G031 microcontroller in SO8 package.
  • Maxim Integrated (ADI) MAX31875 I2C Temperature Sensor on my own breakout board.
  • STMicroelectronics ST25DV64KC-IE6T3 Dynamic I2C NFC Type-5 Tag
  • Green LED

image

BOM

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
STM32G0316-DISCO, Discovery Kit, STM32G031J6M6U, 32 Bit, ARM Cortex-M0+ STMICROELECTRONICS 1 Buy Now
ST25DV64KC-IE8T3, NFC Tag STMICROELECTRONICS 1 Buy Now
MAX31875R0TZS+T, Temperature Sensor, ± 1°C, -20 °C, 150 °C, WLP4 MAXIM INTEGRATED / ANALOG DEVICES 1 Buy Now
CRG0603F4K7, SMD, 4.7 kohm, ± 1%, 100 mW, 0603, Thick Film NEOHM - TE CONNECTIVITY 5 Buy Now
C1608X7R1E104K080AA, SMD MLCC, 0.1 µF, 25 V, 0603, ± 10%, X7R TDK 2 Buy Now
TSW-106-08-L-S-RA, Pin Header, 2.54 mm, 1 Rows, 6 Contacts, THT, Right Angle SAMTEC 1 Buy Now
CC0603JRNPO9BN560, SMD MLCC, 56 pF, 50 V, 0603, ± 5%, C0G / NP0 YAGEO 1 Buy Now
MC0603N100J500CT, SMD MLCC, 10 pF, 50 V, 0603, ± 5%, C0G / NP0 MULTICOMP PRO 3 Buy Now
885012206078, SMD MLCC, 150 pF, 50 V, 0603, ± 10%, X7R WURTH ELEKTRONIK 1 Buy Now
MCL053GD, LED, Green, THT, T-1 3/4 (5mm), 20 mA, 2.1 V, 570 nm MULTICOMP PRO 1 Buy Now
MCF 0.25W 330R, THT, 330 ohm, 250 mW, ± 5%, 250 V MULTICOMP PRO 1 Buy Now
MC001795, Breadboard, 830 Tie Points MULTICOMP 1 Buy Now
MC001810, Jumper Wire Kit, Multicolour, 2 mm - 125 mm, 22 AWG, 140 Piece MULTICOMP 1 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
NFC Tag PCB OSHPark 1
MAX31875 Breakout PCB OSHPark 1

Schematics

Schematics is very similar to block diagram. Interconnects are very simple. There are only 3 MCU GPIOs connected. Two for I2C (SDA and SCL) and third for LED. Other pins are used for reset and SWD, but they are not important for the project. At the end of this blog you can download this schematics in PDF format.

image

On breadboard it looks as follows:

image

Custom NFC Tags

In this project I used my self-designed NFC tags. I designed more types of tags. If you are more interested in my tags, you fan find more detailed description in my second project Custom NFC Tags which I did as part of this Project14 contest.

Firmware

Firmware is developed using STM32CubeIDE and it is written in C. I used STM32CubeMX configurator for generating drivers for I2C, GPIO and RTC controllers (I will describe reasons for RTC later). For interfacing MAX31875 temperature sensor it utilizes my own Open-Source library which I published on Github. As part of this project, I ported it to the STM32 platform. For writing NFC tag, I wrote very simple function which can write first 255 bytes of user memory area of the tag. This is sufficient for this project. It is implemented in DynamicTag.c file. Application logic is implemented in ThermometerApp.c file. It integrates error handling and error correction. Application can “survive” errors from both sensor and NFC tag and try to reinitialize it after error occur. Application also checks for CRC errors from temperature sensor (and also properly generates CRC when configuring sensor). You should never face invalid temperature reading. CRC is good capability of MAX31875 temperature sensor.

Tag Memory Lifespan

Application read temperature every 4 seconds, but NFC tag memory lifespan is not infinite. It is about 1 000 000 writes (depends on temperature, million is at 25 °C). When writing new temperature to the tag every 4 seconds it lifespan is limited to about 46 days. For this reason application do it differently. It remember last temperature written to the tag and saves new temperature to the tag only if it changed from previously saved value by at least 0.3 °C and at least 20 seconds (5 measuring cycles) elapsed since previous write. This mean that if temperature do not change rapidly (which is common behaviour of ambient temperature) tag is write-stressed only rarely. Three times per hour or something like this.

Low-Power Operation

I designed application as low power. It incorporates only 3 chips and I deployed the deepest possible stop mode in MCU firmware (there are also modes when MCU memory is not retained, but I did not go sleep so deep). For waking up I use RTC peripheral which is configured to wake up MCU after 4 second elapsed since going sleep.

Because I recently received Nordic Power Profiler Kit, I used it for analysis. I connected PPK 2 to the STM32G031 DISCO:

image

Then I start collecting power consumption traces. Following screenshot from the profiler shows power consumption of the device.

image

On screenshot you can see spikes which occurs every 4 seconds. This make sense because sensor every 4 second wake up and collect temperature measurement form the temperature sensor. You can see that many spikes are very similar but there are 4 (5 if you count the latest spike on the right edge) which are higher. In case of these spikes, device not only collected temperature but also evaluated that it is needed to update output in NFC tag and blink by LED for 50ms. Following screenshot shows spike that occurred when device was issuing I2C transaction to the temperature sensor (and both devices were executing their logic). It is about 3.5 mA spike every 4 seconds. We can also see detail of power consumption which looked like noise on previous screenshot. They are some smaller spikes, but they are irregular. Some of them are missing and frequency is not very fixed. Now I know their source and I will show it later.

image

Following screenshot show detail of larger peak which contains NFC write and LED blink operation. It is easy to understand all parts of this operation. Power consumption is most of the time below 5 mA but it is increased to this level for significantly higher amount of time in comparison with spikes which do not result to NFC write.

As far average (long-term) power consumption of the device is about 85 uA (0.085 mA). This power consumption is good for battery powered device but still can be much better. It is caused mostly by frequent small spikes which was visible on second image (and on first image they were visible as noise). There are three candidates for their source:

  • MCU and especially its LSI oscillator and RTC peripheral which are the only peripherals running.
  • Temperature Sensor and its internal engine/timer for scheduling regular measurements.
  • NFC Tag which is black box. “Nobody” knows what is inside.

I tried to disconnect temperature sensor and spikes did not disappear, so temperature sensor is not their cause. Before disconnecting MCU (which virtually disconnect everything) I tried to disconnect NFC tag and noise disappear. After reconnecting it appears again.

So now I know source of the most power consumption of the device. Next, I checked datasheet how to minimize power consumption of the NFC Tag chip and found reference to Low power down mode. According to the datasheet it reduces power consumption to less than 1 uA. Note that spikes are

about 400 uA. But unluckily this feature is available only on packages with more pins. Frowning2 It is good point to choose right package when choosing dynamic tags for low-power application.

image

But for me this was sufficient outcome from the project. Now I know that power consumption of the MCU and temperature sensor is very low (when sleeping) and NFC tag requires more polishing than I originally expected but it is still good result, I think.

Conclusion

This is all form my project presentation. Thank you for reading this blog post. In this blog post you have seen my project with my custom dynamic NFC tags used for making user interface to the low-power application without and display or connectivity. It was cool project for me because I was using dynamic tags for a first time. I had also opportunity to measure (and analyse) power consumption by Nordic Profiler Kit. If you are interested in making this project yourself, feel free to download attachments below. BOM table with links to components is above in the BOM section.

Resources

  • Schematics (PDF)
  • MAX31875 Breakout Schematics (PDF)
  • MAX31875 Breakout Gerbers (ZIP)
  • MAX31875 Breakout Kicad Project (ZIP)
  • MAX31875 Library (Github)
  • ST25DV64KC Dynamic NFC Tag Schematics (PDF)
  • ST25DV64KC Dynamic NFC Tag Gerbers (ZIP)
  • ST25DV64KC Dynamic NFC Tag Kicad Project (ZIP)
  • STM32G031 Firmware Sources Project (ZIP)
  • STM32G031 Firmware binary (ELF)
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago +3
    Nice project! Incidentally there are NFC ICs that have a 'SRAM pass-through' mode, e.g. NXP ones, which would provide infinite read/write. I know this is an ST-component project, I'm only mentioning…
  • shabaz
    shabaz over 3 years ago in reply to shabaz +1
    (can't edit the typo, replace " IC to me " with " IC to be")
  • misaz
    misaz over 3 years ago in reply to shabaz +1
    ST have similar functionality in tag which I used but it requires issuing special command which standard NFC reader (avalaible on iPhone) do not use. I did not find any way how to map this region to standard…
Parents
  • shabaz
    shabaz over 3 years ago

    Nice project!

    Incidentally there are NFC ICs that have a 'SRAM pass-through' mode, e.g. NXP ones, which would provide infinite read/write. I know this is an ST-component project, I'm only mentioning it because perhaps ST have such a device with that sort of functionality too. I guess ST have really intended this particular IC to me more for EEPROM replacement for small bits of config, in which case it perfectly meets their intended applications I guess. But nice to stretch a device to see what else can be done with it too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 3 years ago in reply to shabaz

    ST have similar functionality in tag which I used but it requires issuing special command which standard NFC reader (avalaible on iPhone) do not use. I did not find any way how to map this region to standard block 0 which readers read. My idea was to rely on standard readers and do not create custom mobile app for reading temperature. With custom app it is of course possible and can be reimplemented to reading temperature measurement right after user request it in mobile application.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 3 years ago in reply to misaz

    The same applies with NXP NTAG's in that SRAM functionality requires use of specific memory blocks and you have to instruct IC to use via special command. As you say, to use would then require a custom app to be developed as standard apps don't work or you would need to us a NFC controller.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to BigG

    Having mucho difficulty using the editor on desktop, nothing appears to work, I dont see the editor toolbar.. Yet I can type on mobile.

    Block 0 contains the capability container so the text or URL content or whatever needs to appear in block 1 I think. But I'm a beginner so I could be very wrong. The NXP chips do support SRAM for block 1 onward, although they call it Mirror and not Passthrough. I thought they called it Pass through but it's not. Anyway, with the mirror mode, it will allow access to SRAM via the NFC interface, without needing any special app, therefore normal Android at least will understand it, no idea about iPhone. No need to write anything via NFC before reading it. 

    I'm looking at a NXP datasheet for NT3H2111, not checked their latest chips. It is table 13 , SRAM_MIRROR_BLOCK and valid value is 0x01 which corresponds to NFC page 0x04 which according to table 4 in section 8.3.1, is in sector 0, it would be block 1 which seems to be the desired block in sector 0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 3 years ago in reply to shabaz

    Thank you for reply. I double checked datasheet of ST25DV64KC-IE6T3 but I did not find any reference to SRAM mirror mode or something like this. The only mentioned passtrough mode is with fast transfer mode (FTM) buffer which need to be read by special instructions on RF side. NT3H2111 looks good. It is also avalaible in TSSOP8 package, but unluckily it is not pin compatible with ST, so I need to make new PCB before playing with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • misaz
    misaz over 3 years ago in reply to shabaz

    Thank you for reply. I double checked datasheet of ST25DV64KC-IE6T3 but I did not find any reference to SRAM mirror mode or something like this. The only mentioned passtrough mode is with fast transfer mode (FTM) buffer which need to be read by special instructions on RF side. NT3H2111 looks good. It is also avalaible in TSSOP8 package, but unluckily it is not pin compatible with ST, so I need to make new PCB before playing with it.