Smart Alarm Clock
  • Challenges & Projects
  • Project14
  • Smart Alarm Clock
  • More
  • Cancel
Smart Alarm Clock
Blog Tempus Fugit... Part 1: 1978 a.d.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Smart Alarm Clock to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 21 Jul 2018 8:08 PM Date Created
  • Views 3233 views
  • Likes 13 likes
  • Comments 7 comments
  • circuit bending
  • micro:bit
  • clock
  • vintage
  • bbc micro:bit
  • advanced micro:bit projects
  • microbit projects
  • smartalarmch
  • microbit
  • advanced_microbit_projects
  • tempus fugit
  • alarm clock
  • smart
  • time
  • remake
Related
Recommended

Tempus Fugit... Part 1: 1978 a.d.

balearicdynamics
balearicdynamics
21 Jul 2018

    • Introduction
    • Time Shift
      • Step 1
      • Step 2
    • Preparing the device
      • The Clock Buttons
      • The Box and the Other Components
    • The Other Parts

And I started late, too late, just posting the the smart clock Project14 monthly theme. Anyway I hope you like this build.

 

Introduction

The idea to make a smart clock was not in my mind until a few weeks ago, when I found an incredible nice alarm clock of the past century. Alex is a digital alarm clock, design dates 1978 and - as far as I saw on the net = not so easy to find, only partially working,

image

This piece of past attracted me immediately; due to the functional problems I had the opportunity to take it for a ridiculous price. The image below shows the first try to power-on (a sort of road test unpacking first images image )

imageimage

imageimage

The clock main board immediately appeared easy to reverse engineer but the enthusiasm vanished in few time. Powering the device the lowest voltage I have detected following the wires connected was 16V. Also the discrete components left few hope to integrate the original circuit with new features.

Not easy to find, I have identified the microcontroller as MM5387AA, a digital clock controller working at 24V. It is a pity as I had to remove the entire board and change the original plan: only the peripheral parts was possible to be reusde in some way. For users interested in aged ICs you can find the MM5387AA datasheet in attach.

Time Shift

The plan required to shift the clock internal hardware by about 40 years:

Step 1

  • Remove the main board and the 7-segments LED display
  • Clean the box
  • Clean from oxides the clock buttons
  • Remove the old degraded wiring and replace with new ones

Step 2

Assemble a new microcontroller board with the following characteristics

  • Real time clock,
  • Control the new hardware with the original buttons
  • Use a similar 7-segments LED display
  • Make better alarms reusing the 8 Ohm speaker
  • Control the environment light reusing the original light resistor
  • Add smart sensors for environmental adata
  • Connect via BLE with external devices, eventually Android smartphone

Preparing the device

The Clock Buttons

The first cleaning operation has been the clock control buttons. The images below shows the buttons cleaning phases.

{gallery} Buttons cleaning

image

The buttons contacts (upper side) and the connector circuit

image

Cleaning the contacts and sanding the circuit

image

The buttons circuit reassembled

image

The new wires connecting the buttons circuit

image

The clock base with the button cleaned

 

The Box and the Other Components

The images below shows the functional test to the light resistor after cleaning the contacts and desoldering from the main board.

imageimage

Then, a deep cleaning of the interior and exterior of the clock container before starting the changes.

imageimageimage

imageimageimage

And now the clean, empty, new device is ready for a complete rebuild...

 

The Other Parts

Tempus Fugit... Part 2: 2018 a.d.

Tempus Fugit... Part 3: micro:bit Interfacing 5V Logic

Tempus Fugit... Part 4: micro:bit 5V SPI

Attachments:
image F511SURWA-S530-A3.pdf
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +5
    Hi Enrico, Excellent project. That clock is in good hands, looking forward to seeing your results!
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to balearicdynamics +5
    I have the same opinion - In my house, I have cassette and record containers from the 70's in Orange. Love the colour.
  • fmilburn
    fmilburn over 8 years ago +4
    Very fun project. I recently bought a multimeter like yours with my winnings from an Element14 contest. Nice that it matches your clock in color
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Enrico,

     

    Excellent project. That clock is in good hands, looking forward to seeing your results!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago

    Hi Enrico,

     

    Excellent project. That clock is in good hands, looking forward to seeing your results!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to shabaz

    Hi Shabaz, In this project I have met some unexpected issues but it seems going ahead almost well. I though I was able to make it fast instead it revealed a challenge image

    Stay in touch I am ... Coming back in time to shorten the delay.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down