Member and Staff Blogs Analog Discovery Teaser
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 13 Dec 2023 7:31 AM Date Created
  • Views 1694 views
  • Likes 15 likes
  • Comments 7 comments
  • dougw
  • Arbitrary waveform generation
  • Digilent Analog Discovery 3
  • road test
  • ad3
Related
Recommended

Analog Discovery Teaser

dougw
dougw
13 Dec 2023

Intro

I was selected to road test a Digilent Analog Discovery 3,  and the kit has arrived. I will post a couple of blogs as I learn a bit about this instrument before diving in to do the actual road test.

The Analog Discovery 3 is a brilliant design that marries analog output channels and analog input channels with some great software to achieve some powerful capabilities. Not only can it perform the functions of many individual instruments, it can integrate these functions into complete synergistic test and measurement systems.

This blog covers a quick unboxing and some cool arbitrary waveform generator work.

Unboxing

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Teaser #1

Here is a teaser image of the 2 channel arbitrary waveform generator feeding the 2 channel oscilloscope of the AD3:

image

The Digilent Waveforms software has some great features - here I have dragged the scope window to a large screen TV.

This device can handle CSV files directly, which makes it easy to generate arbitrary waveforms.

The element14 waveform is inspired by misaz  who has improved his original work here, although I am trying to tweak the concept to get closer to the proper logo colors. I might get even closer in a future episode.

Teaser #2

This image shows an XY plot of e14 on the big screen and the constituent X and Y channels on the little screen. 

image

The X-Y plot clearly shows each point in the arbitrary waveform, which is a little different than a normal X-Y scope, but the big screen combined with the precision of this instrument really show what the signal looks like.

Discussion

The AD3 has an enormous repertoire of functionality and it will take some time to explore its myriad features, but I will post little blogs as I learn interesting applications.

So far I am enjoying the exploration. Not only are there a lot of nifty and useful features, it is actually loads of fun to try and do strange, weird and unusual things that this synergistic combination of hardware and software allow.

I generally don't think of instruments, even good instruments as being fun, but this one qualifies.

Links:

Raster Text on an AD3

AD3 Unboxing

AD3 Enclosure

My Road Test of the Analog Discovery 3

Digilent Analog Discovery 3 road test page

Digilent AD3 page

  • Sign in to reply
Parents
  • Anthocyanina
    Anthocyanina over 2 years ago

    please do waveform update rate tests and noise floor tests if you can. those are things digilent has kind of avoided mentioning by just going around the questions or being vague. especially a comparison of those things against the AD2 would be welcome. thanks! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to Anthocyanina

    My road test blog will be more of a learning journey than a rigorous certified performance characterization, but I can try to see if I can take some meaningful noise measurements.

    Do you have a suggested method to do update rate measurements? It seems like it would be limited by USB bandwidth (which may be a host computer limitation) and sample rate or buffer size, which are adjustable.

    So far, subjectively, I'm not noticing any lags running on a fairly fast MS Surface.

    I do not have an AD2 to compare to...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to dougw

    to test the waveform update rate, you can make the triggers an output, and check the output on a separate oscilloscope. I get a few dozen waveforms per second on the AD2, which is good enough for what the device offers, but it would be nice to know if the AD3 has improved on that. not asking for like a complete characterization or anything like that, just to get an idea of how it performs. all AD3 reviews i've seen online only explore waveforms, but never go into what the actual hardware can do, which would be nice to see.

    thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to dougw

    to test the waveform update rate, you can make the triggers an output, and check the output on a separate oscilloscope. I get a few dozen waveforms per second on the AD2, which is good enough for what the device offers, but it would be nice to know if the AD3 has improved on that. not asking for like a complete characterization or anything like that, just to get an idea of how it performs. all AD3 reviews i've seen online only explore waveforms, but never go into what the actual hardware can do, which would be nice to see.

    thanks!