Member and Staff Blogs Firmware Version Control with GitHub part 1: Branch Strategy for New Features
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 May 2020 10:09 AM Date Created
  • Views 6124 views
  • Likes 11 likes
  • Comments 21 comments
  • tutorial
  • github
  • version_control
  • learning
  • git
  • gitlab
  • github_repository
Related
Recommended

Firmware Version Control with GitHub part 1: Branch Strategy for New Features

Jan Cumps
Jan Cumps
8 May 2020

image

 

A possible strategy for using GIT and working with branches.

In this part 1: working on new developments.

In part 2: bug fixes on the released code

image

I am suggesting a GitHub process, but it translates to other platforms with pull request support, E.g.: Azure DevOps, GitLab, Bitbucket, ...

The examples are using the repository of the eLoad.

I am using a single repository but it works virtually the same if contributors work from their own forked repository.

 

 

Branch Strategy Principles

 

Single Branch

You can work with a single branch. Git always comes with a default master branch.

If all you want to do is have a version controlled repository, you can give commit access to all contributors and that's that.

No need to read any further. You're good image.

 

image

In the images, the vertical lines represent Git branches. The horizontal arrows are actions.

 

Feature Branches

If you want to control what goes into the master (or any meaningful) branch, you can use the feature branch strategy.

In that case, you allow contributors to create their own branches on the fly*2. You don't give them commit access to the master branch.

Feature branches are short-lived by design. They are meant to work on one aspect of the software.

The developer works in that branch and has all the advantages of version control. Changes are tracked, but they stay safely in that feature branch.

It doesn't matter if non-working or partial code is checked in. The "official" code base is not impacted.

 

Once development is deemed finished - you can set rules here if wanted, like all test cases passed, code style checks passed, .... - the developer can create a pull request.

This is where the hosting site matters*1. They support this process to generate the request and get it merged into the official branch.

Once the repository admins accept that pull request, the feature branch is typically deleted because it has lived its life. No need to keep that.

The change will be eternally traceable via the pull request that stays in the repository forever.

 

Branch Policy

The hosting platforms all have some way to set the rules for branches.

You can set who can commit / merge, what type of merges are allowed, who's approval is needed, or no rules at all (typical for feature branches).

If you want your master branch managed, then restrict commit, and set at least one approver.

A pull request creator should not be able to accept their own changes.

This will take care that no one can directly write into the managed branch, and everything can be reviewed and accepted before merging features.

 

image

If you have an unpopular open source project and you're the only contributor, you can still use this approach, but enable "admin override".

In that case you can accept your own pull requests. Not an issue because it's your repository. You're the boss. You do as you please.

 

Project / Development Branch

When you want a stable master branch that represents the official released code, and you have active development going on, then there's the possibility to create long living additional managed branches.

The development branch starts as a clone from the master.

You'd want to set up a policy for such a branch too, similar as the master branch.

Then developers will create feature branches based on that development branch, not the master.

Their process is the same as explained in the Feature Branch section, while they are developing inside that feature branch.

But once done, they create a pull request to the development branch. Not to the master branch.

When the admin approves the request, code is merged into the development / project branch and the feature branch is deleted. Job done.

The repository admin should not accept direct pushes from such a feature branch into master.

 

At release time, the release manager (or you if you are lonely) will create a pull request with the development / project branch changes to the master branch.

Once the repository admin accepts that request, this is the new released version.

 

image

 

You can have several managed development / project branches in a complex project.

Just keep in min that everyone needs to understand what branch is for what, who manages it and where the results should flow to.

My advise is to start simple. And if that simple approach works, don't make it more complex.

Only if you can't manage the contributions in a simple way, then add. See my last line in the Single Branch section for a similar advice.

 

 

In the next part I'll add an approach to allow bug fixes in the master branch. Managed, and with a solution to integrate them in the development branch.

Comments and critiques are very welcome. There are better approaches than mine.

 

 

 

 

*1: or doesn't matter - if you use Git's own mechanism to create patches and mail notifications to request merge.

That approach is not the subject of this post. I want to document the process with pull management.

 

*2: in open source projects, it's common to have everyone run their own fork, instead of allowing the contributors to create branches in your account.

Everything works similar as here. They can create pull requests from such a forked repository into (one of our) branches.

Advantages:

  • you don't have to create and manage users. And several of the suggested repository hosts have a limit on their free tier.
  • The contributor can have their own strategy and approach. You aren't impacted by how they manage the code.
    The only thing you see is a pull request, just like one from a local feature branch.

Some of the hosts have project / issue management to assist the discussion with the contributors.

 

Related Blog
Firmware Version Control with GitHub part 1: Branch Strategy for New Features
Firmware Version Control with GitHub part 2: Branch Strategy for Bug Fixes
Firmware Release with GitHub: Branch, Issue, Pull Request and Project support
Fix a Bug in Production with GitHub: Issue, Branch, Project and (Draft) Pull Request supported + Eclipse Git Plug-in
Break-Fix with GitHub: part two: push bug fixes to the development team
GitHub and GIT: sign your commits with a certificate
GIT course
  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 6 years ago in reply to Jan Cumps +3
    Jan Cumps I'm willing to take your scratch pad notes and drawing and convert them to vector drawings (Inkscape) if you are interested? I have a few cycles now that my RoadTest review The Road to Raspberry…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to colporteur +3
    yes, everything I post on the community is open - feel free to copy or alter. If you're looking for a cleaner drawing, the link I posted in the previous comment has a different and more organised drawing…
  • colporteur
    colporteur over 6 years ago in reply to Jan Cumps +2
    It was a philanthropic offer to lighten a perceived burden. I was thinking that this was part of a larger project for publication within the E14 Community. If you had a need I am willing to create the…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Workshopshed +2
    Yes, you can plug in automated build. Automated test scenario run. Automated review against coding standards. All of these are wins. And the effort to achieve those lowers significantly if you actually…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Workshopshed +2
    My claim to fame is an mid-2000 unit test project for ERP developers - with CVS at the time, but the process was agile - not at all tied to a version control system Downloaded 20.000 times. Used in commercial…
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    For a full-fledged approach: https://nvie.com/posts/a-successful-git-branching-model/
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    What I haven't discussed here is that GitHub also has "SCRUM board" style project support: The task here is attached both to an "issue" that supports this work .... ... and the related pull request(s)…
  • Workshopshed
    Workshopshed over 6 years ago +1
    Interesting to see embedded development using these techniques. I saw a talk from Arm the other week about CI and automated testing which is something you can do once you start using tools like git.
  • yuricts
    yuricts over 6 years ago in reply to colporteur +1
    Personally I prefer using the console commands for git... I do acknowledge that sometimes it is nice to see graphical interfaces with branches and all, but using the command line just gives me a better…
  • shabaz
    shabaz over 6 years ago in reply to colporteur +1
    Hi Sean, I use Visual Code with Git, however I'm conscious that if I move to a different IDE/editor then I'd need to learn the commands! So it's good to know the command-line syntax, but I don't know it…
Parents
  • Workshopshed
    Workshopshed over 6 years ago

    Interesting to see embedded development using these techniques. I saw a talk from Arm the other week about CI and automated testing which is something you can do once you start using tools like git.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Workshopshed

    Yes, you can plug in automated build. Automated test scenario run. Automated review against coding standards.

     

    All of these are wins. And the effort to achieve those lowers significantly if you actually know what's the source code.

     

    You'd be surprised how many people have to ask around for latest version all the time, and get a wrong file. Or several files wrong on several lines...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 6 years ago in reply to Jan Cumps

    >You'd be surprised how many people have to ask around for latest version all the time, and get a wrong file. Or several files wrong on several lines...
    That was one of the key benefits from CI at my last place. Standardised where to get the release sets from. And answering the question of "what's changed" was also another key benifit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuricts
    yuricts over 6 years ago in reply to Workshopshed

    That's exactly why we are teaching our students how to use Git and they have to use it in many projects (C++, C, engineering projects, digital design), with different people in a team. They learn how to setup ssh, solve merge conflicts, use branches, ...

    Some tools (yes, I am looking at you Vivado) are not as easy as others to push your code into git. It is possible using Tcl scripts, but it would be nice to have a better integration in Vivado.

    (We are using Gitlab at the moment, there are scrum tools in there as well, but we prefer openproject for scrum...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yuricts
    yuricts over 6 years ago in reply to Workshopshed

    That's exactly why we are teaching our students how to use Git and they have to use it in many projects (C++, C, engineering projects, digital design), with different people in a team. They learn how to setup ssh, solve merge conflicts, use branches, ...

    Some tools (yes, I am looking at you Vivado) are not as easy as others to push your code into git. It is possible using Tcl scripts, but it would be nice to have a better integration in Vivado.

    (We are using Gitlab at the moment, there are scrum tools in there as well, but we prefer openproject for scrum...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • colporteur
    colporteur over 6 years ago in reply to yuricts

    A programmer friend of mine encouraged me to use Visual Studio code take advantage of Git support. I've started the exercise do you have any insight?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuricts
    yuricts over 6 years ago in reply to colporteur

    Personally I prefer using the console commands for git...

    I do acknowledge that sometimes it is nice to see graphical interfaces with branches and all, but using the command line just gives me a better feeling of control. Call me old school... just my preference.

     

    When I was talking about Vivado integration I am mostly missing a decent .gitignore file... and last time I tried you always had to run a tcl script before pushing and after pulling (ok, you can trigger those...)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to colporteur

    Hi Sean,

     

    I use Visual Code with Git, however I'm conscious that if I move to a different IDE/editor then I'd need to learn the commands! So it's good to know the command-line syntax, but I don't know it, I'd have to learn from the documentation, or, now, Jan's guides.

    But for now, I love Visual Code so I hope to use that for as long as possible. I've ditched almost all other editors that I used to use, like UltraEdit and Notepad++.

    (Of course, I still use vi : ). It doesn't replace everything for me, but it goes a long way.

    The Git support is built-in into Visual Code, so it's a matter of remembering the clone->stage->commit->sync process, which can be done using the Version Control icon (marked with a red arrow in the screenshot below) on the left-side toolbar in Visual Code (i.e. click it to do any git operation, and as you make changes to any file, it will place the files inside the pane next to it, so it's easy to keep track of what's got modified. It's hard to go wrong as a result, but that only gets you the basics, suitable for code where you don't mind making changes on the 'head'. Jan's guides take it to the next level, discussing how to have a feature branch and do a merge. You can do that with Visual Code too, but good to just practice with the basic method first.

    Also, I've never tried integrating with the project 'board' feature that Jan discusses. That's very powerful, I don't have a good workflow for that with Visual Code although it's probably just a matter of trying it out and experimenting.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to shabaz

    Thanks for sharing your insight. I what I call a Frankenstein programmer. I find spinets of code in my travels and stitch them together to make it work. It is not pretty but does work.

     

    I have taken your screen shot and added to my collection of VSC notes I have been accumulating.

     

    My programmer friend (true programmer) introduced me to VSC. I moved away from using the public version of pycharm to tap VSC remote-ssh: connect to host. I have a write-up to establish a VSC environment on a Pi. The setup allows me to use my desktop VCS to remote into the Pi and manage code. It is so much easier to debug and test when the code is being developed right on the device it will be used on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to colporteur

    Interesting, I didn't realise it was available for Pi too, that's awesome.

    I do the same thing too, reuse code snippets to save a lot of time!