Member's Forum Using 12v at base of transistor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 29 replies
  • Answers 10 answers
  • Subscribers 631 subscribers
  • Views 8146 views
  • Users 0 members are here
  • transistor
  • 12v
  • car
Related

Using 12v at base of transistor

ntewinkel
ntewinkel over 10 years ago

Hi all,

 

I'm thinking of using a transistor in a car circuit, to switch a light depending on the state of another light.

 

So it will be 12v as the signal at the base of the transistor.

 

I have a bunch of pn2222a transistors, and I can't figure out from the datasheet what the maximum means for that. It seems to be a reverse maximum (ie, don't let the output be more than 5v over the base voltage).

 

So the question is - is it possible to switch a transistor like that using 12v at the base?

 

Thanks!

-Nico

 

ps, I know I can easily do this using relays, but those take up more space, and I'd prefer to avoid the mechanical bits.

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    0 ntewinkel over 10 years ago

    Dang, I just realized a logic error in my design!! Noooo!!

     

    Consider brakes are on at an intersection, and turning right.

     

    I just tested this on the 4-wire tailer harness in the car.

     

    In that case the left light stays on, and the right light flashes - and by that I mean there's steady 12v on the left wire, with 12v/0v on the right wire.

     

    Using my logic, when both lights are on, the red brake lights will be on (good),

    BUT when the flashing right light is off, the left light will be the only one on, which using my logic, will make it show the left orange arrow...

     

    so then the result looks like "red brake lights" intermittent with "left orange turn light"... giving the impression that we're turning in the opposite direction that we're actually going.

     

    Dang!

    This just got a whole lot more complicated!

     

    Anyone have any brilliant ideas?

     

    Maybe a large capacitor can keep the "signal" high for enough time to allow the other side to flash without switching to the orange arrow. But then the right turn would only flash the red light, not the arrow. Which is no different from how a regular trailer does it.

     

    I could also run an extra line from the car for the brake signal, but that would be non-standard and the trailer would still have to handle the case where some other vehicle is towing it.

     

    I'm wondering if I need to step this up to microcontroller control. The microcontroller can be kept powered on from the trailer battery. But then the failsafe (controller off or dead) needs to still give some sort of proper indications.

     

    For the time being I might just wire up the arrow and the red part together, with the side effect being that the brake signal will include both orange arrows on.

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to ntewinkel

    ps, this is the circuit I had:

    image

     

    And a video showing how all works well until you press the brakes (both switches on) while blinking one side:
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
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to ntewinkel

    Hello Nico,

     

    Here's my scheme:

     

    image

    The relay can be any 12V coil double pole change over (often called DPDT)  you fancy. The coil resistance should be at least 100R if you want to use up your pn2222a transistors.

     

    The relay will only be energised when both turns inputs are high and the brake lights get the power. If only one turn input is high then the turn indicators get power.

     

    With R1 and R2 as shown the turn on threshold for Q1 on the LT input is only about 0.8V, you could reduce R2 to 100R which would set the threshold at 6V or so.

    The transistor only switches the relay coil current and is protected against supply spikes and relay coil inductive spikes by Z1.

    A small capacitor (100nF ceramic) from Q1 base to emitter wouldn't hurt and might reduce sensitivity to electrical noise.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to michaelkellett

    I was just thinking about this some more...

     

    With your circuit locking the brake lights on, I think I can now make the flashers work properly.

     

    The logic is: if the brakes are not on, then light the signal light that is ON. When the brakes ARE on, light the signal light that is OFF.

     

    That would save getting into more complex microchip or PROM or whatnot.

     

    Cheers,

    -Nico

     

    (ps, camping this weekend, so I'll likely be MIA most of the time)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to ntewinkel

    Note to self, because I'll probably need it later...

    Removing 5 second startup delay for Digispark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to michaelkellett

    Hi Michael,

     

    ...up and running in under 1mS quite easily

    That's really good to know.

     

    For the between-blinks power store I was thinking that would be needed for the case where it's just a turn indicator flashing (no brakes). Out of curiosity I might test to see how long one will run on a capacitor.

     

    Do you have  a micro preference

    I do have a micro preference, mostly due to laziness image  Because my stuff is pretty much all hobby I've decided to focus on Arduino and Raspberry Pi - I found that otherwise I end up spending my time learning new tools instead of building projects. I also have TI MSP430, and CCS isn't too bad, but Energia makes using those super simple too.

     

    I'm still at the DIP stage. I have a few surface mount ATTiny13 chips because I needed one for an art project (it's glued to a rock and "wired" with conductive glue).

     

    I haven't created any PCB's yet. A lot of my projects never go beyond breadboard, and the ones that did I've used perf board - a bit messy but worked well enough.

     

    I do have some nice little 3x2x1 inch project boxes that include perf board in it, that I bought from Radio Shack when they were clearing out all that stuff before they became "The Source" here in Canada. One of those might work well for this.

     

    In terms of controllers inventory, I have a couple of DigiSparks (ATTiny85 based) that might work well for this, or maybe one of the TI MSP430 chips because their DIP format would make them easy to add to a board.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to michaelkellett

    Hi Michael,

     

    ...up and running in under 1mS quite easily

    That's really good to know.

     

    For the between-blinks power store I was thinking that would be needed for the case where it's just a turn indicator flashing (no brakes). Out of curiosity I might test to see how long one will run on a capacitor.

     

    Do you have  a micro preference

    I do have a micro preference, mostly due to laziness image  Because my stuff is pretty much all hobby I've decided to focus on Arduino and Raspberry Pi - I found that otherwise I end up spending my time learning new tools instead of building projects. I also have TI MSP430, and CCS isn't too bad, but Energia makes using those super simple too.

     

    I'm still at the DIP stage. I have a few surface mount ATTiny13 chips because I needed one for an art project (it's glued to a rock and "wired" with conductive glue).

     

    I haven't created any PCB's yet. A lot of my projects never go beyond breadboard, and the ones that did I've used perf board - a bit messy but worked well enough.

     

    I do have some nice little 3x2x1 inch project boxes that include perf board in it, that I bought from Radio Shack when they were clearing out all that stuff before they became "The Source" here in Canada. One of those might work well for this.

     

    In terms of controllers inventory, I have a couple of DigiSparks (ATTiny85 based) that might work well for this, or maybe one of the TI MSP430 chips because their DIP format would make them easy to add to a board.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to ntewinkel

    Note to self, because I'll probably need it later...

    Removing 5 second startup delay for Digispark