Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neilk
  • Date Created: 18 Jul 2014 4:06 PM Date Created
  • Views 13672 views
  • Likes 4 likes
  • Comments 53 comments
  • android
  • bluetooth
  • hc06
  • mit
  • arduino_tutorials
  • arduino tutorials
  • appinventor
  • arduino_tutorial
  • arduino tutorial
  • arduino
Related
Recommended

MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display

neilk
neilk
18 Jul 2014

MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display


I found numerous links via Google for this example; unfortunately a lot of them were the same tutorial posted in different places by the same person. None of them included the Arduino sketch! However, the sketch tuned out to be entirely trivial

 

I won't bother giving any of the links, because the the whole thing is unbelievably simple!

 

Here is the Design screen for the App:

 

                                                              image

The screen is very similar to the previous app, except the On and Off buttons are replaced by 2 Labels: Label2 has the default text of "Data from Arduino" and Label3 is given the default text of "0", in Red with a larger font.


As in the previous App, there is a  Bluetooth Client and we also need to add a  Clock component to act as a timer.  These are both non-visible on the display and are shown below the bottom of the Android device screen.

 

In the Blocks screen we retain the 2 Blocks relating to selecting and connecting to Bluetooth and the Block responsible for disconnecting  from Bluetooth. We  dispense with the Button Blocks.


We then add the following new Block to receive and display the data:

image

In the Design screen, I left the default timer interval on the Clock at 1000mS because we want to have time to actually read the Android display.

 

The Arduino Sketch turned out to be very simple:

 

/*   Demonstration sketch to send data to an Android App via Bluetooth - essentially simple; this is just serial output of integer data.

     The Bluetooth module is connected across the Arduino Rx and Tx lines as before.

      A 10k pot is connected across +5v and ground; the slider is connected to analog input 0, to supply varying data.

 

     Neil Kenyon

     15 July 2014

*/

int potPin = 0;                                  // Define the Analog input

void setup()

{

  Serial.begin(9600);

  pinMode(potPin, INPUT);

}

void loop()

{

    int value = analogRead(potPin);    // read the value of the Analog Input

    Serial.println(value);                     // Print the value; can also be seen on Serial Monitor

    delay(1000);                                   // Don't send too fast or the Android buffer will flood - this worked for me

}

 

This seems to work well enough to demonstrate the ease with which we can send data from the Arduino to the Android App.


Edited on 10 August 2015........problems can arise if the Arduino Transmission and Android Receive delay times are set identically. This wasn't a problem for my set up, but seems to be for others. If you leave the Arduino delay at 1000mS, then reduce the clock/timer delay in App Inventor to 950mS, it should be good image



There are two attachments; the second one - Data_from_Arduino_A.zip does some extra error checking which some Android devices seem to need more than others.

Attachments:
Data_from_Arduino.zip
Data_from_Arduino - A.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +2
    Thank you for all your help, I have now (after some playing) successfully able to receive accelerometer data via bluetooth to an android device!!!!! Thanks!
  • e14 Contributor
    e14 Contributor over 11 years ago +2
    I found that the following youtube video was very helpful: https://www.youtube.com/watch?v=DkGGilznfG8
  • e14 Contributor
    e14 Contributor over 11 years ago +2
    Hey everybody... Could You Do Me a Favour? I got problem here when I'm trying to make android app using AppInventor2. I'm going to make android app to showed data "TempValue", "MoistureValue", "ldrvalue…
Parents
  • neilk
    neilk over 11 years ago

    summi Ok what's happening here is that the Android read and the Arduino send are overlapping so that the Android read buffer is corrupted. This happens very very rarely on my Android devices - can't explain why it's so frequent on yours.

     

    The only solution I can think of is to test the data read from Bluetooth and makes sure it's a number. I've had this running for a long time with no problems

     

    Here is the modified code block which does that: I will attach a copy of the modified .aia file to the original post.

    image

    I hope this fixes your problem

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    That sadly didn't fix it, because the sended data's characters are only numbers so nothing happend image. But i fixd the problem I bought a new phone, just kidding image. I modified the arduino's sketch. The sended data is now a string and the sensor's value's are divides withc comma's like thes:

     

    int potPin = 0;    // Define the Analog input

    char data;

    void setup()

    {

      Serial.begin(9600);

      pinMode(potPin, INPUT);

    }

    void loop()

    {

        int value = analogRead(potPin);    // read the value of the Analog Input

        int value2=value/2;

        String data=","+String (value)+ ","+ String (value2)+",";

        Serial.println(data);    // Print the value; can also be seen on Serial Monitor

        delay(1000);                                  // Don't send too fast or the Android buffer will flood - this worked for me

    }

    The first comma is neded just for my phone for others it isn't necessary. And the apk is loks like thes:

    image

    it is necessary to take the timer's Timerinterval lower than the arduino's sending time intervall, becasue thes way there wil be no bufferd two line in the droid's buffer. Thes way you can send multiple data too. I know thes is not the best way to  make the communication but it's working image .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    That sadly didn't fix it, because the sended data's characters are only numbers so nothing happend image. But i fixd the problem I bought a new phone, just kidding image. I modified the arduino's sketch. The sended data is now a string and the sensor's value's are divides withc comma's like thes:

     

    int potPin = 0;    // Define the Analog input

    char data;

    void setup()

    {

      Serial.begin(9600);

      pinMode(potPin, INPUT);

    }

    void loop()

    {

        int value = analogRead(potPin);    // read the value of the Analog Input

        int value2=value/2;

        String data=","+String (value)+ ","+ String (value2)+",";

        Serial.println(data);    // Print the value; can also be seen on Serial Monitor

        delay(1000);                                  // Don't send too fast or the Android buffer will flood - this worked for me

    }

    The first comma is neded just for my phone for others it isn't necessary. And the apk is loks like thes:

    image

    it is necessary to take the timer's Timerinterval lower than the arduino's sending time intervall, becasue thes way there wil be no bufferd two line in the droid's buffer. Thes way you can send multiple data too. I know thes is not the best way to  make the communication but it's working image .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I am experiencing the exact same issues (first number in extra line). Is this really the only way to fix this? Could you please comment your solution? Do i need all thos commas for one value to be transferred? Did it work for you "out of the box" (without the changes above) on other phones?

    So causes the problem? The phone? The arduino code? Is it an App Inventor Bug?

    Thanks a lot!

    (this behaviour really sucks image i am trying to solve this for days now. With the serial terminal the data is shown correctly)

     

    The workaround with the leading comma (String data=","+String (value)) kind of works. But i'm getting the error "The operation <= cannot accept the arguments [,] [50]" The 50 isn't sent anywher from the arduino and isn't shown in the serial terminal app.

    Any ideas on what could be the reason?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    Hi vdp1331

     

    I'm sorry you are having trouble with this image. The thread now has so many strands to it, it can be very difficult to follow even for me!

     

    First of all, my original posting was intended to transmit a single item of data - a number, or a string of text to the Android device.

     

    The solution you have been following,  by Kovacs Lajos, is sending 2 numeric data items as a concatenated text string - in fact sort of .csv data. Why his phone needs the leading comma, I don't know - I get the same error as you if I try his code.

     

    So if you are only wanting to transmit a single data item, my original solution should work, but maybe not out of the box - sorry!

     

    I'm pretty sure that the problem you have is probably caused by the transmit and receive both running at the same nominal delay - ie 1000mS. This results in the Android buffer sometimes containing 2 transmissions from the Arduino.

     

    I get the problem sometimes, but not very often!

     

    However, if you reduce the clock/timer time in the App Inventor from 1000mS to 950mS, while leaving the delay in the Arduino at 1000mS, that should fix it. If not, try reducing it to 900mS.

     

    Hope this helps

     

    Neil