Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Fox Valley Linux User Group: August 2013 meeting

    fustini
    fustini
    I attended a suburban Chicago Linux User Group last weekend for the first time - as it turns out - in my hometown of Batavia where Fermilab is located: Fox Valley Linux User Group - August 2013 meeting:http://www.meetup.com/FoxValleyLUG/events/1...
    • 23 Aug 2013
  • Raspberry Pi server cluster

    e14 Contributor
    e14 Contributor
    I recently built a Raspberry Pi cluster just to see how it's done.  I have no idea how to use a super computer, so I built a web server cluster instead.  I used four Raspberry Pi nodes, and I'm using a PC as a load balancer to distribute HT...
    • 21 Aug 2013
  • About me (If your interested)!!

    dwinhold
    dwinhold
    Let's start with my name is Dale Winhold, I'm 44, started with computers when I was around 8. The Apple was the first one I got to play with at school. My first computer I owned was a TI99-4A with a massive 16K of memory (kind of makes me laugh now)....
    • 16 Aug 2013
  • Exploring FPGAs

    billabott
    billabott
    Thanks to a wonderful fellow engineer, Mr. Shabaz, I now have a KNJN.com Pluto II FPGA board with an Altera Cyclone installed to experiment with.  It seems to offer the same kind of fun exploration and experimentation as many of the microcontrol...
    • 14 Aug 2013
  • Active Sensor/Probe Interface, and USBPSoC

    uplatise
    uplatise
    Purpose of this project is to design a configurable active sensor/probe interface based on 4-pole jack interface featuring all standard digital interfaces, such as UART, I2C, 1-Wire, 2-Wire SPI, IrDA, besides GPIO, high performance analog interface w...
    • 10 Aug 2013
  • Pure Pi Beauty

    billabott
    billabott
    http://www.youtube.com/watch?v=wK7tq7L0N8E
    • 10 Aug 2013
  • MCU-controlled buck regulator

    RWM
    RWM
    If you need some simple regulated power supply, you can build it using MCU and few external components:PWM frequency 250kHz for max. output curent 500mA and supply voltage 12V with 100uH coil. Output voltage regulated from 0.3 to +SUPPLY-0.7V @Io=200...
    • 9 Aug 2013
  • MODBUS master in my cell phone

    gihu
    gihu
    In this post I would like to show the community a project I started last summer: The goal:   Read an 8 analog input MODBUS RTU module with an android phone.   Motivations: Learn about MODBUS.  Build my first android app (afte...
    • 5 Aug 2013
  • Why the Internet Exists

    bluescreen
    bluescreen
    • 5 Aug 2013
  • Digital Logic for the Unenlightened

    billabott
    billabott
    In my Quest for Oneness with the Universe, I recently stumbled upon some very new and very useful resources on the WWW.  They are an Open Source book and a software sim.  The free e-book can be downloaded from http://www.lulu.com/shop/georg...
    • 4 Aug 2013
  • RPi/Z-wave project: Adding in the Pi-Face

    packetgeek
    packetgeek
    Had a little time on my hands today.  Ended up putting the Pi-Face on the second RPi and connecting doorbell buttons to it.  Wrote a C program and two Perl scripts to toggle the office lights when one of the doorbell buttons is pushed.&nbsp...
    • 3 Aug 2013
  • How to Properly Destroy a Hard Drive

    e14 Contributor
    e14 Contributor
    Today’s technological advances are presenting a wide variety of problems that must be solved. From implementing the best software applications to buying the most recent computer hardware, businesses all over the world are constantly making transition...
    • 2 Aug 2013
  • Insight: How Samsung is beating Apple in China

    e14 Contributor
    e14 Contributor
    Source Link GUANGZHOU, China/SEOUL (Reuters) - Apple Chief Executive Tim Cook believes that "over the arc of time" China is a huge opportunity for his path breaking company. But time looks to be on the side of rival Samsung Electronics Co Ltd, w...
    • 29 Jul 2013
  • My PiCam and PiGlasses

    fidelsalinas
    fidelsalinas
    It has been a while since I've had my pi CSI CAM. My original plans are to make somewhat of a baby monitor with the CSI CAM.I started by messing around with python and point reconition so that way I can take a photo of the baby every day in the same ...
    • 27 Jul 2013
  • Adding WiFi to a Raspberry Pi

    e14 Contributor
    e14 Contributor
    Adding a WiFi option to the Raspberry Pi is an easy way to set your raspberry free so you dont have to worry about running network cables when deploying a raspberry pi project. This guide is based of a how-to I wrote for the raspberrypihq.com website...
    • 27 Jul 2013
  • RPi/Z-wave project: Controlling lights with wget

    packetgeek
    packetgeek
    Had a chance to play with the RaZberry yesterday.  In reading about it, noticed that you could control devices via either JSON or simple URLs (via a browser).  Being a total n00b, it took me an hour or so to figure out what was needed to co...
    • 27 Jul 2013
  • RPi/Z-wave project: Lessons Learned #1

    packetgeek
    packetgeek
    I now have a working controller, using the demo software provided with the RaZberry board.   However, I did waste some money and time in learning the following about incompatibilities with the IRIS system. Unusable Hardware - IRIS Smar...
    • 25 Jul 2013
  • RPi/Z-wave project on hold (Update 2)

    packetgeek
    packetgeek
    Project is no longer on hold as I now have a GE Lamp Module, Model ZW3101, which I picked up at Lowes*.  It works with the Razberry demo software with no extra fuss.  More later (another busy week ahead). * Important!!  Lowes appe...
    • 23 Jul 2013
  • RPi/Z-wave project on hold (Update 1)

    packetgeek
    packetgeek
    I received the Razberry daughterboard this week.  Installation is only slightly buggy in that I couldn't use the wget statement in the docs to pipe the download to a shell.  Instead, I had to download the "install" script and run it via:&nb...
    • 21 Jul 2013
  • Review of the XBMC Bundle for Raspberry Pi

    GreenYamo
    GreenYamo
    I recently acquired the XBMC bundle that Farnell have put together for the Raspbery Pi and this is my review of the kit. The package is well presented in a small box (As you can see left) and includes an SD card, HDMI lead, network cable and wha...
    • 21 Jul 2013
  • Giant Robot From Comic Con 2013

    patkelly
    patkelly
    This is just too amazing not to share. www.youtube.com/watch 
    • 19 Jul 2013
  • My blog

    e14 Contributor
    e14 Contributor
    My current blog is not this one it is http://techedison.blogspot.com/I am going to keep this blog updated (hopefully) just in case you do not want to go to my real blog.Here are a few pictures of my blog...
    • 16 Jul 2013
  • Panasonic SP Cap

    jing.liu
    jing.liu
    As leading manufacturer for polymer capacitor technology, Panasonic has developed "SP Cap" since 1984.Its full name is "Conductive Polymer Aluminium Electrolytic Capacitor" or "Specilty Polymer Aluminium Electrolytic Capacitor". However, we usually p...
    • 15 Jul 2013
  • Panasonic A-FR series: Low ESR Aluminum Electrolytic Capacitors (radial lead type)

    jing.liu
    jing.liu
    Low ESR, high ripple current, long lifetime, small case size, AND of course low cost(!)... Very often engineers have to search for "perfect" capacitors solution for their designs.Panasonic has dedicated himself to providing such solution with its THT...
    • 15 Jul 2013
  • Project case construction

    billabott
    billabott
    Having purchased some of these DC POWER JACK 2.1MM ENCLOSED FRAME WITH SWITCH, I began to wonder how am I going to create the proper precise opening to insert and secure it to. Will someone point me in the right direction and the right terminolo...
    • 15 Jul 2013
<>