Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog I Love Wire
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 18 Aug 2017 4:10 AM Date Created
  • Views 1752 views
  • Likes 11 likes
  • Comments 25 comments
  • wire
Related
Recommended

I Love Wire

jw0752
jw0752
18 Aug 2017

Yes I admit it, I confess, I Love Wire!

 

image

 

A while back Alpha Wire announced the release of a new wire called Thermo Thin Hook-up Wire. Here is their announcement on e14 in case you missed it.

 

https://www.element14.com/community/groups/alphawire/blog/2017/06/08/alpha-wire-releases-all-new-600v-thermothin-hook-up-wire

 

The announcement offered a free sample so I signed up. That was June 8th. Today two months later I received 2 FEDEX packages each containing 2 feet of Red Thermo Thin Hook-up Wire. Since I had forgotten about my request it was a really nice surprise. Did I mention that I love wire.

 

image

 

This is 22 gauge Thermo Thin wire and it has 19 strands of 34 gauge wire covered by an ECA flouropolymer insulation that is rated at 600 volts. The insulation is quite flexible and can deal with a temperature range of minus 150 degrees C all the way to +300 degrees C. The excellent qualities of the insulation keep the external diameter of the 22 gauge wire to approximately 1 mm. One of the first things that caught my eye was how tightly the strands were wound. As close as I could figure it out we see a 360 degree twist for every cm. This gives the wire a lot of extra flexibility as the single strands are slightly helical and can flex without being stretched beyond their ability to recover or suffer damage. I have no test equipment capable of testing the claims of the manufacturer but I see no reason to doubt them.

Here is a link to Thermo Thin wire on Newark Electronics:

 

http://www.newark.com/alpha-wire/2922-bk005/hook-up-wire-22awg-black-30-5m/dp/22AC3402

 

I really wish I had a good application for this wire at this time. I can see that it would be a pleasure to work with compared to the stiff Teflon covered wire we used to use on sterilizers and other heat intensive equipment in the dental equipment field.

 

While we are on one of my favorite subjects I want to continue to talk about some of the wire technologies that have a special place in my heart.

 

The next one is the wire that was used in the coil cords of corded telephones. For those of us who spent most of our lives using corded phones it has to be a surprise that with all the use and all the abuse the coiled cords almost never failed. They could be stretched, pulled, swung and pulled between ones toes while simultaneously scratching the back of ones neck and continue to function properly for decades. In case you ever wondered why here is the secret.

 

image

 

Each of the 4 wires of the coiled cord had its own 4 separate conductors. Each of these conductors consisted of a nylon string with a flat ribbon of copper conductor wound around it like a coiled spring. If you look at the picture you can see where I have separated the copper ribbon from the inner nylon string on one conductor. Remember how impressed I was with the tight winding of the Thermo Thin with 1 twist per cm, well the phone wire has upwards of 15 coils per cm. In this configuration the wire is very much like a coiled spring and our bending and twisting has little or no effect on the copper conductor at any point. The internal nylon string takes up all the linear force and leaves the ribbon of copper to do its job of conducting electrons. One of the products that I developed for the dental industry used this technology to solve a problem. In the dental clinics there were wall mounted x-ray units to take radiographs of the patient's teeth. Each of these units had a coiled cord with a thumb switch attached so that the operator could step out of the room, away from the x-ray radiation, and push the button to make the exposure. These cords were very prone to failure and were constantly in need of repair or replacement. My re-purposing of telephone technology brought the telephone cord into the dental operatory to be used as the cord on these x-ray exposure switches. These cords are still being sold to dental equipment repair people across the world.

 

http://www.chapmanhuffman.com/index.php?main_page=product_info&cPath=7&products_id=461

 

Another of my favorite wires are the rubberized (silicone) test probe and patch cord wires made by Pomona. These 18 gauge beauties just call out to me and beg me to make them into test leads and patch cords.

 

image

 

They are composed of many small gauge strands (192 strands of 41ga according to the data sheet) that make them flexible and durable. I have lived long enough to know that the rubberized insulation will eventually ( 40 years or so ) harden and crumble but no one would be disappointed in this kind of a life span and perhaps the new silicone version will last even longer. In case you would like to make some nice cords for your own lab here is the link to the wire on e14 Newark Electronics. The Red is denoted by a -2 and the black by a -0.  Just a side feature, (they smell nice too).

 

http://www.newark.com/pomona/6733-2/test-lead-wire-50ft-18awg-copper/dp/63H2515

 

Another of my pet wires is not to be found easily. I call them High Strand wire and I have only been able to get them by salvaging them out of expensive dental equipment cords. They are used in the cords that go between a table top machines and the handpieces used by the dentist. In some case they supply the 2 or 3 watts of power needed to light a small halogen bulb that lights the inside of the patients mouth. These wires can have up to a hundred or more individual strands of fine gauge wire all in a 20 to 24 overall gauge conductor. They are extremely flexible and durable. I like to use then in any application where I need to handle currents of up to an ampere and where the wire will under go a lot of bending and flexing. I would not use these wires for voltages over 30 or 40 volts as I am quite sure that the insulation is not rated for higher voltages. If you want to get a hold of some of this wire check with your local dentists and ask them to save their old handpiece cords for you or if you have a dental equipment repair man in your area he probably has a pile of them in a corner of his shop.

 

image

 

The last wire that I will cover here is the Kynar wire wrap hookup wire. I was reminded of this wire the other day when I read shabaz 's excellent DIY test instrument project:

 

https://www.element14.com/community/community/project14/diytestequipment/blog/2017/07/14/cyclops-1000-an-electronic-eye-for-rotational-speed-measurement

 

If you look carefully at the first picture in his blog of the perf board prototype you can see how he has skillfully used the Kynar wire as hookup wire. It is very small diameter and can be threaded through the perf board holes to provide beauty and strain relief. The insulation on this wire is a cousin of the insulation on the Thermo Thin and as such is quite high voltage and tolerant of heat, cold and chemicals. Here is a picture of a 30 gauge Kynar wire:

 

image

 

Now that I have introduced you to some of my favorite wires I invite you to send me pictures and stories about your own favorite wire technology. When it comes to wires just remember that I am a little like a cat lady and your favorite might end up being part of my collection too.

 

John

 

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to mcb1 +7
    One of my favorite wires is the very opposite. We used 49 and 50 SWG enameled copper wire to wind microphone coils. The 50SWG is 0.001" diameter and you could break it by heavy breathing (almost ). We…
  • michaelkellett
    michaelkellett over 9 years ago +6
    I can remember using the very flexible telephone style wire (we called them tinsel conductors) - they were a pain to solder and were often finished off at the ends by binding thin copper wire round the…
  • mcb1
    mcb1 over 9 years ago +6
    This was done by machine, not by hand. I can remember doing the odd one when required ... by hand. You are right there was no other way to do it. jw0752 I Love Wire! I've done a quick search and I haven…
Parents
  • the-dubster
    the-dubster over 9 years ago

    mcb1 We used to have GORETm Microwave Cables in the venerable Panavia Tornado ADV (F3 fighter) - it had a frequency range right from DC up to 10's of GHz area (later 'Times' cable then 'GORE-FLIGHTTm ' which actually was better for aircraft installations - the name gave that away . . . ).

     

    One of our 'audiophile' colleagues managed to scrounge some decent lengths of the 'failed on aircraft' cable (frequency dead-spots aren't great in the surface to air missile search/track and fire-control radar frequency areas - not on a Radar Homing Warning System anyway).

     

    He was made up with the stuff - apparently his home HiFi speakers sounded sooooooo much better!

     

     

     

    shabaz and mcb1 that's why I now only ever buy the good jump leads - thin useless ones offer far too much resistance and have prevented me from jump starting a car on several occasions . . . a lesson learned about being cheap (and being stuck with a dead battery too)!!

     

     

     

    jw0752 Can I further get your juices flowing with some rather lovely aviation old fashioned Nyvin or super light PTFE Coated, Kapton (Polyimide insulation) wires? ( +260 deg C / 600V)  PAN6428 or newer (-65 ̊C to 150 ̊C / 600V RMS) JN1007 standard if you ever get bored . . . . .

     

    Ah, the joys of poor wiring husbandry and kapton insulation - carbon arc tracking!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • the-dubster
    the-dubster over 9 years ago

    mcb1 We used to have GORETm Microwave Cables in the venerable Panavia Tornado ADV (F3 fighter) - it had a frequency range right from DC up to 10's of GHz area (later 'Times' cable then 'GORE-FLIGHTTm ' which actually was better for aircraft installations - the name gave that away . . . ).

     

    One of our 'audiophile' colleagues managed to scrounge some decent lengths of the 'failed on aircraft' cable (frequency dead-spots aren't great in the surface to air missile search/track and fire-control radar frequency areas - not on a Radar Homing Warning System anyway).

     

    He was made up with the stuff - apparently his home HiFi speakers sounded sooooooo much better!

     

     

     

    shabaz and mcb1 that's why I now only ever buy the good jump leads - thin useless ones offer far too much resistance and have prevented me from jump starting a car on several occasions . . . a lesson learned about being cheap (and being stuck with a dead battery too)!!

     

     

     

    jw0752 Can I further get your juices flowing with some rather lovely aviation old fashioned Nyvin or super light PTFE Coated, Kapton (Polyimide insulation) wires? ( +260 deg C / 600V)  PAN6428 or newer (-65 ̊C to 150 ̊C / 600V RMS) JN1007 standard if you ever get bored . . . . .

     

    Ah, the joys of poor wiring husbandry and kapton insulation - carbon arc tracking!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 9 years ago in reply to the-dubster

    Hi Andrew,

    Those sound like fascinating specialty wires. I will google them and try to learn more about them tonight. Thanks for the information.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to the-dubster

    apparently his home HiFi speakers sounded sooooooo much better!

    I need to find the cartoon that came out when everyone was pushing 'monster cables' for speakers.

    It consisted of a hose pipe with a t piece and the end above the amplifier.

    The hose was filled with mercury and funnel so you could top it up.

     

    Wish I had scanned it now,

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • the-dubster
    the-dubster over 9 years ago in reply to jw0752

    You're welcome John!

     

    Kapton cable has been the subject of very bad press over the years - it's used in aviation (and the shuttle program) because of the weight saving over alternatives with the same capabilities.

     

    The major issue (one that has been partly addressed with the JN1007 standard) is the polyamide wrap insulation. If it gets moisture ingress it can arc - the arc deposits carbon char - carbon conducts (luckily) and whole sections of wire (or even looms) can pretty much vaporise.

     

    Protection CBs usually trip, but when reset the arc starts again (usually tripping the CB). Unfortunately I have known of (and still hear about) aircraft technicians 'holding in' a tripping CB . . . . . . . . .

     

    You can guess the rest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • the-dubster
    the-dubster over 9 years ago in reply to mcb1

    Whilst I appreciate that twin bell wire with a cross sectional area (CSA) of about 0.8mm is probably a limiting factor for a high-end sound system, I do not subscribe to all of the ridiculous claims of some of the OFC copper / gold plated / Bi-Wiring stuff I've heard of . . . . . . . .