Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Solar Crawlspace Fan Controller - Arduino Day 2021
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 25 Mar 2021 4:10 AM Date Created
  • Views 3617 views
  • Likes 12 likes
  • Comments 11 comments
  • mqtt
  • m5stickc plus
  • vent fan
  • rpi4
  • buck convertor
  • solar powered projects
  • node-red
  • arduino day 2021
  • arduino nano 33 iot
Related
Recommended

Solar Crawlspace Fan Controller - Arduino Day 2021

ralphjy
ralphjy
25 Mar 2021

For my Arduino Day 2021 Project I built a controller for my solar powered crawlspace vent fan.  I provided an overview of the project in a previous post - Arduino Day 2021 Project Intro .

 

The following documents my implementation.

 

Bill of Material:

Product Name

Manufacturer

Quantity

Arduino Nano 33 IoTArduino1
LM2596 Buck Converter Module1
HW-803 5V Relay Module1
BME280 Temperature Sensor Board2
M5StickC PlusM5Stack1
Raspberry Pi 4 2GBRaspberry Pi1
SPDT Slide Switch1
Molex Mini-Fit Jr 2 pin 18-24 AWG Connector PairMolex1
Weatherproof Junction Box 3.9 X 3.9 X 2.8 inchLeMoTech1
Louver Vent Hood 6 inchLambro Industries2

 

Additional Parts:

Product Name

3D Printed Plate
ProtoBoard
Wires

 

Vent Louvers

This is the non-electronic part of the project.  I found a couple of 6" Louver Vent Hoods and built a wooden frame that I attached to the foundation vent using a couple of magnetic cabinet latches.  I thought it would improve the look and it provides some form of passive automatic closure when the fan isn't running.

image

image

 

Proto board assemblies

I printed a mounting plate for the boards that are going into the weatherproof enclosure.  I have them wired up so that I could start software development.  I don't have the 20V power connectors attached yet.  We are having a typical Oregon spring - cold and wet.  I may end up doing my project demo indoors and deploy the circuit when it gets sunnier and drier.  I have a portable 20V power supply that I can use to emulate the solar panel and I've put an LED on the relay output to test the switching of the 20V supply.  For initial programming and testing I'm not using the 20V input (i.e. not using the buck converter, though I've set the 5V output and tested that separately with 20-25V at the input).  I'm also using 5V as "solar voltage" for the A/D measurement.  When I get to final test, I'll use the 20V circuits.

 

The remote sensor that I'm using was built for a different project.  It uses an M5StickC Plus module with the same BME280 sensor that I'm using for the local temperature.  I had posted about my experience with the M5StickC earlier M5StickC Modules .  The Plus module has a larger display and a higher capacity battery.  I will probably switch to using a more power optimized remote sensor later as this sensor will be battery powered and inconveniently located under the house..

 

The modules from top to bottom

  1. M5StickC Plus with BME280
  2. LM2596 Buck Converter
  3. HW-803 5V Opto-isolated Relay
  4. Nano 33 IoT with BME280 on protoboard

image

 

Node-RED MQTT Dashboard

For this project I am using MQTT for monitoring and control, so I decided to use a Node-RED MQTT Dashboard.  I found a very useful set of tutorials by Random Nerd Tutorials for setting up a Mosquito MQTT broker (server) on a Raspberry Pi using Node-RED.  This requires installing 3 components which are covered in the following tutorials:

  1. Node-RED
  2. Node-RED Dashboard
  3. Mosquitto Broker

 

I'm using an RPi4 2GB for the MQTT Server.  I run it headless, 24/7 with UPS backup.

 

The elements that I want to monitor on the dashboard:

  1. Local Temperature (outside crawlspace - local to the controller - this is the outside temperature that I'll use to turn the fan on and off)
  2. Local Humidity
  3. Solar Voltage (the voltage from the solar panel)
  4. Relay State (I am using the normally open contact, so the default state is off - no fan power)
  5. Remote Temperature (temperature inside crawlspace)
  6. Remote Humidity

 

The elements that I want to control from the dashboard:

  1. Set Temperature (the local temperature at which the fan will turn on - defaults to 32 F)
  2. Override Enable (when enabled, the relay will be controlled by Relay Set)
  3. Relay Set (turn relay on/off if Override is enabled)

 

Here is the dashboard I implemented (I'm a Node-Red noob, so I kept it simple):

 

This is the dashboard in reset state (charts are not populated)

image

 

 

The Node-RED flow to implement the MQTT interaction with the dashboard

 

Node-RED Subscribe Flow for data charting

This flow has 4 elements for each sensor data input:

  1. mqtt in - receives data (subscribes to topics) from the Nano 33 IoT
  2. inject - to reset initial state (clear chart data)
  3. debug - provides received data logging for debug
  4. chart - line chart of received data

 

image

Example for Temperature data:

image

Properties:

  1. Server - the Rpi4 is both web host and MQTT server so using localhost on standard port 1883
  2. Topic - this is the subscribed topic that is being published by the Nano 33 IoT
  3. QoS - 2 guarantees that there is only a single response received
  4. Output - autodetect data type
  5. Name - optional, if left blank it will take the topic name

 

image

image

Properties:

  1. Output - this could be the msg payload, the complete message object, or an javascript expression
  2. To - selects where to put the output, defaults to debug window - but I only select when debugging to reduce clutter
  3. Name - optional, if left blank it will take the output name

 

image

image

Properties: most are obvious in context

  1. Group - this selects the particular dashboard and tab to place the chart
  2. Size - you can manually resize if desired
  3. Type - Chart types
    • Line
    • Bar
    • Bar (H)
    • Pie
    • Polar area
    • Radar

 

 

image

image

Properties: Lots of options here.  I use the following:

  1. Blank data array {[]} to clear out the chart data.
  2. Text string to initialize value (e.g. On/Off for switches)
  3. Numerical data to initialize (e.g. 32 for slider)

 

image

 

 

Node-RED Subscribe/Publish Flow for monitor/control

This flow has the additional elements:

  1. mqtt out - publishes topics
  2. switch - to set Override Enable and Relay Set on/off values
  3. slider - sets the control temperature value
  4. text - displays Relay State on dashboard

 

image

Example for Override Enable:

image

 

image

Example for Override Enable:

image

 

image

image

 

image

image

 

image

 

Dashboard Display while running final program

This is still running indoors (not deployed), but using the 20V Portable Power Supply.  The 20V (Solar Voltage) measurement is still somewhat noisy, I'll need to take a look at that.  The Remote Battery reading is high because I'm running on a USB battery bank (LiPo battery is in charge mode).  The Remote is in a colder room in the house (not the crawlspace).  The Relay is on because the temperature is above the Set Temperature.

 

 

image

 

20V Test Setup

image

 

The LED on the terminal block on the right side of the relay module is the proxy for the vent fan (running off the switched 20V with a 1.2K ohm series resistor).

image

 

 

Arduino Control Program

The program startup sequence:

  1. Connect to WiFi
  2. Connect to MQTT Server (RPi4)
  3. Publish
    • Local Temperature
    • Local Humidity
    • Solar Voltage
    • Relay State
  4. Subscribe
    • Set Temperature
    • Override Enable
    • Relay Set

 

Program defaults:

  • Relay State = 0
  • Set Temperature = 32 F
  • Override Enable = 0
  • Relay Set = 0

 

Here is debug serial output of the startup (currently publishes every 10 seconds for debug - probably extend it to 60 seconds when I deploy):

This output was captured prior to switching to the 20V setup (no USB connection for serial output in that case).

image

 

Relay State = 1 because the Temperature is above the Set Temperature (32 F)

Solar Voltage ~4.7V (this is 5V that comes from the USB - it's quite noisy, I'll need to check it at 20V)

 

Change the Set Temperature to 70 F from dashboard

Message is received and Set Temperature is changed

Relay State = 0

image

 

After about 5 more minutes of operation the Temperature rises to above 70 F and Relay State = 1

image

 

Program Code

Crawlspace_Fan_Control.ino

/*
  MQTT Client for Crawlspace Vent Fan


  the arduino_secrets.h file:
  #define SECRET_SSID ""    // network name
  #define SECRET_PASS ""    // network password
  #define SECRET_MQTT_USER "public" // broker username - not used
  #define SECRET_MQTT_PASS "public" // broker password - not used


  created 14 March 2021
  by Ralph Yamamoto
*/
#include <avr/dtostrf.h>
#include <Wire.h>
#include <SPI.h>
#include <Adafruit_Sensor.h>
#include <Adafruit_BME280.h>


#include <WiFiNINA.h>
#include <PubSubClient.h>
#include "arduino_secrets.h"


#define WAIT_SERIAL true //wait for serial to start
#define DEBUG true  //set to true for debug output, false for no debug output
#define DEBUG_SERIAL if(DEBUG)Serial


#define relayPin 2
#define solarvoltagePin A7


#define ADC_AVERAGES 10


Adafruit_BME280 bme; // I2C


float tempBME = 0.0;
float humBME = 0.0;
float voltSolar = 0.0;
float setTemp = 32.0;  //default


uint32_t readAccumulator = 0;
unsigned long delayTime = 1000;


int relayState = 0;
int relayOverride = 0;
int relaySet = 0;


// initialize WiFi connection:
WiFiClient wifi;
//MqttClient mqttClient(wifi);
PubSubClient client(wifi);
long lastMsg = 0;
char msg[50];
int value = 0;


// details for MQTT client:
const char* mqtt_server = "10.0.0.234";


void callback(char* topic, byte* message, unsigned int length) {
  DEBUG_SERIAL.print("Message arrived on topic: ");
  DEBUG_SERIAL.print(topic);
  DEBUG_SERIAL.print(". Message: ");
  String messageTemp;
  
  for (int i = 0; i < length; i++) {
    DEBUG_SERIAL.print((char)message[i]);
    messageTemp += (char)message[i];
  }
  DEBUG_SERIAL.println();


  // If a message is received on the topic crawlspace/override, you check if the message is either "on" or "off". 
  // Changes the output state according to the message
  if (String(topic) == "crawlspace/override") {
    DEBUG_SERIAL.print("Changing override to ");
    if(messageTemp == "on"){
      DEBUG_SERIAL.println("on");
      relayOverride = 1;
    }
    else if(messageTemp == "off"){
      DEBUG_SERIAL.println("off");
      relayOverride = 0;
    }
  }
  // If a message is received on the topic crawlspace/relayset, you check if the message is either "on" or "off". 
  // Changes the output state according to the message
  if (String(topic) == "crawlspace/relayset") {
    DEBUG_SERIAL.print("Changing relayset to ");
    if(messageTemp == "on"){
      DEBUG_SERIAL.println("on");
      relaySet = 1;
    }
    else if(messageTemp == "off"){
      DEBUG_SERIAL.println("off");
      relaySet = 0;
    }
  }  
  // If a message is received on the topic crawlspace/settemperature, you check if the message is either "on" or "off". 
  // Changes the output state according to the message
  if (String(topic) == "crawlspace/settemp") {
    DEBUG_SERIAL.print("Changing Set Temperature to ");
    setTemp = atof(messageTemp.c_str());
    DEBUG_SERIAL.println(setTemp);
  }  
}


void setup() {
  //set relayPin as output
  pinMode(relayPin, OUTPUT);
  digitalWrite(relayPin, LOW);  //set to NC
      
  // initialize serial:
  DEBUG_SERIAL.begin(9600);
  // wait for serial monitor to open:
  if(WAIT_SERIAL)while (!Serial);  // time to get serial running - take out after debug
  DEBUG_SERIAL.println(F("Crawlspace Fan Control test"));


  unsigned status;
    
  // default settings
  // (you can also pass in a Wire library object like &Wire2)
  status = bme.begin(0x76);  
  if (!status) {
      DEBUG_SERIAL.println("Could not find a valid BME280 sensor, check wiring, address, sensor ID!");
      DEBUG_SERIAL.print("SensorID was: 0x"); DEBUG_SERIAL.println(bme.sensorID(),16);
      DEBUG_SERIAL.print("        ID of 0xFF probably means a bad address, a BMP 180 or BMP 085\n");
      DEBUG_SERIAL.print("   ID of 0x56-0x58 represents a BMP 280,\n");
      DEBUG_SERIAL.print("        ID of 0x60 represents a BME 280.\n");
      DEBUG_SERIAL.print("        ID of 0x61 represents a BME 680.\n");
      while (1);
  }


  DEBUG_SERIAL.println();


  // initialize WiFi, if not connected:
  while (WiFi.status() != WL_CONNECTED) {
    DEBUG_SERIAL.print("Connecting to ");
    DEBUG_SERIAL.println("WiFi");   //could print SSID
    WiFi.begin(SECRET_SSID, SECRET_PASS);
    delay(2000);
  }
  // print IP address once connected:
  DEBUG_SERIAL.print("Connected. My IP address: ");
  DEBUG_SERIAL.println(WiFi.localIP());


  // setup the MQTT client:
  client.setServer(mqtt_server, 1883);
  client.setCallback(callback);  


}


void reconnect() {
  // Loop until we're reconnected
  while (!client.connected()) {
    Serial.print("Attempting MQTT connection...");
    // Attempt to connect
    if (client.connect("Nano33IoTClient")) {
      Serial.println("connected");
      // Subscribe
      client.subscribe("crawlspace/override");
      client.subscribe("crawlspace/relayset");
      client.subscribe("crawlspace/settemp");
    } else {
      Serial.print("failed, rc=");
      Serial.print(client.state());
      Serial.println(" try again in 5 seconds");
      // Wait 5 seconds before retrying
      delay(5000);
    }
  }
}


void printValues() {
    DEBUG_SERIAL.print("Temperature = ");
    DEBUG_SERIAL.print(bme.readTemperature()*1.8 + 32);
    DEBUG_SERIAL.println(" *F");


//    DEBUG_SERIAL.print("Pressure = ");
//    DEBUG_SERIAL.print(bme.readPressure() / 100.0F);
//    DEBUG_SERIAL.println(" hPa");


    DEBUG_SERIAL.print("Humidity = ");
    DEBUG_SERIAL.print(bme.readHumidity());
    DEBUG_SERIAL.println(" %");


    DEBUG_SERIAL.print("Solar Voltage = ");
    DEBUG_SERIAL.print(voltSolar);
    DEBUG_SERIAL.println(" V");


    DEBUG_SERIAL.print("Relay State = ");
    DEBUG_SERIAL.println(relayState);


    DEBUG_SERIAL.print("Set Temperature = ");
    DEBUG_SERIAL.println(setTemp);
        
    DEBUG_SERIAL.print("Override Enable = ");
    DEBUG_SERIAL.println(relayOverride);


    DEBUG_SERIAL.print("Relay Set = ");
    DEBUG_SERIAL.println(relaySet);
        
   
    DEBUG_SERIAL.println();
}


void loop() {
  // if not connected to the broker, try to connect:
    if (!client.connected()) {
      reconnect();
    }
    client.loop();
  
    long now = millis();
    if (now - lastMsg > 10000) {
      lastMsg = now;


    // publish temperature
      // Convert the value to a char array
      char tempString[8];  
      tempBME = bme.readTemperature()*1.8 + 32;
      dtostrf(tempBME, 6, 2, tempString);
      // start a new message on the topic:
      client.publish("crawlspace/temperature", tempString);
  
    // publish humidity
      // Convert the value to a char array
      char humString[8];  
      humBME = bme.readHumidity();
      dtostrf(humBME, 6, 2, humString);
      // start a new message on the topic:
      client.publish("crawlspace/humidity", humString);
  
    // publish solar panel voltage
      // Convert the value to a char array
      char voltString[8];  
      readAccumulator = 0;
      for (int i = 0; i < ADC_AVERAGES; ++i)
        readAccumulator += analogRead(solarvoltagePin);  
      voltSolar = (readAccumulator * 3.3 * 10 / 1024) / ADC_AVERAGES;
      dtostrf(voltSolar, 5, 2, voltString);
      // start a new message on the topic:
      client.publish("crawlspace/solarvoltage", voltString);
      
    
    //control relay
      if (relayOverride == 1) {
        if (relaySet == 1) {
          digitalWrite(relayPin, HIGH);
          relayState = 1;
        } else {
          digitalWrite(relayPin, LOW);
          relayState = 0;
        }
      } else {
        if (tempBME > setTemp){
          digitalWrite(relayPin, HIGH);
          relayState = 1;
        }
        else{
          digitalWrite(relayPin, LOW);
          relayState = 0;
        }
      }
      // publish relayState
      if (relayState == 1) {
        client.publish("crawlspace/relaystate", "On");
      }else{
        client.publish("crawlspace/relaystate", "Off");
      }


      // print values
      printValues();
      
    } 


}

 

Demo Video

Demo showing the interaction between the MQTT Dashboard and the Nano 33 IoT.  The operational delay is due to the 10 second update rate.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Summary

Well, that's my Arduino Day Project for 2021.  I made a silly mistake when loading the contacts of the Mini Fit JR connectors (I loaded the wrong sex into the housings - had them reversed).  I'll blame pandemic brain fog which in reality is probably true.  I can't manage to get the contacts extracted, so I'll need to make another set.  So, another reason to wait for it to dry out before I deploy/mount this outside.  I've measured the solar panel and fan setup, so there shouldn't be any issues.  The max voltage that I've measured is about 21.5V and the max current is less than 500mA (surprised me that it was that low, but I can't read the fan label to check the spec).

 

The feature that I would also like to incorporate before deploying is OTA (over the air update).  I've done this with ESP32s and I'm sure there is an equivalent process for WiFi Arduinos.

And there is plenty of space left:

image

  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 4 years ago +3
    I recognize the buck-boost board from some of my own projects. I recently smoked and I mean literally let the smoke of out a Arduino Nano by reversing the 12V power. Your suggestion of pandemic brain fog…
  • neilk
    neilk over 4 years ago +2
    Great project, Ralph. Extremely well documented. Neil
  • ntewinkel
    ntewinkel over 4 years ago +2
    This is a really great project! Thank you for sharing all the how-to details too. I have a few projects that need to do nearly all of what you've just outlined, so your post is surely going to be a helpful…
Parents
  • ntewinkel
    ntewinkel over 4 years ago

    This is a really great project!

     

    Thank you for sharing all the how-to details too.

    I have a few projects that need to do nearly all of what you've just outlined, so your post is surely going to be a helpful guide for me.

     

    ps, I think you gave the answer, but to double check - I thought NodeRed included MQTT, but it looks like you still had to install Mosquito. Does that mean NodeRed doesn't do it, or is Mosquito better?

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 4 years ago

    This is a really great project!

     

    Thank you for sharing all the how-to details too.

    I have a few projects that need to do nearly all of what you've just outlined, so your post is surely going to be a helpful guide for me.

     

    ps, I think you gave the answer, but to double check - I thought NodeRed included MQTT, but it looks like you still had to install Mosquito. Does that mean NodeRed doesn't do it, or is Mosquito better?

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 4 years ago in reply to ntewinkel

    Also general building-science question - did you seal up all the passive crawl space vents as part of this update? if so, how are you handling make-up air supply, or is that just using the usual air leakage?

     

    I'm planning on sealing up all the vents and insulating the crawlspace at the renovation house, which seems to be the new standard for the 2000's. It does also require adding vapour barrier to the entire crawlspace floor of course.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to ntewinkel

    Hi Nico,

     

    Node-RED has the capability to interface with MQTT servers, but does not include one that I am aware of.  Plus, Mosquito does work well. 

     

    Relative to your building-science question, I did not seal up the other vents.  I haven't researched how newer houses are built (mine isn't that old - built in 1995), so I'll probably learn something from you image.  I would probably need to do a lot of rework if I wanted to seal those vents permanently.  I did have a full coverage vapor barrier, but it has perforated in spots due to age.  It would be nice to have vents that automatically opened and closed.  Let me know if you find a good air intake solution and maybe I can give it a try.  I'll probably get someone to replace my vapor barrier after the pandemic calms down.  I'm too old to do that kind of work in a restricted space.

     

    -Ralph 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 4 years ago in reply to ralphjy

    >I haven't researched how newer houses are built (mine isn't that old - built in 1995)

    The renovation house has a new addition built around that time, along with the failure-prone poly-B plumbing pipes, so now I know far more about that crawlspace that I wanted to! image

    It has the same open/closable air vents, with vapour barrier just loosely thrown down.

     

    The house I live in was built in 2001, and has a sealed+insulated crawlspace.

    It's a relatively tall crawlspace at about 6' height, with a basic concrete slab, so we use it for storage, and it allows us to keep the gas hot water tank down there.

    So that's kind of why this part of the renovation update started, having seen how nice it can be!

     

    For humidity control we have a standard bathroom fan with an exit vent.

    I was going to copy that idea for the renovation house.

     

    The thing is that the gas hot water tank adds extra ventilation.

    For building-code, we had to install a fresh air supply vent that has the pipe ending right near the bottom of the HW tank.

    It's a basic B-vent, meaning a basic metal chimney pipe straight up, with kind of a fume-hood style intake a few inches above the tank exhaust. - in other words, not super efficient, but has the side effect of continuously pulling air out through the chimney while fresh air replaces it via the supply pipe at its base.

     

    So... short story already long ;P

     

    I was thinking to add the bathroom exhaust fan in the new addition area, but I'm not sure if I should add a fresh-air intake somewhere on the opposite end of the house.

    Right now there's loads of leakage, but that might change after insulation goes in.

     

    ps, the quick bit of research I did online showed humidity levels actually improve when the crawl vents are sealed up and mechanical ventilation is added. So I think we're on the right track.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to ntewinkel

    Sounds like you have better situation than I have.  My house has what is a "standard" raised foundation in this area.  There is no concrete slab, just a perimeter concrete foundation to support the outer walls and individual concrete footings to support the interior posts.  I have a dirt surface under my vapor barrier and a clearance of only 3'-4'.  That's one reason that I wanted continuous ventilation except when it's too cold.  We don't have that much of an issue with outside humidity in the summer.  I had thought about getting my air intake from the garage, but unfortunately it is on the same side of the house as the vent fan and I wouldn't get cross ventilation.

     

    I have the same type of passive gas water heater vertical vent that you described, but my water heater is in the garage,