Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino connection help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 38 replies
  • Answers 11 answers
  • Subscribers 420 subscribers
  • Views 4491 views
  • Users 0 members are here
Related

Arduino connection help

alexparker2002
alexparker2002 over 9 years ago

I have made an integrated arduino monitoring system with 3 sensors....

I have used leds to show their values

But i want to add a lcd to it and an ethernet shield to it..... Is it possible?

Let me tell you that I am a beginner.....

Ive attached the schematics please modify it and tell me...... Please!!!!!!

Attachments:
imageFA5RM0AHX1W2JT3.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2 suggested
    You should be able to do it but You will need to use a WS5100 type ethernet shield as it will offload some of the software to the hardware. It will plug into the Arduino UNO, it uses pins 10,11,12,13 you…
  • beacon_dave
    beacon_dave over 9 years ago in reply to beacon_dave +2 suggested
    Also perhaps be aware that the power rails on some breadboards are not continuous but instead are interrupted half way along. You may find that you need to place a jumper on your ground rail between block…
  • mcb1
    mcb1 over 9 years ago in reply to alexparker2002 +2 suggested
    alexparker2002 Part of learning is the LEARNING part. Having someone do all the work for you is not learning, but copying . I suggest you explore the examples that are provided in the Arduino IDE. There…
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to dwinhold

    Can I use sensor shield to connect the sensors and lcd to arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    Depends on a number of things such as the type of sensor shield, the type of sensors, the type of LCD etc.

    Perhaps if you can provide some information / links to the devices you are looking at ?

     

    Have you considered the likes of the Grove Starter Kit for Arduino ?

    https://www.seeedstudio.com/Grove-Starter-Kit-for-Arduino-p-1855.html

    Grove - Starter Kit v3 - Seeed Wiki

     

    It provides a base shield with connectors which makes it very easy for beginners to connect devices to.

    It comes with a 2-line LCD display

    Grove - LCD RGB Backlight - Seeed Wiki

    a LED module

    Grove - LED Socket Kit - Seeed Wiki

    a light sensor

    Grove - Light Sensor - Seeed Wiki

    and a temperature sensor module

    Grove - Temperature Sensor - Seeed Wiki

     

    You could then add a moisture sensor

    Grove - Moisture Sensor - Seeed Wiki

    and two more LED modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Sensor Shield V5.0 sensor expansion board for arduino: Amazon.in: Electronics

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Plz visit this link to view the sensor shield

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    And instead of ethernet shield I've decided to use a wifi module....  will it be easier?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    The Sensor Shield you are looking at basically passively re-maps the Arduino IO pins to a variety of connectors and provides a bit of power distribution.

     

    So any sensors / displays that you can connect directly to the Arduino IO pins should also be able to be connected via the Sensor Shield.

     

    Note that a number of IO pins are shared between a number of connectors on the Sensor Shield. It is not giving you more IO, just more convenience.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Is it suitable for my project?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Will i be able to use all the sensors and display with it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    Why do you think that it might be ?

     

    What functionality do you think it will bring to your project as opposed to using the Arduino without it ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    You've not said what display you intend to use yet. Displays have different types interfaces which they use to connect to the host microcontroller.

     

    The Sensor Shield you have chosen looks like it is designed to work with the common 12864 type LCD display either with a 14pin or a 6pin IDC type connector. If your display doesn't already have that connection then you will have to make a cable just as you would if connecting directly to an Arduino.

     

    As has been mentioned  previously, you need to keep track of which IO pins on the microcontroller you are intending on using for each device. If you look closely, in parallel mode the 12864 LCD display consumes most of your digital IO pins (D2-D13). In serial mode it only consumes three (D2-D4). Alternatively you could use a I2C type display which will consume two of your analogue IO pins (A4-A5) 

     

    The photo resistor, soil probe and temperature sensor should work equally well with or without that shield. They just require to be connected to 3 of the 6 analogue input pins on the Arduino.

     

    As you have some resistors and LEDs to incorporate then you may find that a prototyping shield would be a better investment than that sensor shield but I suspect that you don't have experience in soldering electronic circuits ? If that is the case then the Grove shield I mentioned earlier would likely be a better choice as it all just plugs together.

     

    However you appear to be getting a bit ahead of yourself. Judging by your questions so far you would be better off starting with trying to get the core of this project working on a simulator like http://circuits.io first, then once you have the LED's, sensors, and LCD display working there, then you can move onto physical components and breadboard, before moving onto tackling the Ethernet networking before finally considering how you are going to build the project in its final form. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<>