Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Troubleshooting why Arduino logical operators doesn't compute
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 414 subscribers
  • Views 8958 views
  • Users 0 members are here
Related

Troubleshooting why Arduino logical operators doesn't compute

colporteur
colporteur over 4 years ago

image

How would you write the expression to test sensors Departure (A or B) HIGH AND Arrival (A or B) HIGH?

The first else if statement shown below doesn't work. Departure A OR Departure B HIgh AND Arrival A OR Arrival B High. The OR doesn't work. Only when both Departure A AND B are HIGH the serial print. The same applies to the third else if statement both Departure A and B have to be low for the statement to function. What am I coding wrong for the OR?

      if ((digitalRead(s1DeparturePinA) == LOW || digitalRead(s1DeparturePinB) == LOW) &&
          (digitalRead(s1ArrivalPinA) == HIGH || digitalRead(s1ArrivalPinB) == HIGH))
        {
         Serial.println(F("Train on siding 1 status DEPARTURE")); 
         delay(1);
        }
      else if ((digitalRead(s1DeparturePinA) == HIGH || digitalRead(s1DeparturePinB) == HIGH)&&
               (digitalRead(s1ArrivalPinA) == HIGH || digitalRead(s1ArrivalPinB) == HIGH))
        {
          Serial.println(F("Train on siding 1 status IN TRANSIT"));
          delay(1);
        }
      else if ((digitalRead(s1DeparturePinA) == HIGH || digitalRead(s1DeparturePinB) == HIGH) &&
               (digitalRead(s1ArrivalPinA) == LOW || digitalRead(s1ArrivalPinB) == LOW))
        {
          Serial.println(F("Train on siding 1 status ARRIVAL"));
          delay(1);
          s1ArrivalDetect = LOW;
        }
      else if ((digitalRead(s1DeparturePinA) == LOW || digitalRead(s1DeparturePinB) == LOW) && 
               (digitalRead(s1ArrivalPinA) == LOW || digitalRead(s1ArrivalPinB) == LOW) &&
                s1ArrivalDetect == LOW)
        {
          Serial.println(F("Train on siding 1 status STOP"));
          delay(1);       
        trainOneOut = LOW; //train selection flip_flop L=train on siding 2
        s1ArrivalDetect = HIGH;
        digitalWrite(l1_TurnoutL, LOW);  //unset departure and arrival turnouts for train1
        digitalWrite(s1_Power, LOW);        //unset power on for train1
        digitalWrite(l1_TurnoutR, HIGH);  //set departure and arrival turnouts for train2
        digitalWrite(s2_Power, HIGH);        //set power on for train2
        }

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +5
    I would use some kind of linear encoder. If in your case you only have to detect the arrival and departure always in the same direction, the logic is reduced to detecting the rising edge of one sensor…
  • Jan Cumps
    Jan Cumps over 4 years ago +4
    First assign each pin's status to a variable' then print that variable to the serial monitor. You can then see if it's related to your logic, or to a pin not being correctly read. Added bonus: if you…
  • javagoza
    javagoza over 4 years ago in reply to colporteur +3
    For example In setup set the two ISRs // detect rising edge for switch A attachInterrupt(digitalPinToInterrupt(s1ArrivalPinA), isrArrivalSwitchRising, RISING); // detect falling edge for departure…
  • Jan Cumps
    Jan Cumps over 4 years ago

    First assign each pin's status to a variable' then print that variable to the serial monitor.

    You can then see if it's related to your logic, or to a pin not being correctly read.

    Added bonus: if you then use those variables in your comparisons, yoy have less gpio function calls.

    Added bonus 2: consistent state throughout the evaluation. In your code, there is no guarantee that these pins have the same status during the logic's execution.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to Jan Cumps

    Bare with me while I carve out an understanding.

    Before the first if statement, read the pins and assign the status to a variable. Then all the conditional statements are evaluated against those recorded states. The states are read each time through the loop.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to colporteur

    Yes. And if you want to test the logic, I'd first manually assign TRUE or FALSE to the variables, instead of reading pins. And see if the code does what you expect.

    If it does, then assign the variables from pin state, and try again.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... also, if your input changes are caused by a mechanical event (switch, optocoupler detecting movement, magnetic sensor) , you may need to debounce/clean the input signals.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 4 years ago

    I would use some kind of linear encoder. If in your case you only have to detect the arrival and departure always in the same direction, the logic is reduced to detecting the rising edge of one sensor and the falling edge of the other.

    You can use interrupt service routines to detect both the rising edge transition and the falling edge transition.

    image


    dougw has a good project on the subject.

    dougw
    The Logical Project
    Intro I always had a lot of fun designing digital circuits that used Boolean logic, but these days it is rare to see designs with lots of discrete gates. With this little project I'm going to have some…
    By dougw over 5 years ago in Digital Fever > Blog
    14 comments


    I based on the same for this project that you see in the video. In this case I needed to detect the direction of movement, it's a different case but it uses the same quadrature encoder principle using a DIY magnetic linear encoder with two magnetic reed switches and a magnet.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    In this blog you can get the complete source code for this solution.

    javagoza
    VenTTracker #06 -  Window Sensor Prototype
    One of the main components of our ventilation routine monitoring project is the sensor for the status of doors, windows and blinds. During this week we have given a boost to the creation of that sensor…
    By javagoza over 5 years ago in Design For A Cause 2021 > Blog
    2 comments

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to javagoza

    I like the debounce idea for use on reading the sensors. I reviewed your application and got lost. Not a programmer. I then went in search of simplified code examples. I'm thinking of trying to assemble code for a test first to see if I can get a working model. I need some of that anti-aging formula to grasp this stuff:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 4 years ago in reply to colporteur

    For example 

    In setup set the two ISRs

    // detect rising edge for switch A
    attachInterrupt(digitalPinToInterrupt(s1ArrivalPinA), isrArrivalSwitchRising, RISING);
    
    // detect falling edge for departure
    attachInterrupt(digitalPinToInterrupt(s1DeparturePinB), isrDepartureSwitchFalling, FALLING);

    Then define the two ISR, two functions

    void isrArrivalSwitchRising() {
       state = TRAIN_ARRIVED 
    }
    
    void isrDepartureSwitchFalling() {
       state = TRAIN_DEPARTED 
    }

    and in your loop method check for state changes

    if (state==TRAIN_ARRIVED) {
       state == TRAIN_PARKED;
       doMyArrivingStuff();
    }
    
    if(state==TRAIN_DEPARTED) {
       state == TRAIN_RUNNING;
       doMyDepartureStuff();
    }

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago

    If you remove the else clause and run your code as 4 separate if statements you will see their are input cases that overlap. The only way for the first if statement to fail is for both departure inputs to be high.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to javagoza

    Did you hear that? That was my head hitting the desk:) I'm envious of the knowledge, yet my age creates limits on what I can use or retain.

    attachInterrupt(digitalPinToInterrupt(s1ArrivalPinA), isrArrivalSwitchRising, RISING);

    This call, if the sensor input s1ArrivalPinA is RISING (i.e. HIGH) run the isr routine? I will get this a little bits at a time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to scottiebabe

    HUmmm...I don't see that. Will look again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>