Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Unable to capture video data with Vivado20.1 bit file with FMC MULTI-CAM4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 367 subscribers
  • Views 1179 views
  • Users 0 members are here
  • zcu102
  • multi-camera_fmc
  • aes-fmc-multicam4-g
  • zedboardcmty
Related

Unable to capture video data with Vivado20.1 bit file with FMC MULTI-CAM4

saipradeep523
saipradeep523 over 4 years ago

I have ported the reference design to Vivado 20.1 and generated the bit file. But i have not updated any drivers on kernel. I am  Unable to get  the data with Vivado version 20.1 generated bit file.

If i change the bit file from 20.1 to 18.3 version data is captured. But I ported 18.3 project to 19.1 and 19.2 Vivado version , these bit files are working fine. Only problem with 20.1 Vivado version bit file only.

 

Here I found  up to 19.2 vivado version support only https://xterra2.avnet.com/xilinx/vitis_embedded_platform_source/zcu102/zcu102_mc4 

Is there updated BSP available with AVNET for Vivado 20.1 version or PetaLinux 20.1?

  • Sign in to reply
  • Cancel

Top Replies

  • saipradeep523
    saipradeep523 over 4 years ago in reply to drozwood90 +1
    Thanks Daniel, The QuadCam + VCU link is helpful. Thank you very much for your help.
Parents
  • drozwood90
    0 drozwood90 over 4 years ago

    Hi there,

     

    All of our BSPs are located at the

    http://avnet.me/ZedSupport

    URL.  There you will see the supported stock BSPs for 2019.2, 2020.1 and the start of 2020.2.  Please know that 2020.2 is not released at this time.

    3683.contentimage_207733.png

    You will also find other supported reference files (for AI and Vitis HLS).

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • saipradeep523
    0 saipradeep523 over 4 years ago in reply to drozwood90

    Thanks Daniel for the reply. I have downloaded  2020.1 version and verified in it. FMC-MULTI-CAM4 related BSP for ZCU102 or ZCU104 or any other board is not found.

     

    Can you provide the BSP for FMC-MULTI-CAM4 for any board? if you have ZCU102 it is useful for me.

     

    FMC-MULTI-CAM4  2018.3 Avnet provided Linux drivers are compatible with 4.14 kernel (May be compatible 4.xx kernel version) but Vivado 20.1 (or PetaLinux 20.1) uses 5.4 kernel version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • saipradeep523
    0 saipradeep523 over 4 years ago in reply to drozwood90

    Thanks Daniel for the reply. I have downloaded  2020.1 version and verified in it. FMC-MULTI-CAM4 related BSP for ZCU102 or ZCU104 or any other board is not found.

     

    Can you provide the BSP for FMC-MULTI-CAM4 for any board? if you have ZCU102 it is useful for me.

     

    FMC-MULTI-CAM4  2018.3 Avnet provided Linux drivers are compatible with 4.14 kernel (May be compatible 4.xx kernel version) but Vivado 20.1 (or PetaLinux 20.1) uses 5.4 kernel version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • drozwood90
    0 drozwood90 over 4 years ago in reply to saipradeep523

    Hi there,

     

    I am sorry I misunderstood.  I thought you were porting the design around from something else and needed the base BSP.

    You keep mentioning the ZCU102/ZCU104. I do not support those.  If you need support for those, you need to try over at the Xilinx forums.

    The design you have there was a one off.

     

    The Quadcam is being brought into the normal flow for our Designed By Avnet boards.  It has already been ported to the UltraZed-EV.

    This will be for the 2020.2 release.  We did not have a 2020.1 release of the Quadcam as far as I am aware.

     

    If you would like to build the BSP yourself, our 2020.2 is not stable at this time, but might help you in your efforts.

     

    **Clone our 3 related repos, checkout 2020.2 branch, then in the scripts folder, you will see make_uz7ev_evcc_quadcam_h.sh **

     

    Run that and you should get a BSP out that will run on an UltraZed-EV.  Note that you will need an HDMI license.  You can get one of those by contacting your local FAE.  I am not sure if you can self-serve a demo, but you can check under xilinx.com/getlicense to see if there is a self-serve option for the HDMI license.  I can't check for you as I have a different type of account and have access to different licenses than you will.

     

    If you have never worked with our repos, you can take a look at this blog, while old, should still be able to help you through - coupled with the notes I added above.

    Using Avnet Build Scripts to Build a PetaLinux BSP (2019.2 and earlier)

     

    --Dan