Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere Contest Server -> Wi-Fi not configured
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 12 answers
  • Subscribers 55 subscribers
  • Views 1521 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Azure Sphere Contest Server -> Wi-Fi not configured

wizardatlarge
wizardatlarge over 7 years ago

Trying to do the daily "Azure Sphere Starter Kit Sync with Contest Server" thingie

  • When I click on "Read Device", Device IP is "Wi-Fi not configured"
    • ==> the response:
      • "Device ID" is valid
      • "Device MAC" is valid
      • "Device IP" Wi-Fi not configured
  • If I enter the following at the command prompt:
    • azsphere device wifi show-status
    • ==> the response:
SSID(for my eyes only)
Configuration stateenabled
Connection state: connected
Security state  : psk
Frequency       : 2437
Mode            : station
Key management  : WPA2-PSK
WPA State       : COMPLETED
IP Address      : 192.168.1.111
MAC Address     (for my eyese only)

 

 

Because "Wi-Fi not configured", when I tap the "Send to Server" button, an error message pops up with "deviceIP":"Wi-Fi not configured","error":"0"

 

So, what is going on with the app? The app is not seeing that the device is provisioned on the network and thus not allowing me to log-in for that daily clicks.

 

How am I supposed to log 15 days if the app is not working like it is supoosed to?

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 7 years ago +4 suggested
    As Clem stated, reconnecting to the wifi can sometimes take a bit of time. I use a PAUSE statement instead. Edit the sk_check.bat. ... azsphere device restart echo. PAUSE <--- add this or put the delay…
  • clem57
    clem57 over 7 years ago +3 suggested
    What happens if you eject USB and re-plug it back in? For me the WiFi reconnected. Also I modified the bat file to put in a 5 second Pause command. Seems like scanning the WiFi in my neighbourhood takes…
  • evanroode
    evanroode over 7 years ago +3 suggested
    I'm getting that popup and no wifi listed as well, but I'm getting counts anyway.
Parents
  • jabourke
    0 jabourke over 7 years ago

    I was having the same issue; I edited the sk_check.bat to add the timeout that's been suggested and that resolved the WiFi issue for check-in, but after sending my info to the server I'm still showing the same count.

     

    ...is there a delay on the count...?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sanyaade
    0 sanyaade over 7 years ago in reply to jabourke

    I have same issue getting reply from Azure cloud server.

    I am not getting server confirmation for today having ping the azure server several times today. This is unusual.  It looks like the Azure Cloud is down. I hope not being affected by hurricane Dorian

     

    Anyone having same issue?

     

    God blesses!!!

     

    Best regards,
    Sanyaade

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • danzima
    0 danzima over 7 years ago in reply to sanyaade

    peterfenn

    Hi Peter, can you see the above comments?


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 7 years ago in reply to sanyaade

    You are right!  I didn't get the email.  However, the Server appears to be receiving because it counted my login from earlier this morning.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jabourke
    0 jabourke over 7 years ago in reply to sanyaade

    I've noticed a slight delay on the count incrementing after sending to server - a few minutes. Nothing long, just a long enough pause to get me wondering if something was amiss in spite of the confirmation pop-up.

     

    And then the updated count shows up.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jabourke
    0 jabourke over 7 years ago in reply to sanyaade

    I've noticed a slight delay on the count incrementing after sending to server - a few minutes. Nothing long, just a long enough pause to get me wondering if something was amiss in spite of the confirmation pop-up.

     

    And then the updated count shows up.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer