Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Pinmux - enabling SPI
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 58 subscribers
  • Views 7533 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • bb_black
  • beagle_bone_black
Related

Pinmux - enabling SPI

e14 Contributor
e14 Contributor over 13 years ago

As the Black has a new 3.8.x generation kernel, omap_mux has gone and we're in the realms of using pinctrl for setting up the pins on the expansion headers.

 

Looking through the bonescript library it appears to try omap_mux and if that fails it just reverts to treating the pin as a gpio. That's all very well until you want to enable a PWM, UART, SPI etc.

 

So does anyone know what magic is needed on the black ?   I'm suffering here from plenty of information on enabling SPI on the original beaglebone with a 3.2.x kernel, but basically zero info on the current state for the Black.

 

/proc/config.gz says CONFIG_SPI_OMAP24XX=y and I've loaded spi-dev, still no /dev entries for spi and the pinmux settings look wrong.  I'm missing something or doing something wrong I'm sure, but right now it seems as if going through /dev/mem, behind pinctrl's back, might be the only way ?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I have been playing with dtbo to enable spi0 on the BeagleBone Black. You can read about it on inbedded.net . Hope that will help, Christophe
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    Hi Christophe, and welcome to Element 14's BBB community! That's a nice set of BBB articles at your site. My discarded Nokia Communicator 9210 has been looking at me with some anxiety since I began reading…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    There's a newly posted pinmux table here:

    https://docs.google.com/spreadsheet/ccc?key=0AmI_ryMKXUGJdDQ3LXB4X3VBWlpxQTFWbGh6RGJHUEE#gid=0

     

    referenced here:

    http://www.element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/07/17/hackerspace-challenge--leeds-only-pru-can-make-the-leds-bright

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Nice of them to hide it behind something that requires a login before you can view it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    We need a notes column too, which can indicate where that pin is being used on the board today, e.g. some are being used for MMC, so we can discount using them, etc.

    Today, I use three references to decide how to use a pin: (1) Schematic to double-check the pin is available, (2) your table which is similar to this one, and (3) I used to use the "Pin Mux Utility" from TI, but now there is the http://pinmux.tking.org/ site, which is basically just some html+javascript, but seems bug-free now, and tells the value to put in the dts fragment file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    I'll happily take pull requests to add or update things on my table.  After all, it's not useful if it doesn't have the particular piece of info you need.

    That's why it's publicly available on github and anyone can access it (without a login), fork it, use it as a starting point for something better or whatever they want.

     

    The ods file I have on github should have the pins used by eMMC and HDMI marked, but I noticed that I've missed either the i2c or spi pins used for audio with hdmi.

     

    I also noticed that there's several of these tables popping up, so I'm quite happy if someone else comes up with a better one.  I'll happily make mine disappear image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I'll happily make mine disappear image

    Don't do that.  Monocultures are bad, biodiversity is good. image

     

    It's not really a joke.  Open source shares quite a few properties with biological systems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Yes,

     

    Please don't, I still use it :-) Currently I trust this version, it has not let me down! (I don't go to the github, but I have the URL bookmarked to the table (in reply 5) that was inserted in the discusion and I just search in there using Ctrl-F - nice and simple!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<