Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum SBC CPU Throughput
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 88 replies
  • Subscribers 63 subscribers
  • Views 11297 views
  • Users 0 members are here
  • cubieboard
  • olinuxino
  • sabrelite
  • bbb
  • BeagleBone
  • rpi
Related

SBC CPU Throughput

morgaine
morgaine over 13 years ago

I notice that people are doing some initial benchmarking of BBB and other boards on the RPF forum.  Results roughly as expected I guess:

 

Using just a simple

 

time echo "scale=2000;4*a(1)" | bc -l

 

as a lightweight benchmark, I see these numbers reported (smaller Time is better):

 

[table now updated with extra datapoints reported in current thread below]

 

Submitter
Time (s)
Board
SoC
Clock (MHz)
O/S
shuckle26.488Raspberry Pi BBCM2835700Raspbian 3.1.9
morgaine25.719Raspberry Pi BBCM2835700Raspbian 3.1.9+ #272
shuckle25.009Raspberry Pi BBCM2835700Raspbian 3.2.27
trn24.280Raspberry Pi BBCM2835700Raspbian ?
morgaine22.456Raspberry Pi BBCM2835800Raspbian 3.1.9+ #272
morgaine21.256Raspberry Pi BBCM2835800Raspbian 3.6.11+ #545, new firmware only
selsinork21.0MinnowboardAtom E640T1000Angstrom minnow-2013.07.10.img
shuckle17.0Raspberry Pi BBCM28351000Raspbian ?
morgaine16.153BB (white)AM3359720Angstrom v2012.01-core 3.2.5+, user-gov
selsinork15.850A20-OLinuXino-MICROA20912Debian 7.0, 3.4.67+
selsinork15.328CubieboardA20912Ubuntu/Debian 7.1
pluggy14.510BBBAM33591000Debian
morgaine14.153BBBAM33591000Debian 7.0, 3.8.13-bone20, perf-gov
selsinork13.927A10-OLinuXino-LIMEA101000Debian 7.0, 3.4.67+
Heydt13.159CubieboardA101000?
selsinork12.8Sabre-litei.MX61000Debian armhf
selsinork12.752CubieboardA20912Ubuntu/Debian 7.1 + Angstrom bc
selsinork12.090BBBAM33591000Angstrom dmnd-gov
pluggy11.923BBBAM33591000Angstrom
selsinork11.86BBBAM33591000Angstrom perf-gov
selsinork9.7Sabre-litei.MX61000Debian armhf + Angstrom bc
selsinork9.606Sabre-litei.MX61000LFS 3.12, gcc-4.8.2, glibc-2.18

 

 

As usual, take benchmarks with a truckload of salt, and evaluate with a suitable mixture of suspicion, snoring, and mirth. Use the numbers wisely, and don't draw inappropriate conclusions. image

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +2
    floating point doesn't get you 2000 digits.
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    Data is always good, and sharing it is also good. The warnings are to help people avoid unwarranted conclusions. And when used properly, synthetic and other artificial benchmarks can be very valuable,…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +1
    > and don't understand why you think it is a good idea to keep it in the loop so you can benchmark it. Come on. It's not that complicated. Johnny wanted to know how fast his new computer was. He decided…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Reading that thread is depressing. The general lack of comprehension of cpu speed governors - yep, it's doing nothing, so slow down the clock turn things off etc to save power. That's why it shows 300 bogomips, nowt to do with what connector you supply power through.

    Would we really like our smart phones battery to last 5 mins instead of (maybe) a day ?  Or is this technology a good thing ?  

    (I prefer the phones battery to last a week, no smartphone for me!)

     

    Anyway, I claim victory on the benchmark

    Submitter
    Time (s)
    Bored
    Clock (MHz)
    O/S
    me!1.944yes800MCC

     

    I'm sure it'd be faster if it'd run long enough to bring the processor out of idle and off the slowest clock speed too. image

     

    On a more serious note, it's about 12.8 secs on a sabre-lite with debian armhf, so the BBB angstrom build seems to have been better optimised than the generic debian.

    On the BBB with angstrom I get 12.090 with the ondemand governor and 11.86 with the performance governor, showing that the governor has some latency, but nothing that anyone will care about.

    Bogomips on the A9 core of the sabre-lite is 1988 per core vs 990 on the BBB's A8 showing the futility of artificial benchmarks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    I did my share of chuckling at some of the beginners' posts there too while looking for usable numbers, but I think the interaction with CPU speed governers eventually dawned even on the beginners in the thread (well aided by people like dom), so it occurred to me while browsing that the discussion there was having a useful educational effect.

     

    They were even advising caution about assigning inappropriate meaning to BogoMips.  Win! \o/ image

     

    PS. I added your Sabre-lite and BBB findings to the table as additional datapoints.

     

    PPS. Cortex-A8 looks set to having a long life, despite many newcomers buzzing around its heels.  It's also the ARM core in my original Samsung Galaxy Tab 7" tablet, and has no trouble being snappy enough for that application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    floating point doesn't get you 2000 digits.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Run the program and count the digits yourself. It is a well know exercise to compute pi to way more digits that are available on any processor architecture

    that I am aware of. I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    >I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

     

    floating point doesn't get you 10^13 digits either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    So how do they do it ?

     

    Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries for

    several languages and allows higher precisions than are directly supported by the native hardware and use the

    native hardware to do it.

     

    I don't believe that's how they calculate pi to so many digits (very clever algorithms I suspect, not my area of expertise)

    but I'm pretty sure they do use floating point since it is normally done on a supercomputer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries

     

    no, I've never heard of an arbitrary precision arithmetic library that uses floating point.

    Perhaps you can show an example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    http://www.hvks.com/Numerical/arbitrary_precision.html

    http://www.apfloat.org/apfloat/

    http://gmplib.org/

     

    There are more, and you can find them using google.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to shabaz

    As part of a suite of benchmark programs, exactly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    I was looking for ones that are implemented using floating-point.

    All the ones I'm aware of use integers, as described in Knuth's Volume 2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to morgaine

    Nobody here has made any inappropriate conclusions from this data

     

    Never said they did, I just said that useful conclusions can't be derived from the data.

     

    so whatever are you arguing about?

     

    DAB says it best:

     

    In my architecture analysis days we used the term " Lies, damn lies and benchmarks!"

     

    Most computer architectures are too varied to assess with simple benchmarks.  You really need to look at your proposed application and look into the system architecture to get a good feel about how well one processor will perform over another.

     

    Unless you work with each processor in assembly language, you will seldom collect anything but interesting data.

     

    True performance is always dependant upon the compiler, application structure, operating system, I/O drivers and many other details.

     

    Raw power is seldom the only answer needed for a good system design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    http://www.nongnu.org/hpalib/

     

    "The functions forming the HPA library are all implemented in a portable fashion in the C language. The IEEE 754 standard for floating point hardware and software is assumed in the PC/Unix version of this library."

     

    There are also several papers (pdfs) from that describe using IEEE 754 floating point hardware for arbitrary precision arithmetic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    http://www.nongnu.org/hpalib/

     

    "The functions forming the HPA library are all implemented in a portable fashion in the C language. The IEEE 754 standard for floating point hardware and software is assumed in the PC/Unix version of this library."

     

    There are also several papers (pdfs) from that describe using IEEE 754 floating point hardware for arbitrary precision arithmetic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > The functions forming the HPA library are all implemented in a portable fashion in the C language.

     

    I have looked at this C code, and it sure looks to me like it is doing everything using integers.

    For example, xadd.c contains the code to add two numbers, and it declares these variables:

     

         unsigned short pe[XDIM + 1], h, u;  

         register unsigned short *pa, *pb, *pc, *pf = pe;  

         register unsigned int n = 0;  

         short e;  

         register short k;

     

    all of which are integers. 

     

    The arbitrary precision numbers are stored in a struct called xpr,

    declared in xpre.h, defined as:

     

      struct xpr  

      {    

         unsigned short nmm[XDIM + 1];  

      };

     

    which is clearly declaring an array of integers.

     

    Where are you seeing the floating-point operations in this library?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    I didn't have time to check the C code so I searched the main page for references to hardware and then the documentation page looking for the use of float

    or double in declarations of functions that were not conversions from one of those two formats to the extended precision format and I found several of those.

    I also searched for a description of the xpr structure on the document page to see if it was using integers but could not find one. I should have looked at the

    code to be sure. While writing this I found a description of the extended numbers format used in the xpr structure on the document page that I somehow

    missed the first time which confirms that it uses integers.

     

    I also checked out bc more carefully. I have never used it in any of the shell scripts that I've written so far but every reference on shell programming I've read says

    to use it if you need floating point numbers in a shell script. What I found was that it uses a selectable precision fixed point decimal digit format for its arithmetic

    operations that it allows you to select an arbitrary number of digits on both sides of the decimal point. So no floating point here either.