Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum SBC CPU Throughput
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 88 replies
  • Subscribers 63 subscribers
  • Views 11310 views
  • Users 0 members are here
  • cubieboard
  • olinuxino
  • sabrelite
  • bbb
  • BeagleBone
  • rpi
Related

SBC CPU Throughput

morgaine
morgaine over 13 years ago

I notice that people are doing some initial benchmarking of BBB and other boards on the RPF forum.  Results roughly as expected I guess:

 

Using just a simple

 

time echo "scale=2000;4*a(1)" | bc -l

 

as a lightweight benchmark, I see these numbers reported (smaller Time is better):

 

[table now updated with extra datapoints reported in current thread below]

 

Submitter
Time (s)
Board
SoC
Clock (MHz)
O/S
shuckle26.488Raspberry Pi BBCM2835700Raspbian 3.1.9
morgaine25.719Raspberry Pi BBCM2835700Raspbian 3.1.9+ #272
shuckle25.009Raspberry Pi BBCM2835700Raspbian 3.2.27
trn24.280Raspberry Pi BBCM2835700Raspbian ?
morgaine22.456Raspberry Pi BBCM2835800Raspbian 3.1.9+ #272
morgaine21.256Raspberry Pi BBCM2835800Raspbian 3.6.11+ #545, new firmware only
selsinork21.0MinnowboardAtom E640T1000Angstrom minnow-2013.07.10.img
shuckle17.0Raspberry Pi BBCM28351000Raspbian ?
morgaine16.153BB (white)AM3359720Angstrom v2012.01-core 3.2.5+, user-gov
selsinork15.850A20-OLinuXino-MICROA20912Debian 7.0, 3.4.67+
selsinork15.328CubieboardA20912Ubuntu/Debian 7.1
pluggy14.510BBBAM33591000Debian
morgaine14.153BBBAM33591000Debian 7.0, 3.8.13-bone20, perf-gov
selsinork13.927A10-OLinuXino-LIMEA101000Debian 7.0, 3.4.67+
Heydt13.159CubieboardA101000?
selsinork12.8Sabre-litei.MX61000Debian armhf
selsinork12.752CubieboardA20912Ubuntu/Debian 7.1 + Angstrom bc
selsinork12.090BBBAM33591000Angstrom dmnd-gov
pluggy11.923BBBAM33591000Angstrom
selsinork11.86BBBAM33591000Angstrom perf-gov
selsinork9.7Sabre-litei.MX61000Debian armhf + Angstrom bc
selsinork9.606Sabre-litei.MX61000LFS 3.12, gcc-4.8.2, glibc-2.18

 

 

As usual, take benchmarks with a truckload of salt, and evaluate with a suitable mixture of suspicion, snoring, and mirth. Use the numbers wisely, and don't draw inappropriate conclusions. image

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +2
    floating point doesn't get you 2000 digits.
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    Data is always good, and sharing it is also good. The warnings are to help people avoid unwarranted conclusions. And when used properly, synthetic and other artificial benchmarks can be very valuable,…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +1
    > and don't understand why you think it is a good idea to keep it in the loop so you can benchmark it. Come on. It's not that complicated. Johnny wanted to know how fast his new computer was. He decided…
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Loop unrolling is what I meant to say. Loop invariant code hoisting removes code that should not be in the loop to begin with because the results

    obtained from executing the code does not change (invariant) with each iteration of the loop so you are just wasting CPU cycles each time it

    executes inside the loop. I personally try to keep such code out of loops in the first place because as far as I know it is generally considered to

    be bad programming (wastingCPU cycles and all that) and don't understand why you think it is a good idea to keep it in the loop so you can

    benchmark it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Run the program and count the digits yourself. It is a well know exercise to compute pi to way more digits that are available on any processor architecture

    that I am aware of. I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > and don't understand why you think it is a good idea to keep it in the loop so you can benchmark it.

     

    Come on.  It's not that complicated.


    Johnny wanted to know how fast his new computer was.  He decided to measure how long it takes

    to multiply two numbers together.  He wrote a program that did that, but it ran so fast that his

    stopwatch was useless.  He got a brilliant idea.  Put the multiplication inside a loop that iterates

    1,000,000 times, and time that, and divide the time by 1,000,000.  But his compiler recognized

    the multiplication as loop invariant, and hoisted it out of the loop, so his program only ended up

    doing one multiplication, and his stopwatch was still useless.  Finally he recognized that an

    important feature of a benchmark program is that it avoids doing a calculation repeatedly in a loop.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    >I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

     

    floating point doesn't get you 10^13 digits either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    image I think we need to be more logical about this:

     

    1.  Nothing is better than an accurate benchmark.

     

    2.  But an inaccurate benchmark is better than nothing.

     

    3.  Therefore, an inaccurate benchmark is better than an accurate benchmark.

     

    [Adapted from a favorite sillygism image]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Come on.  It's not that complicated.


    Read it again, carefully. Yes you can waste as many CPU cycles as you want to executing code over and over again

    inside a loop that produces a result that never changes (that's why it's called invariant) no matter how many times

    the code is run in the loop.

     

    Why do you want to ? It serves no purpose, at all other than wasting CPU cycles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    Yep I agree that is a sillygism.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Johnny put his multiplication statement inside a loop so that his program would

    run long enough for his stopwatch to be useful.  Turned out his stopwatch still

    wasn't useful because the compiler hoisted the multiplication outside of the loop.

    So Johnny learned his lesson and from now on insists on benchmarks that

    don't involve a loop containing an invariant calculation.  

     

    For example, Johnny would much rather benchmark a calculation of pi to 2000 digits

    than he would a loop that calculates 200 digits 10 times over.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    So how do they do it ?

     

    Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries for

    several languages and allows higher precisions than are directly supported by the native hardware and use the

    native hardware to do it.

     

    I don't believe that's how they calculate pi to so many digits (very clever algorithms I suspect, not my area of expertise)

    but I'm pretty sure they do use floating point since it is normally done on a supercomputer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries

     

    no, I've never heard of an arbitrary precision arithmetic library that uses floating point.

    Perhaps you can show an example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>