Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Comparing BeagleBone Black & Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 60 subscribers
  • Views 4684 views
  • Users 0 members are here
  • pi
  • beaglebone_black
  • sbc
  • oshw
  • raspberry_pi
  • bbb
  • BeagleBone
  • beagleboard
  • open_source_hardware
  • linux
Related

Comparing BeagleBone Black & Raspberry Pi

fustini
fustini over 13 years ago

A discussion thread recently popped up on the ChiBots mailing list to which I subscribe.  One of the members had just heard about the BeagleBone Black (BBB) and was curious to how it compars to the Raspberry Pi B.  Here's the reply I sent to the list which I thought might be useful to others.  And I thought subsequent discussion here would help me flesh out some additional advantages and disadvantages of both:

BBB $45 vs RPi Model B $35: BBB includes 2GB built-in flash & can run off

computer USB port [<500mA] so that would make up the cost

difference if one has to buy SD card and power supply for Pi.

 

BBB is Open Source Hardware: schematics, layout & BOM, plus it only uses

parts that are avail in low qty. RPi only have schematics released and

its processor is not available (only via high volume contract). I think

BBB is great for design engineers to prototype with and then modify for

their specific application.

 

BBB has programmable realtime units (PRU or PRUSS): Two 200 Mhz

microcontrollers built-in to its main processor.  It is possible to offload realtime control to the PRU where

instructions are single cycle.  Great blog posts about PRU:

 

http://www.element14.com/community/community/knode/single-board_computers/next-g\
en_beaglebone/blog/2013/06/07/bbb--building-a-thermal-imaging-camera

http://hipstercircuits.com/accelerated-stepper-motors-on-beaglebone/

http://bb-lcnc.blogspot.com/

 

BBB has no video decode/encode hardware: It does video in software. It

is ARM Cortex A8 (ARM v7) with NEON (vector processing) so it can play

video but it won't be the video workhorse the Pi is.  I believe

media center is the best use case for RPi model B over the BBB.

 

BBB has the ARM v7 instruction set so there is a wider range of distros

available. Things are still in progress post April launch, but the orig

Bone had Android, Debian, Fedora, Ubuntu, Angstrom & many more. The Pi's

ARM v6 instruction set holds it back requiring specialized distros that

recompile packages for the older instruction set (like Raspbian).

 

BeagleBoard.org and the BeagleBone leaders are passionate about getting

everything in the mainline kernel. They work with Linux kernel

maintainers to get their patches accepted upstream. I've been told they

hope to have everything in the mainline by sometime this year. BBB was a

big jump forward from BB White as they went from Linux 3.2 to Linux 3.8

*and* the shift to Device Tree for configuration of peripherals. This

was been alot of work for the Beagle developers but they are now the first

ARM dev board to embrace DT. This has the advantage of making hardware

configuration as simple change to a config file rather than having to

recompile the kernel. The transition has to be done by an new ARM board

looking to get accepted upstream. TL;DR - BBB has a strong commitment to

running the latest Linux kernel and not getting stuck in some vendor

specific fork of Linux.

 

Cheers,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • colecago
    colecago over 13 years ago +1
    Cool. I'd also like to see how the pcDuino fits in there.
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Drew Fustini wrote: BBB $45 vs RPi Model B $35: BBB includes 2GB built-in flash & can run off computer USB port [<500mA] so that would make up the cost difference if one has to buy SD card and power supply…
  • johnbeetem
    johnbeetem over 13 years ago +1
    There's a very long discussion about this here: http://www.element14.com/community/thread/23575?tstart=0 I'll quote from my first comment at that thread, since it makes IMO a good "elevator speech" summary…
Parents
  • morgaine
    morgaine over 13 years ago

    Just linking John's well researched comparison of the state of openness and/or documentation for the two boards here, so that it doesn't get lost.  That thread in the Pi Group is growing like topsy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Also,

    This:

    image

    (by the way, it looks like the ticks on the silkscreen near the headers is ideal for counting off 10 pins at a time)

    versus this:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Also,

    This:

    image

    (by the way, it looks like the ticks on the silkscreen near the headers is ideal for counting off 10 pins at a time)

    versus this:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to shabaz

    Also,

    image

    (We could use these images to annotate any mods/changes we make).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to shabaz

    A bit more documentation-friendly: