Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum TGIF Roundup: GPIO, GSoC & the assembly line
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 58 subscribers
  • Views 1592 views
  • Users 0 members are here
  • python
  • Black
  • beaglebone_black
  • bbb
  • BeagleBone
  • bb_black
  • beagle_bone_black
Related

TGIF Roundup: GPIO, GSoC & the assembly line

fustini
fustini over 13 years ago

TGIF - the weekend is almost here! image

 

The manufacturer of the BeagleBone Black, CircuitCo in Texas, has a great video:

 

The making of BeagleBone Black

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Adafruit has added a BBB tutorial:

Setting up IO Python Library on BeagleBone Black

 

Derek Malloy has created an excellent video that explains BBB GPIO and device tree:

Introduction to GPIOs - Using Device Tree Overlays under Linux 3.8+

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

BeagleBoard.org Google Summer of Code 2013

coding starts this Monday, June 17

http://beagleboard.blogspot.com/2013/06/beagleboardorg-google-summer-of-code.html

 

 

Capture input events via GPIO on BeagleBone black

http://hipstercircuits.com/capture-input-events-via-gpio-on-beaglebone-black/

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cheers,

Drew

htttp://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +2
    Hello! My first GSoC proposal was to boot a kernel+initrd over usb from an Android device and afterwards communicate via ADK with the device to use it as touchscreen. This proposal was made on the assumption…
  • shabaz
    shabaz over 13 years ago +1
    Thanks for the links! The 'Making of Beaglebone' video was great to watch - I'd never seen how the selective wave soldering was done before. The 'Flashing and burn-in" at 3:15 with all the blue lights…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    There are many ways to solder the bottom side, that's just one approach. Others that have been used are to put the board into a heat resistant carrier that's machined out to mask off certain areas, it…
Parents
  • shabaz
    shabaz over 13 years ago

    Thanks for the links! The 'Making of Beaglebone' video was great to watch - I'd never seen how the selective wave soldering was done before. The 'Flashing and burn-in" at 3:15 with all the blue lights on dozens of boards looks a little scary :-)

    Regarding the Adafruit tutorial, I'm not sure if the 'opkg update' is advisable on that web page, I think that step should be avoided currently.

    The GSoC link is interesting. I hadn't realized there was any interest in reviving Minix though. The work on the JTAG is interesting, especially if there will be some drivers for programming popular devices (e.g. Atmel, Xilinx), to save having to buy so many separate tools, although costs have gone down nowadays. I wonder if 'LCD debug/patchwork' includes the ability to easily customize the frequency and resolution without people having to compile a driver, so that any generic TFT can be driven.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    shabaz wrote:

     

    The 'Flashing and burn-in" at 3:15 with all the blue lights on dozens of boards looks a little scary :-)

     

    I was in stitches when I saw that, immediately picturing the screams of pain and horror issuing from some quarters. image

     

    I hadn't realized there was any interest in reviving Minix though.

     

    Minix could turn into something very interesting for embedded work.  I looked at several different microkernels a few months back, and they all seem to have different pros and cons.  It's a very active research area to find a good microkernel model that still provides an effective POSIX-compliant subsystem and is able to harness the vast mountain of Unix-type software that realistically cannot be ignored.  Minix isn't likely to become a big-time microkernel for everything, but it's still worth exploring I think.  Expanding one's mental horizons is always good.

     

    Linus doesn't want to admit it but microkernels are definitely the future, and I fully expect Linux to move slowly in that general direction without anyone saying so openly and honestly, at least not until Linus retires from the driving seat.  Eventually he'll fudge some kind of political excuse like "We're restructuring the kernel to provide more runtime modularity, but avoided all the pitfalls preached by the microkernel advocates" ...  Well, whatever excuse works for you Linus, lol.

     

    The point is, monolithic systems have no future, and that should be so obvious to any software engineer that it's barely worth justifying.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    BBB resources are going from strength to strength.  This is all highly encouraging.

     

    Morgaine.

    As we suspected months ago, the real-time possibilities with the BBB are really helpful. I think it will tempt people to use the BBB in places they would not have considered in the past.

    For example, I've been working (slowly!) on a reflow oven for about 6 months now (I don't get much time to work on it) and I was going to use a low cost AVR, but I'm now considering the PRU for control because it could continue running even if there was some fault in the Linux application software (I have a hardware cutout if all fails), and the Linux application side is nice, because I would like to have a capture of data that I can easily retrieve and graph. With an AVR, I would have had to send serial data and post process; with the BBB I can in theory just dump the entire file to flash and SFTP it any time.

     

    Morgaine Dinova wrote:

     

    Linus doesn't want to admit it but microkernels are definitely the future

     

    I need to read more about it, but I'm seeing a similar thing in industry, where it's very convenient to develop "features" for products once, as long as the underlying architecture allows it to be scalable to consume resources on a single CPU shared with other features, or ported across to a separate CPU as a single or multiple instance of the feature, or to separate physical boxes. Time for me to read some of Tanenbaum's book, it's been on the bookshelf for ages. I don't really know much about Minix.  Although it must have changed an awful lot since he wrote the book.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    BBB resources are going from strength to strength.  This is all highly encouraging.

     

    Morgaine.

    As we suspected months ago, the real-time possibilities with the BBB are really helpful. I think it will tempt people to use the BBB in places they would not have considered in the past.

    For example, I've been working (slowly!) on a reflow oven for about 6 months now (I don't get much time to work on it) and I was going to use a low cost AVR, but I'm now considering the PRU for control because it could continue running even if there was some fault in the Linux application software (I have a hardware cutout if all fails), and the Linux application side is nice, because I would like to have a capture of data that I can easily retrieve and graph. With an AVR, I would have had to send serial data and post process; with the BBB I can in theory just dump the entire file to flash and SFTP it any time.

     

    Morgaine Dinova wrote:

     

    Linus doesn't want to admit it but microkernels are definitely the future

     

    I need to read more about it, but I'm seeing a similar thing in industry, where it's very convenient to develop "features" for products once, as long as the underlying architecture allows it to be scalable to consume resources on a single CPU shared with other features, or ported across to a separate CPU as a single or multiple instance of the feature, or to separate physical boxes. Time for me to read some of Tanenbaum's book, it's been on the bookshelf for ages. I don't really know much about Minix.  Although it must have changed an awful lot since he wrote the book.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to shabaz

    Maybe we should create a separate post or blog to follow the GSoC work, but basically Vlad's project (full name Vlad Victor Ungureanu, from Romania) is explained here, and he's started coding. It's very interesting - if I understand it correctly, it should allow an android device to deploy and run software onto the BBB, and also direct the display from the BBB  to the android device if desired. I suppose in theory, BBB apps could then appear on an app store, and you could plug your mobile into the BBB to transfer it.

    I've not had a chance to look into the other projects yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    Hello! My first GSoC proposal was to boot a kernel+initrd over usb from an Android device and afterwards communicate via ADK with the device to use it as touchscreen. This proposal was made on the assumption that U-Boot SPL was already on the board and could initiate transfers. In the end, after discussed with the mentors, we decided to take the rough way ROM booting the board(board does not have anything on eMMC, no MMC inserted). ROM, U-Boot SPL and U-Boot implement same way of thinking RNDIS->Ethernet2->IP->BOOTP + TFTP. In a couple of days I will have a working Linux example if anybody is intrested( https://github.com/ungureanuvladvictor/BBBabb ) *beware code at this point is really sloppy, don`t get scared*. The progress of the project can be read at http://beagleboot.vdev.ro/ . Now the blog is mainly empty but after i get it working on Linux I will explain the flow of operations and how to use it. If a new thread is created it`s fine by me, I can post from time to time there to keep people up to date with the progress.