Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum TGIF Roundup: GPIO, GSoC & the assembly line
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 58 subscribers
  • Views 1591 views
  • Users 0 members are here
  • python
  • Black
  • beaglebone_black
  • bbb
  • BeagleBone
  • bb_black
  • beagle_bone_black
Related

TGIF Roundup: GPIO, GSoC & the assembly line

fustini
fustini over 13 years ago

TGIF - the weekend is almost here! image

 

The manufacturer of the BeagleBone Black, CircuitCo in Texas, has a great video:

 

The making of BeagleBone Black

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Adafruit has added a BBB tutorial:

Setting up IO Python Library on BeagleBone Black

 

Derek Malloy has created an excellent video that explains BBB GPIO and device tree:

Introduction to GPIOs - Using Device Tree Overlays under Linux 3.8+

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

BeagleBoard.org Google Summer of Code 2013

coding starts this Monday, June 17

http://beagleboard.blogspot.com/2013/06/beagleboardorg-google-summer-of-code.html

 

 

Capture input events via GPIO on BeagleBone black

http://hipstercircuits.com/capture-input-events-via-gpio-on-beaglebone-black/

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cheers,

Drew

htttp://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +2
    Hello! My first GSoC proposal was to boot a kernel+initrd over usb from an Android device and afterwards communicate via ADK with the device to use it as touchscreen. This proposal was made on the assumption…
  • shabaz
    shabaz over 13 years ago +1
    Thanks for the links! The 'Making of Beaglebone' video was great to watch - I'd never seen how the selective wave soldering was done before. The 'Flashing and burn-in" at 3:15 with all the blue lights…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    There are many ways to solder the bottom side, that's just one approach. Others that have been used are to put the board into a heat resistant carrier that's machined out to mask off certain areas, it…
Parents
  • shabaz
    shabaz over 13 years ago

    Zubair's blog is here, he's got some good links. His full name is Zubair Lutfullah Kakakhel and he is based in Leeds, currently doing an MSc. This is his project summary. He will be working on ADC drivers as far as I can tell, which will be useful for user applications, as well as touchscreens and for power management, so this is lots of useful infrastructure stuff as well as a user API. There are quite a few (7) analog dedicated (i.e. no muxing with other functions) pins that are brought out to the P9 header, internally multiplexed to a single 12-bit ADC.

     

    Also, hopefully he can tell us how to set the charge voltage on the power management IC on the BBB to 4.2V instead of 4.1V, since some batteries are spec'd for 4.2V charge.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago

    Zubair's blog is here, he's got some good links. His full name is Zubair Lutfullah Kakakhel and he is based in Leeds, currently doing an MSc. This is his project summary. He will be working on ADC drivers as far as I can tell, which will be useful for user applications, as well as touchscreens and for power management, so this is lots of useful infrastructure stuff as well as a user API. There are quite a few (7) analog dedicated (i.e. no muxing with other functions) pins that are brought out to the P9 header, internally multiplexed to a single 12-bit ADC.

     

    Also, hopefully he can tell us how to set the charge voltage on the power management IC on the BBB to 4.2V instead of 4.1V, since some batteries are spec'd for 4.2V charge.