Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Software-defined GPS receiver: BeagleBone Black + FPGA
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 59 subscribers
  • Views 3193 views
  • Users 0 members are here
  • beaglebone_black
  • software_defined_radio
  • bbb
  • BeagleBone
  • sdr
  • satellite
  • gps
  • bb_black
  • beagle_bone_black
Related

Software-defined GPS receiver: BeagleBone Black + FPGA

fustini
fustini over 12 years ago

From http://www.jks.com/sdgps/sdgps.html

Here is my breadboard version of Andrew Holme's homemade GPS receiver.

I used a BeagleBone Black (USD$45) running the preloaded Angstrom Linux. A breadboard "cape" plugs into the BBB expansion connectors to which I attached a XuLA2 FPGA development board (USD$119) based on the Xilinx Spartan-6 LX25.

This quote is a gem:

You haven't really lived until you've dead-bugged a 4 x 4 mm QFN package with 0.5 mm pitch pads using 40 AWG wire.

Anyone working with software-defined radios?  Or have steady enough hands to try this project? image

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +2
    Beware the cursed waters of RF, Here Be Dragons! (I studied them ...) And I also have a copy of Puff The Magic Dragon , which struck terror into the hearts of even the most bold. Maybe the best part of…
  • Problemchild
    Problemchild over 12 years ago +2
    Geri Elsworth did a bit on FPGA based SDRs in which she did a load of Dead bugging and Manhattan style construction . I'm sure you can manage it Drew I'd lay off the coffee for a day or two to let the…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild +2
    I think E14 is in need of a FPGA tutorial http://www.youtube.com/v/gUsHwi4M4xE
Parents
  • Problemchild
    Problemchild over 12 years ago

    Drew On the original  Radio he made the reciever prity much from the base parts and then did the baseband stuff in the FPGA using a soft CPU to do the lifting.

    On this guy's design he's used one of the high integration recievers with a seperate SAW filter and a few L's and C's. Did he then copy the other guy's CPU or did he roll or customise his own ??

    This part seemed to be missing which in fact may of been the most interesting part given the Radio integration, I was lookin forward to a description of the FPGA contents.

     

    Also what parts did he use for the SAW and the inductors I see that most of those SAWs have 2 or 40ish BW not 20 Mhz which is what the chip's data sheet states or is this a typo ??

     

    I'm all very interested in this cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to Problemchild

    I think he may have use Andrew Holme's FPGA+code. I've been a long-time reader of A. Holme's web pages - he's done some very impressive stuff, especially with frequency synthesizers. If I was to follow any design, it would be his : )

    It's amazing how integrated some ICs are, containing virtually the entire radio, whereas Andrew's one is more discrete and very sophisticated (and he's using a passive mixer). Some approaches are more harder to design into the IC, although I'm not sure at these extremely high frequencies like GPS.

    Also it is down to 0402-sized parts at these frequencies (and it looks like it from Andrew's photographs).

    Incidentally, I took apart a USB SDR dongle recently, inside it just had two main ICs, and hardly any passive components at all. It didn't pick up many local FM stations, maybe it just needs some filtering (it may be picking up wifi, or other stuff nearby and that may be overloading it).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Coder 27 that's not a tutorial but a brief overview  for his tutorial series he's working on but not started yet.

    Also I've also made a blog post over it ages ago!!

    It's very good but also very much at 10000 ft !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to shabaz

    Yes Shabaz I have it's quite good but yet another entry in to this market in this case you can buy it from the other UK  electronics distributer  that probably won't be mentioned here image

     

    Also very much more appropriately I would consider the XMOS parts also they are developed from the original Transputer line that was used in Electronics and wireless world's GPS project in the 90's

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to shabaz

    shabaz wrote:

     

    Speaking of Forth (which is what Andrew's embedded CPU used), it's not a language I'm familiar with...

    Forth a wonderful language is.  It very simple syntax semantics and has reverse Polish notation uses you don't need parentheses so objects shown in the order they executed are are and and.  I why it never caught on wonder?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to johnbeetem

    LOL : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 12 years ago in reply to johnbeetem

    I always considered Forth a Write Once Read Never language.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to johnbeetem

    Yeah the good thing about Forth is that it operates the way CPUs operate and as such it's simple to implement and pritty  simple to understand once you have got over the idea of RPN and stacking everything image.

     

    I did a Forth in Z80 assembler for my ZX Spectrum that's now 30 years ago and you have made me look at the grey tufts on the side of my head ... your fault DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to Problemchild

    John Alexander wrote:

     

    Yeah the good thing about Forth is that it operates the way CPUs operate

     

    Actually, Forth operates the same way that humans operate too ... which is not the same way in which we write arithmetic.

     

    When we evaluate the written expression (A + B), we take A and we take B and only then do we perform addition on them, just like both Forth and RPN do.  We don't take A and then do an addition, since there is no 2nd operand to add yet.  The '+' in the arithmetic expression is just put into temporary mental storage and is brought back after we've acquired B, and then we do the operation it denotes.

     

    Written arithmetic expressions are just a learned syntax, in much the same way that we learn language.  The order in which the terms of an expression are written is not the same order in which we evaluate the operations within the expression.  It's just a formal language that defines the meaning unambiguously, but we perform the operations in exactly the same order as Forth or RPN, because that's the necessary order if you want to obtain the right result.  It has nothing to do with computers.  The same applies when using pencil and paper.

     

    As to why the natural ordering of operations is not used in written nor spoken language, the other John nailed that one with his funny example.  The lack of delimiters causes extreme difficulty and ambiguity for humans.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    In Lisp, just to be different, you would say  (+ A B)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to Problemchild

    I just documented a Beaglebone Xilinx programmer, so that we can easily get going without buying expensive tools. It was nice and easy, since the code mostly existed from Xilinx. I was also looking at FTDI,but at the price the BBB is much more favourable (and cheaper than the RPI currently too!). The FRDM boards would have been a good option too, but I think one of my CodeWarrior licenses has expired :-(

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to shabaz

    I just read it,  excellent! image

     

    I rarely have any of the BBBs connected to HDMI anymore but only through ssh, so can your transfer program be invoked from the commandline with the .xsvf filename as argument?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to shabaz

    I just read it,  excellent! image

     

    I rarely have any of the BBBs connected to HDMI anymore but only through ssh, so can your transfer program be invoked from the commandline with the .xsvf filename as argument?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 12 years ago in reply to morgaine

    Hi Morgaine,

     

    Yes, SSH with CLI is possible, just passing the filename to it. Like you, I don't connect it often at all via HDMI (or USB, I just plug into a spare port on a switch and SSH). Just zipping up the code now : ) I've only tried it on a CPLD so far, but it seems stable.