Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Arduino: now a Single Board Computer!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 69 replies
  • Subscribers 63 subscribers
  • Views 10411 views
  • Users 0 members are here
  • intel
  • rome
  • makerfaire
  • arduino_tre
  • arm_cortex_a8
  • cortex_a8
  • beaglebone_black
  • sbc
  • embedded
  • tre
  • bbb
  • maker_faire_rome
  • BeagleBone
  • sitara
  • texas_instruments
  • bb_black
  • am335x
  • maker_faire
  • beagle_bone_black
  • arm
  • arduino
  • italy
  • ti
Related

Arduino: now a Single Board Computer!

fustini
fustini over 12 years ago

So I often get annoyed when folks refer to the AVR-based Arduino boards (or even the ARM microcontroller DUE) as a Single Board Computer.  The Yun blurred the lines a bit... but the news today from Maker Faire Rome has the Arduino brand fully in the SBC world now:

 

Arduino Announces new Boards and Collaboration with Intel and T.I.

http://makezine.com/2013/10/03/arduino-announces-two-new-linux-boards/

image

 

coder27 posted about the Intel-based Arduino board, and there is also an upcoming Arduino model based on the TI Sitara (same as in the BeagleBone Black - an ARM Cortex A8).

 

I just read an interview on Make with jkridner about the new Arduino TRE:

 

Talking to Jason Kridner About the new Arduino Tre

http://makezine.com/2013/10/03/talking-to-jason-kridner-about-the-new-arduino-tre/

"The focus is on simplicity. It isn’t just a BeagleBone split in the middle [...] If you know Linux, you’ll be able to come in that way. If you know Arduino, you’ll be able to use the AVR as the system master."

image

 

I'm not sure exactly what this all means, but it is exciting to have more SBC options and the Arduino brand will be an interesting influence on the SBC market.  I do know that I didn't need any coffee to feel wide awake this morning image

 

What is the feeling of our SBC discussion group here?

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +1
    I like the term "bare metal microcontroller" to denote the processors on Arduino AVR and ARM Cortex-M class boards. These contrast strongly with those boards which are based on "application processors…
  • johnbeetem
    johnbeetem over 12 years ago +1
    I have no problem with this use of Single-Board Computer. The earliest SBCs had very simple processors like Intel 8080 or MOS Technology 6502, which didn't have MMUs and didn't address much memory. When…
  • morgaine
    morgaine over 12 years ago +1
    Drew, leaving aside the puzzling situation with Galileo and how it's managing to run its peculiar version of Yocto, the Arduino TRE looks very good indeed! In fact, over the last year and a half, haven…
Parents
  • morgaine
    morgaine over 12 years ago

    I like the term "bare metal microcontroller" to denote the processors on Arduino AVR and ARM Cortex-M class boards.  These contrast strongly with those boards which are based on "application processors" that have an MMU and therefore run full operating systems (mostly Linux) and so their applications execute as user-mode processes in virtual memory --- definitely not "bare metal".

     

    It provides a clear distinction and so keeps discussions from attempting to compare apples with orangutans.

     

    PS. It's appalling to see makezine.com make this elementary error though. image

     

    PPS.  The source of the error seems to be Intel themselves!

     

    Intel writes (in the FAQ):

     

    Q: Can I run Linux on IntelRegistered Galileo?

     

    A: Yes. IntelRegistered Galileo runs Linux* out of the box. It comes in two flavors; the default is a small Linux. If you add an SD card to your kit, you can add a more fully-featured Linux. Refer to the IntelRegistered Galileo Getting Started Guide and IntelRegistered Quark SoC X1000 IoT Development Kit Software GSG.

     

    I'm still figuring out exactly what this means, but at best it's going to be something like the old uClinux, which was pretty horrible at best.  After all there is no MMU in Quark to support the normal Linux kernel --- see the Quark datasheet.  (uClinux is effectively EOL now owing to MMUs having become so ubiquitous.)

     

    PPPS.  The Galileo Getting Started Guide refers only to Linux support on the host side, not on the board.

     

    PPPPS. Oh dear.  If you zoom into the image showing what they load from uSD card, it boots into:

     

    Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4.1 clanton /dev/ttyS1

     

    I've got a very bad feeling about this.  I thought the days of MMU-less "Linux" derivatives were over.

     

    ===

     

    IMPORTANT ADDENDUM:  Quark does have an MMU, it's just not mentioned in the SoC Datasheet.  See this post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Intel writes (in the FAQ):

     

    Q: Can I run Linux on IntelRegistered Galileo?

     

    A: Yes. IntelRegistered Galileo runs Linux* out of the box. It comes in two flavors; the default is a small Linux. If you add an SD card to your kit, you can add a more fully-featured Linux. Refer to the IntelRegistered Galileo Getting Started Guide and IntelRegistered Quark SoC X1000 IoT Development Kit Software GSG.

    Does this imply that your choices for boot device are either onboard or SD card, but not USB or network?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Intel writes (in the FAQ):

     

    Q: Can I run Linux on IntelRegistered Galileo?

     

    A: Yes. IntelRegistered Galileo runs Linux* out of the box. It comes in two flavors; the default is a small Linux. If you add an SD card to your kit, you can add a more fully-featured Linux. Refer to the IntelRegistered Galileo Getting Started Guide and IntelRegistered Quark SoC X1000 IoT Development Kit Software GSG.

    Does this imply that your choices for boot device are either onboard or SD card, but not USB or network?

     

    Curious, isn't it?  Their very odd phrasing "a small Linux" and "a more fully-featured Linux" without mentioning any names of standard distros was one of the reasons that suggested to me (or at least didn't contradict) that this was uClinux running on a microcontroller --- this is not the case, as we now know.  But why the reticence to state the name of the distro in the FAQ?  There's nothing shameful in running Yocto.

     

    It seems unlikely that Intel would have built in such a severe restriction on boot sources at hardware level, so perhaps this is a temporary limitation while they sort out drivers.  The mini-PCIe connector is a likely candidate for disk interfaces in the future, but Intel's brief 13-page Galileo Datasheet (more like a set of slides) suggests that mini-PCIe support is currently limited to "the WiFi library".

     

    I think the latter term refers to support within Arduino sketches  though.  In plain Linux you might be able to do everything that Linux can do, driver support allowing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    but Intel's brief 13-page Galileo Datasheet (more like a set of slides) suggests that mini-PCIe support is currently limited to "the WiFi library".

    I saw mention in one of the docs (I would have to hunt for it again) that the mini-PCIe

    could be used for an additional host USB port, among other things like cellular network.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Curious, isn't it?  Their very odd phrasing "a small Linux" and "a more fully-featured Linux"

    That could simply be the difference between Debian and something where 99% of stuff is provided by busybox. Depending on what else is in there, the 8MByte of SPI flash would be enough for a linux install, albeit nothing resembling what you'd find on a desktop install.

     

    It seems unlikely that Intel would have built in such a severe restriction on boot sources at hardware level,

    Depends. Seems more likely to be a firmware limitation. For example, the Minnow has very limited firmware, nothing like what you'd commonly find on x86 desktop/server boards.

     

    Also consider the target market. Can RPi, BBB, etc. boot from network or USB ?  Do other Arduino boards ?   For something that's supposedly going to be around $60 you have to think that a lot of the complex (and therefore expensive) x86 baggage needs to get left out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    coder27 wrote:

     

    but Intel's brief 13-page Galileo Datasheet (more like a set of slides) suggests that mini-PCIe support is currently limited to "the WiFi library".

    I saw mention in one of the docs (I would have to hunt for it again) that the mini-PCIe

    could be used for an additional host USB port, among other things like cellular network.

    Part of the spec for miniPCIe is that it has a usb port wired to the connector as well as stuff like led and sim card connections. In some circumstances various parts are optional and I've seen at least one board that only provides usb to the connector.

    There seems to have been some thought put into the miniPCIe physical connector to allow it to be used for a wide range of purposes, traditional wifi, cellular modem with remote SIM, usb bluetooth, all in the same form factor, possibly on separate cards, or even combined onto one.

     

    One of my first thoughts from the wording was that the connector on the Galileo would be a usb only version and therefore limited in scope. However there's a block diagram in one of the docs that shows both PCIe x1 and USB2.0 going to the connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Can RPi, BBB, etc. boot from network or USB ?

     

    Pi can't boot from network or USB because booting is done by the utterly closed VideoCore.  However, BBB can boot from anywhere, in principle, since U-boot runs on the ARM which is free to configure any devices it wants prior to finding and loading a kernel.  And the 2GB flash means that U-boot always has somewhere to run and keep its configs while sorting out from where to get a kernel.

     

    This doesn't mean it's easy if the boot support that one wants doesn't exist yet, but in the open source community that tends to get rectified pretty quick.

     

    Ultimately though, anything can boot from anywhere (with the exception of secure boot systems), since whatever it is that loads the Linux kernel can load a generic boot loader instead.  Even poor ol' Pi has that possibility.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Part of the spec for miniPCIe is that it has a usb port wired to the connector as well as stuff like led and sim card connections. In some circumstances various parts are optional and I've seen at least one board that only provides usb to the connector.

     

    There seems to have been some thought put into the miniPCIe physical connector to allow it to be used for a wide range of purposes, traditional wifi, cellular modem with remote SIM, usb bluetooth, all in the same form factor, possibly on separate cards, or even combined onto one.

     

    One of my first thoughts from the wording was that the connector on the Galileo would be a usb only version and therefore limited in scope. However there's a block diagram in one of the docs that shows both PCIe x1 and USB2.0 going to the connector.

    I'm glad to hear that the Finnegan board (I can't bear to call a Quark-based Irish board "Galileo") has PCIe.  I have a major FPGA design that's currently using 32-bit PCI and it's getting harder to find processors with PCI.  (I don't need the bandwidth -- I just need the connectivity.)  At some point I may need to change the PCI interfaces to PCIe -- once I can get a cheap enough FPGA that has built-in PCIe.  So Finnegan would be a cheap way to exercise the PCI interface -- with lots of fun bare-metal programming image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    It's curious how ARM is taking over the world without really having a coordinated strategy for high-bandwidth I/O.  Maybe Galileo will give them a bit of a push in that direction, although a single PCIe connector isn't really pushing anything when the board lacks both SATA and gigabit Ethernet and so needs at least two just to be on par.

     

    It's worth pointing out that the Ethernet MAC on the Quark is only 10/100Mbps, so this chip has limited life expectancy in a world where network speeds and expectations are heading rapidly skywards.  TI's low-cost AM3359 device has two gigabit MACs and has been around for a long time now, so Intel has some way to go to stay in touch with the field in this area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    It's curious how ARM is taking over the world without really having a coordinated strategy for high-bandwidth I/O.  Maybe Galileo will give them a bit of a push in that direction, although a single PCIe connector isn't really pushing anything when the board lacks both SATA and gigabit Ethernet and so needs at least two just to be on par.

     

    It's worth pointing out that the Ethernet MAC on the Quark is only 10/100Mbps, so this chip has limited life expectancy in a world where network speeds and expectations are heading rapidly skywards.  TI's low-cost AM3359 device has two gigabit MACs and has been around for a long time now, so Intel has some way to go to stay in touch with the field in this area.

    The vast majority of ARM applications are cell/smart phones and tablets.  Both are limited to wireless networking speeds, so 100 Mb/s is adequate.  Even a wired media center is limited by the bandwidth into your home.  ARM processors with high-performance video are usually integrated SoCs, so who needs PCIe if you have 64-bit on-chip buses?  Also, you usually don't have a hard drive in your phone or tablet, so you don't need SATA.

     

    In contrast, AM3359 is designed for high-performance industrial networking, so GBE is definitely useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    It's curious how ARM is taking over the world without really having a coordinated strategy for high-bandwidth I/O.  Maybe Galileo will give them a bit of a push in that direction, although a single PCIe connector isn't really pushing anything when the board lacks both SATA and gigabit Ethernet and so needs at least two just to be on par.

     

    It's worth pointing out that the Ethernet MAC on the Quark is only 10/100Mbps, so this chip has limited life expectancy in a world where network speeds and expectations are heading rapidly skywards.  TI's low-cost AM3359 device has two gigabit MACs and has been around for a long time now, so Intel has some way to go to stay in touch with the field in this area.

    The vast majority of ARM applications are cell/smart phones and tablets.  Both are limited to wireless networking speeds, so 100 Mb/s is adequate.  Even a wired media center is limited by the bandwidth into your home.  ARM processors with high-performance video are usually integrated SoCs, so who needs PCIe if you have 64-bit on-chip buses?  Also, you usually don't have a hard drive in your phone or tablet, so you don't need SATA.

     

    In contrast, AM3359 is designed for high-performance industrial networking, so GBE is definitely useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

    The vast majority of ARM applications are cell/smart phones and tablets.  Both are limited to wireless networking speeds, so 100 Mb/s is adequate.  Even a wired media center is limited by the bandwidth into your home. 

    Wireless networking can already exceed 100Mb/s, cheap consumer internet connections are already reaching 100Mb/s here and set to exceed it soon.  With deep enough pockets I could have 10Gb/s to my home in a few months time (the few months being mostly lead time to run the fibre).

    The only thing that's realitively certain is that both bandwidth requirements and availibility will continue to increase over time and that devices that don't keep up are destined to die.

     

    On the other hand, taking into account use cases and target price range, 100Mb/s was probably the right choice. There's bound to be a new spin of the SoC along soon enough that'll include updated capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    There's bound to be a new spin of the SoC along soon enough that'll include updated capabilities.

     

    Yep, extremely likely.  I can't believe that Intel want their name associated with low-performance embedded only.

     

    Today's embedded ARM SoCs are having their cake and eating it too, combining high performance with low power consumption, and the level of integration is extreme.  And as if that weren't enough, the killer problem for Intel is one that they have not faced before:  very low prices.  Catch-up with ARM is going to be hard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    And as if that weren't enough, the killer problem for Intel is one that they have not faced before:  very low prices.  Catch-up with ARM is going to be hard.

    The thing about having Intel as the opposition is that it's like tip-toe around the slumbering beast, do you really want to wake it up and have it focus it's attention on you ?

     

    They obviously have some strategic/political reasons for pushing x86 as far as they can, but you can't really blame them when it's historically been very lucrative.

     

    However I wouldn't bet against them if they ever decided to truly focus on the Arm segment without dragging along the x86 baggage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    selsinork wrote:

     

    There's bound to be a new spin of the SoC along soon enough that'll include updated capabilities.

     

    Yep, extremely likely.  I can't believe that Intel want their name associated with low-performance embedded only.

     

    Today's embedded ARM SoCs are having their cake and eating it too, combining high performance with low power consumption, and the level of integration is extreme.  And as if that weren't enough, the killer problem for Intel is one that they have not faced before: very low prices.  Catch-up with ARM is going to be hard.

    Yes, Intel has to be very careful here that the low-cost chips don't have high enough performance to eat into the high-margin chips that they need to pay the bills.  ARM is a low-overhead operation, since they don't need to build fabs and keep them busy.  ARM is also not greedy -- they are happy to license billions of older ARMs for pennies and charge more for the newest ARMs.  A few years ago Intel tried to license Atom, but for whatever reasons didn't get any nibbles.  My guess is they charged too much, either per copy or with up-front fees, or both.

     

    The thing with technology is that you have to use the profits from today's technology to design the next generation which will make your current technology obsolete.  It's what your competition is doing, so if you try to extend the lifetime of a cash cow too far you're likely to have a lot of trouble down the road.  Artificially limiting the performance of a low-cost new product so it doesn't compete with your older product usually ends in disaster.  My favorite example of this is the IBM PCjr.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    So which future do you think will happen?

     

    • ARM will continue increasing performance into Core2* and Xeon territory and beyond, while prices will remain roughly at current levels because of competition among ARM licensees.  As a result, Intel's cash cow withers and Intel dies.

     

    • Intel will bring x86 power requirements down to that of ARM and x86 pricing down by 1 or 2 orders of magnitude to match ARM.  As a result, Intel's profitability and R&D funding withers and Intel dies.

     

    Is there a third alternative? image

     

    Personally, I want there to be a third alternative (a real one), as it's very unhealthy for ARM to be unopposed.  There's also the very important factor (for me) that Intel is a good citizen in open source, while ARM itself is comparatively lacklustre (some ARM licensees are good in this respect though).  If there's a way for Intel to survive this ARM onslaught, that would be good.

     

     

    PS. Note that AMD seems to be aware of the danger ahead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    So which future do you think will happen?

     

    • ARM will continue increasing performance into Core2* and Xeon territory and beyond, while prices will remain roughly at current levels because of competition among ARM licensees.  As a result, Intel's cash cow withers and Intel dies.

     

    • Intel will bring x86 power requirements down to that of ARM and x86 pricing down by 1 or 2 orders of magnitude to match ARM.  As a result, Intel's profitability and R&D funding withers and Intel dies.

     

    Is there a third alternative? image

     

    Personally, I want there to be a third alternative (a real one), as it's very unhealthy for ARM to be unopposed.  There's also the very important factor (for me) that Intel is a good citizen in open source, while ARM itself is comparatively lacklustre (some ARM licensees are good in this respect though).  If there's a way for Intel to survive this ARM onslaught, that would be good.

     

     

    PS. Note that AMD seems to be aware of the danger ahead.

    I wouldn't underestimate Intel.  IMO nobody is better than Intel at getting performance out of silicon, and since they have control of both architecture and fabrication processing that gives them a theoretical edge over ARM who can only control architecture and foundries who can only control process.  Intel was lulled into a false sense of security by their long-term duopoly with Microsoft, which terminated rather unexpectedly thanks to iPhone and Android.  Intel has a lot of catching up to do with ARM on the low-power front, but ARM has a lot of catching up to do on the performance front.  However, Intel may be hamstrung by internal politics (see Law of Large Organizations) and expectations from Wall Street.

     

    AMD is a wild card.  To me, the exciting news is that Jim Keller, the VP of design at P.A. Semi is now at AMD which could give them some high-risk / high-payoff results.  P.A. Semi had some very attractive PowerPC offerings in the works when they were acquired by Apple.  People then had high expectations that Apple would be able to do great things with their own architecture people, but the key P.A. Semi people left Apple shortly after the acquisition (or probably, shortly after their retention bonuses timed out).

     

    With the Intel/Microsoft duopoly at an end, there's possibility for a lot of pent-up architectural ideas to flourish.  Both Intel Architecture and ARM are really messy, and something much cleaner like PowerPC or DEC Alpha has a lot of potential in the hands of P.A. Semi kind of engineers.  As Margaret Mead said: "Never doubt that a small group of committed people can change the world. Indeed, it is the only thing that ever has."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    With the Intel/Microsoft duopoly at an end, there's possibility for a lot of pent-up architectural ideas to flourish.  Both Intel Architecture and ARM are really messy, and something much cleaner like PowerPC or DEC Alpha has a lot of potential in the hands of P.A. Semi kind of engineers.  As Margaret Mead said: "Never doubt that a small group of committed people can change the world. Indeed, it is the only thing that ever has."

    She forgot to add "... but it's an uphill struggle." image

     

    You mentioned PowerPC, and I can think of one company that has more experience of PowerPC than everyone else in the world combined, but they certainly don't fit the "small group of committed people"  model.  With both Intel and ARM being a real mess archtecturally (with very different histories, but in both cases the mess can be attributed to legacy), now would be a good time for IBM to pop out of its self-imposed exile from the mass market space and offer an alternative.

     

    IBM has the design skills in depth, it has the silicon fabs, it has software expertise and numbers in overwhelming quantities.  Pity that it has decided that consorting with mere mortals is beneath it.  But that could change.

     

    While I'm at it, note that many people are currently saying that the PC architecture is ripe for change.  Well guess who created the PC legacy with which we are still living?  It's almost a cue for action!  The time would be right.

     

    Someone send this to an IBM blog please. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

    Margaret Mead said: "Never doubt that a small group of committed people can change the world. Indeed, it is the only thing that ever has."

    She forgot to add "... but it's an uphill struggle." image

    "Problems worthy of attack prove their worth by fighting back." [Piet Hein]

     

    You mentioned PowerPC, and I can think of one company that has more experience of PowerPC than everyone else in the world combined, but they certainly don't fit the "small group of committed people"  model.  With both Intel and ARM being a real mess archtecturally (with very different histories, but in both cases the mess can be attributed to legacy), now would be a good time for IBM to pop out of its self-imposed exile from the mass market space and offer an alternative.

     

    IBM has the design skills in depth, it has the silicon fabs, it has software expertise and numbers in overwhelming quantities.  Pity that it has decided that consorting with mere mortals is beneath it.  But that could change.

    Actually, the original IBM 801 people were "a small group of committed people" fighting against Armonk's IBM360/370 mind-set -- a major up-hill struggle.

     

    At one time IBM had a nice set of embedded PowerPC chips (403GA, 401GF -- PowerPC in an 80-pin TQFP!) which I used in several products for a previous employer.  The documentation was excellent.  IBM sold the line to AMCC who's now moving on to 64-bit ARM.  I've used the AMCC 405EP in a design, and it's a great part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Personally, I want there to be a third alternative (a real one), as it's very unhealthy for ARM to be unopposed.

    One possibility would be that Arm sticks to relatively low power devices while Intel stays in the datacenter and both remain somewhat complimentary since the devices rely on the datacenter for a lot of what they do. Sorry, BS terms like 'cloud' stick in my throat image

     

    Another would be that Intel jumps into bed with Arm in a big way, Intel gains low power processors, Arm gains access to some of the best process technology. Could be a win for both, but likely impossible due to internal politics in Intel keeping the focus on x86.  Not without some precedent though, remember that Intel were (possibly still are) an Arm licensee with XScale.

     

    Other less likely alternatives would be Intel spending some pocket change and buying Arm.

     

    Arm isn't entirely unopposed, they have two ways of licensing their stuff, one where you license the full design, the other where you license the instruction set and can build your own implementation. So there's a possibility that someone with the engineering expertise could produce a better Arm implementation than Arm themselves are able to.  I'd expect that Intel has the expertise, whether they have the will to do it is another matter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    While I'm at it, note that many people are currently saying that the PC architecture is ripe for change.  Well guess who created the PC legacy with which we are still living?  It's almost a cue for action!  The time would be right.

    I don't think IBM have any interest in PC hardware anymore. They have quite successfully moved on, unlike some of the others.

     

    The PC has been ripe for change for some time now, but you're back to that 'warm fuzzy feeling' problem. It's familiar, relatively standardised across manufacturers, and mass produced. Whoever steps out of line first has a huge battle to gain acceptance from both the other hardware manufacturers and the software suppliers.

     

    One of the biggest strengths of the x86 PC is that it's not single source and that all of the different manufacturers mostly follow the same standards.  This is where Arm falters with the proliferation of manufacturers doing their own thing and all being sufficiently incompatible to be a problem.

     

    So who is big enough, has deep enough pockets, to take on the Dell's and HP's and the wall street vested interests?  Who will be the Compaq to their IBM and drive competition on the re-imagined platform ?