Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum 6502 Video Out
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 18 answers
  • Subscribers 66 subscribers
  • Views 7283 views
  • Users 0 members are here
  • composite
  • mos
  • 6502
  • video out
Related

6502 Video Out

nick123
nick123 over 10 years ago

Hello,

I've been working on a 6502 SBC recently, and I wanted it to output to a composite video signal. I looked around the internet and didn't find much of anything. Anyone know a way I can do this?

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 10 years ago in reply to nick123 +5 suggested
    Some info of what used to be here https://en.m.wikipedia.org/wiki/Video_display_controller The video subsystems of these oldies used to make up the bulk of the electronics in those machines and the display…
  • DAB
    DAB over 10 years ago +4 suggested
    Hi Nick, As I recall, the Commodore PET that I have used a batch of memory to hold the video data. All you need is a couple of counter chips to run through the addresses of the RAM chips. You take the…
  • michaelkellett
    michaelkellett over 10 years ago +4 suggested
    If you want to remain "classic" you would need to use a video controller MC6845 or perhaps 6569: MOS 6569R3 C64 VIC-II PAL chip, Mutant Caterpillar Games Ltd Retro Store Google for the 6845 data sheet…
  • shabaz
    0 shabaz over 10 years ago

    Hi Nick,

     

    Generally the 6502 can't do that, it cannot generate a 6MHz signal on its own with the right timings and content (there may be some hacks I'm sure that might obtain a low-res image onto a display however, through clever coding in assembler etc). Usually the old home computers used separate ICs and sometimes custom logic for that, but of course they are not manufactured nowadays. You could look at old home computer schematics and hope to find the parts on e-bay. Or you could use slightly more modern parts to create a video encoder (Analog Devices has some parts) but you still need a way of getting data from memory to the encoder, and that entails using a CPLD or FPGA usually.

    Basically times have moved on, and if you just want to display very simple information to a screen then you might want to consider (say) LCD displays with in-built memory and a simplified interface. If you're trying to recreate a vintage computer then you may need to consider programmable logic.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Might check out http://www.6502.org/homebuilt Bet someone has way to output.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Saw this Retro Computing – Page 6502 – About small SBC systems which reminded me of the KIM-1. We never output to video, but did write data to a serial teletype. They were only 4K memory of which 1/2 was dedicated to a simple OS.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to clem57

    Shoot you can get the schematics to the Commodore 64 /pub/cbm/schematics/computers/c64/

     

    They had to interface to the VIC chip IIRC.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 10 years ago

    Hi Nick,

     

    As I recall, the Commodore PET that I have used a batch of memory to hold the video data.

    All you need is a couple of counter chips to run through the addresses of the RAM chips.

    You take the digital output and run it into a transistor with a couple of capacitors and resisters to create the analog out, synchronize the Horizontal and vertical sync waveforms and you have video output.

     

    Back in the OLD days we used this approach for all types of microprocessors.

    Later, people came out with digital to video out chips.

     

    Plus you always have the option of hacking an old PC video card.  Most of them allowed you to load digital information into the onboard ram and the card took care of the sync.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nick123
    0 nick123 over 10 years ago in reply to DAB

    This sounds interesting, do you have example schematics?

     

    Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago

    If you want to remain "classic" you would need to use a video controller MC6845 or perhaps 6569:

     

     

    MOS 6569R3 C64 VIC-II PAL chip, Mutant Caterpillar Games Ltd Retro Store

     

    Google for the 6845 data sheet which is useful for understanding how these things work. You'll probably end up with a lot of glue logic as well.

     

    What's the point/aim ?

     

    You can replicate all this stuff in an FPGA (including the 6502) and it will crank at 10x the original speed as well - if you want to run old software this may be better route.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bwelsby
    0 bwelsby over 10 years ago in reply to nick123

    Some info of what used to be here  https://en.m.wikipedia.org/wiki/Video_display_controller

    The video subsystems of these oldies used to make up the bulk of the electronics in those machines and the display resolutions were only something like 320x240 .

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 10 years ago in reply to nick123

    Maybe.

     

    I will have a quick look in my basement to see if there are any schematics of this basic design.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago

    I interfaced an MC6847 to a 6502 way back in the day. I think I still have the wire-wrapped display card I built for my AIM65.

    This was one of the simplest ways to implement a video display back then, probably still is.

    These chips are still available on the net.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>