BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Welcome the BeagleY-AI !
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 106 subscribers
  • Views 5453 views
  • Users 0 members are here
  • beagley-ai
  • beagleboard
Related

Welcome the BeagleY-AI !

cstanton
cstanton over 2 years ago

Beagleboard have brought out a new single-board computer aimed at artificial intelligence and it's in a form factor that's very different to its previous offerings:

Find out more here  BeagleY-AI 

beagley-ai 

The BeagleY-AI is available to pre-order from our online stores and I'm told we will have stock from June/July time, if not earlier. Meanwhile, the documentation is being fleshed out more than it is already, so we could consider this a 'soft launch'.

beagley-ai specs

Full schematics and details are on their github page, and all relevant links are on our product pages as I receive them.

This beagleboard intends to be an affordable Ai accelerated board compared to other offerings, and at about £57 the price is rather nice!

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 2 years ago +3
    If, like me, you got very excited and pre-ordered one then I suggest you check your order. I heard on the BeagleBoard Discord channel that they're hoping boards will arrive at the distributors very soon…
  • dougw
    dougw over 2 years ago +2
    Great feature set. I hope it catches on and builds an eco system.
  • robogary
    robogary over 2 years ago +2
    looks like a Pi :-)
Parents
  • embeddedguy
    embeddedguy over 2 years ago

    Good board.

    I have not tried more sbcs than a raspberry pi. I have beaglebone black without wireless. That is kind of useless.

    I don't get why these boards provide 4 USB ports and only one ethernet port. I am looking for boards that have two ethernet ports. That way I could try some networking stuffs and also would make sense if I use poe hat. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 2 years ago in reply to embeddedguy

    On the other hand 4 USB ports if all of them are used at once the sbc gets less power and warns about having less power than required.thats why it does not make sense to me having 4 of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to embeddedguy
    embeddedguy said:
    On the other hand 4 USB ports if all of them are used at once the sbc gets less power and warns about having less power than required

    This happens on the Pi only if you're not using a power adapter that provides sufficient power. The focus of the Pi generally is to expect you to plug in a keyboard and mouse, to the USB 2 ports, and then have demanding items in the USB3 ports, at least on the latest model.

    In my experience, power delivery has not been an issue with Beagleboard's products. 

    embeddedguy said:
    I have beaglebone black without wireless. That is kind of useless

    USB WiFi adapters work well with the beaglebone black.

    Fred27 said:
    You can add a USB ethernet adapter if you want a second ethernet port. We needed a Pi to span both an internal and external network and did this. Probably not the highest speed, but worked for our use case.

    I have done this too, gigabit ethernet USB adapters work well on the USB3 ports and have an adequate throughput.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 2 years ago in reply to embeddedguy
    embeddedguy said:
    On the other hand 4 USB ports if all of them are used at once the sbc gets less power and warns about having less power than required

    This happens on the Pi only if you're not using a power adapter that provides sufficient power. The focus of the Pi generally is to expect you to plug in a keyboard and mouse, to the USB 2 ports, and then have demanding items in the USB3 ports, at least on the latest model.

    In my experience, power delivery has not been an issue with Beagleboard's products. 

    embeddedguy said:
    I have beaglebone black without wireless. That is kind of useless

    USB WiFi adapters work well with the beaglebone black.

    Fred27 said:
    You can add a USB ethernet adapter if you want a second ethernet port. We needed a Pi to span both an internal and external network and did this. Probably not the highest speed, but worked for our use case.

    I have done this too, gigabit ethernet USB adapters work well on the USB3 ports and have an adequate throughput.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • embeddedguy
    embeddedguy over 2 years ago in reply to cstanton
    cstanton said:
    This happens on the Pi only if you're not using a power adapter that provides sufficient power. The focus of the Pi generally is to expect you to plug in a keyboard and mouse, to the USB 2 ports, and then have demanding items in the USB3 ports, at least on the latest model.

    yes, I had USB mouse+keyboard and an HDMI monitor. That just required much power than what RPI can provide. Also, cooling was needed such as fan. In such a small form factor it is sometimes hard to accommodate everything.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 2 years ago in reply to cstanton
    cstanton said:
    , to the USB 2 ports, and then have demanding items in the USB3 ports, at least on the latest model.

    Could you please tell me example of demanding USB requirements after mouse and keyboard? haha. Please don't say USB to ethernet adapter.. haha

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to embeddedguy

    I don't fully understand your question, however I'll explain what I meant.

    USB3 ports are better suited for high-speed devices, such as a USB to ethernet adapter, but also USB storage for SSDs or hard drives. USB3 in its specification should also be able to negotiate higher power draw than USB2.

    USB3 should allow for up to 900mA at 5v, USB2 is 500mA at 5v by default