Technical Library
  • Products & Partners
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents Gertboard Kit - Add-on GPIO expansion board for the Raspberry Pi
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 2 Aug 2012 5:19 AM Date Created
  • Last Updated Last Updated: 23 Jan 2014 9:58 PM
  • Views 8832 views
  • Likes 2 likes
  • Comments 26 comments
Related
Recommended

Gertboard Kit - Add-on GPIO expansion board for the Raspberry Pi

BUY NOWBUY NOWSoftware ToolsTechnical DocumentsVideoFeaturesKit Contents

image

The GertboardTM is an add-on board that extends the use of Raspberry Pi to devices in the real world, including motor/lamp control, and the sensing of voltages and currents. It also contains a host micro that can be programmed with code written and compiled for it, on the Raspberry Pi. The GertboardTM Kit contains the bareboard PCB and electronic components that allow you to self assemble your own GertboardTM.

 

 

It comes with a large variety of components, including buttons, LEDs, A/D and D/A converters, a motor controller, and an Atmel AVR microcontroller. There is a suite of test/example programs for the GertboardTM, written in C. , which is freely available from below Design Elements. The GertboardTM Kit is supported by a number of videos featuring Gert van Loo, creator of the GertboardTM and Paul Gibbon from Weller.  These video materials demonstrate how to solder through hole and surface mount components onto the GertboardTM.

 

 

Key Applications: Add-on GPIO expansion board for the Raspberry Pi

More Development Kits and Tools
imageRaspberry Pi - Single Board ComputerimageDevelopment Platform and Kits
imageGertboard Kit - Add-on GPIO board for Raspberry Piimageelement14 Knode

 

Technical Documents

 


Learning Center

TypeDescription
User ManualGertboard: User Manual for Gertboard Kit
Assembly ManualGertboard: Assembly Manual for the Gertboard Kit

 

Design Elements

 

TypeDescription
SchematicGertboard: Schematic for Gertboard Kit
Application LibraryGertboard: Application Library for Gertboard Kit (Linux)

 

Back to top

 

Video

 


 

Videos on Gertboard Kit

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Video 1: Exclusive interview with Gert van Loo, creator of the Gertboard for Raspberry Pi

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Video 2: Advice on getting ready to assemble your own Gertboard Kit

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Video 3: Through Hole Soldering Tips on the Gertboard Kit

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Video 4: Surface Mount Soldering Tips on the Gertboard Kit

 

 

Back to top

 

Kit Features

 


 

image

The major building blocks on GertboardTM are:


  • 12x buffered I/O
  • 3x push button
  • 6x Open collector driver (50V, 0.5A)
  • 48V, 4A motor controller
  • 28-pin dual in line ATmega device
  • 2-channel 8/10/12 bits Digital to Analogue converter
  • 2-channel 10 bits Analogue to Digital converter

 

 

 

 

 

 

 

 

 

 

Back to top

Kit Contents

 


  • Assembled Gertboard

 

Back to top

 


 

 


  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    I've just 'surfaced' from designing my version of a Gertboard. I wanted a different layout and don't need an Arduino - well not yet anyway. I'm here reading for a break. It's a shame there are so many…
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Soldering is easy, but a little confidence boost can never hurt!  For a fun & quick exercise, I'd recommend Make's Learn to Solder badge.  Tens of thousands of complete beginners make these in minutes at Maker Faire.  In fact, I just taught my mom and sister to solder with this badge.

     

    I've run soldering activities in the element14 booth at previous Maker Faires where hundreds of beginners successfully made the Adafruit MiniPOV and Adafruit Drawdio kits.  I also ran a soldering table at my local mini Maker Faire last weekend where several beginners made the Trippy RGB Wave kit from Mitch Altman.

     

    I would really recommend anyone interested in electronics never be afraid to solder.  I used to severely avoid soldering until Mitch Altman showed me that it is in fact easy when visiting my hackerspace a couple years ago.  The more you do it, the easier it gets!  I also used to think surface mount was too hard.  But I've done several surface mount kits now and realized that it's pretty easy too with a bit of experience (and I even prefer it now).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    First of all, nice work on the board and for providing so many videos, manuals, etc. for building and using it. However, while Gert's 10yr old daughter might be a soldering protege, it is a bit tricky to get right as some others have mentioned. It will require a steady hand and care not to lose tiny components. Also, the amount of time required to do this build is likely to be more significant that it first might appear. Why was there not an option to buy an already built board? Honestly, I put the board in my "basket" this morning and still haven't checked out. I'm still debating if I have the necessary time to dedicate to building it... I'm sure I won't be the only one. Hopefully at some point there will be a pre-built board. For me at least, cost is secondary to finding time for a project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Everybody, I asume, should be aware that asambling a circuit, is not a aesy thing to do.

    For me, I worked for several years in a electronic factory...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Looks a bit too complex for those new to computing and interfacing to computers. Anyone attempting to construct this board, and new to solding, should first try and make a few other circuits up first to get the hang of soldering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I just 'pre-orderd'. Waiting... Stll waiting ...

    Not yet, Not Yet ....

     

    (Is the flat cable included?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 14 years ago

    Looking forward to tinkering with the Gertboard!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<