Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Where is my lbr file?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 4342 views
  • Users 0 members are here
Related

Where is my lbr file?

e14 Contributor
e14 Contributor over 12 years ago

I'm new to Eagle and trying to use it for some projects I am working on.  I started a personal library, but I can't seem to find the actual file it is in.  I can see it in the Open dialog in Eagle, but it is not visible in Windows Explorer.  The file is present because if I try to create a new file in the library directory by that name, it reports a file already exists.  The thing I don't understand is the lock image on the file.  I attached a screenshot and marked two of these directories.  One of them is an old install of Eagle.  What is going on with this?

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    Am 11.07.2014 04:21, schrieb Elmo Clarity:

    I'm new to Eagle and trying to use it for some projects I am working

    on.  I started a personal library, but I can't seem to find the actual

    file it is in.  I can see it in the Open dialog in Eagle, but it is not

    visible in Windows Explorer.  The file is present because if I try to

    create a new file in the library directory by that name, it reports a

    file already exists.  The thing I don't understand is the lock image on

    the file.  I attached a screenshot and marked two of these directories.

    One of them is an old install of Eagle.  What is going on with this?

     

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/120013

     

     

    I do not see your image, but assume that you are working with

    Windows 7/8/8.1.

    The User rights manangement puts all your data into a roaming

    folder. This could be something like, C:\users\your_

    name_\Appdata\Roaming\Local\CadSoft\Eagle\.......

    Windows Explorer does not show these folders by default!

     

     

    Hope this helps.

     

    BTW: If you would install EAGLE not in the C\program files folder

    it would be less complicated to find such files. Then they would

    stored in the given EAGLE folders.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to autodeskguest

    On 2014-07-23 09:32, Richard Hammerl wrote:

    Am 11.07.2014 04:21, schrieb Elmo Clarity:

     

    BTW: If you would install EAGLE not in the C\program files folder

    it would be less complicated to find such files. Then they would

    stored in the given EAGLE folders.

     

    Reading such bullshit, I start to vomit. Guys! You can't be serious,

    writing such nonsense!

    It shows great ignorance of the ways programs should be written under

    Windows. Data like libraries and design files clearly do not belong in

    the "C:\Program Files" or "C:\Program Files (x86)" folders. This is a

    very well known fact, Cadsoft chooses to ignore for so many years. And

    suggesting to install a program into the root folder is really stupid at

    all. It has absolutely nothing to do there. No one would ever come up

    with such an idea on a Linux system. So why always try that under Windows?

     

    Carsten

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to autodeskguest

    On 26/07/14 11:27, Carsten Wille wrote:

    It shows great ignorance of the ways programs should be written under

    Windows. Data like libraries and design files clearly do not belong in

    the "C:\Program Files" or "C:\Program Files (x86)" folders. This is a

    very well known fact, Cadsoft chooses to ignore for so many years. And

    suggesting to install a program into the root folder is really stupid at

    all. It has absolutely nothing to do there. No one would ever come up

    with such an idea on a Linux system. So why always try that under Windows?

     

    All of which has a grain of truth and would be a reasonable argument

    (were it not clearly in the form of a flaming rant!) except for two things.

     

    The catastrophically stupid habit of putting program data in a

    subdirectory of "Program Files" was actually a Microsoft recommended

    practice on Win95.

     

    The apparently preferred alternative location, "Program Data", is also

    subject to Microsoft's "let's make everything madly confusing,

    impossible to find and even harder to control" folder virtualisation.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to autodeskguest

    Hello Rob Pearce !:

    ....

    The catastrophically stupid habit of putting program data in a

    subdirectory of "Program Files" was actually a Microsoft recommended

    practice on Win95.

     

    The apparently preferred alternative location, "Program Data", is also

    subject to Microsoft's "let's make everything madly confusing,

    impossible to find and even harder to control" folder virtualisation.

     

    Each Windows user which has a brain - will install nothing important on

    a system partition !!! Programs and data as well. In case of partition

    recovery need (MS Windows common sytuation after some time !!!) all this

    important programs/data will be destroyed !

     

    My personal recomendation is :

     

    One partition for system

     

    Another partition for programs,and maybe data - as in Eagle

     

    And other one for data ...

     

    But anybody can install as wanted. In any case the worst option is the

    MS recomendation - all in one system partition ...

     

    regards

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to autodeskguest

    Hello Rob Pearce !:

    ....

    The catastrophically stupid habit of putting program data in a

    subdirectory of "Program Files" was actually a Microsoft recommended

    practice on Win95.

     

    The apparently preferred alternative location, "Program Data", is also

    subject to Microsoft's "let's make everything madly confusing,

    impossible to find and even harder to control" folder virtualisation.

     

    Each Windows user which has a brain - will install nothing important on

    a system partition !!! Programs and data as well. In case of partition

    recovery need (MS Windows common sytuation after some time !!!) all this

    important programs/data will be destroyed !

     

    My personal recomendation is :

     

    One partition for system

     

    Another partition for programs,and maybe data - as in Eagle

     

    And other one for data ...

     

    But anybody can install as wanted. In any case the worst option is the

    MS recomendation - all in one system partition ...

     

    regards

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515