Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) in V6.0.0 manual routing got really hard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 190 subscribers
  • Views 4664 views
  • Users 0 members are here
Related

in V6.0.0 manual routing got really hard

e14 Contributor
e14 Contributor over 14 years ago

somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

5.11 didnt do this... i have messed with alot of settings, nothing seems to help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 16.12.2011 18:55, schrieb Mitch Solomon:

    somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

    5.11 didnt do this... i have messed with alot of settings, nothing seems to help

     

     

    Gentlemen, so far I have followed all this postings and noticed that

    there is is very little information about what machine and operating

    system you are using.

    I think to mention this would be a great help for cadsoft in eliminating

    these errors.

    I don't have this error on my windows xp sp3.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/01/2012 13:36, Joern Paschedag wrote:

    Am 16.12.2011 18:55, schrieb Mitch Solomon:

    >> somethings changed, when i manually route and click on the destination

    >> pad, if i dont click dead center now... im left with tiny tiny airwires

    >> 5.11 didnt do this... i have messed with alot of settings, nothing

    >> seems to help

    >>

    >

    Gentlemen, so far I have followed all this postings and noticed that

    there is is very little information about what machine and operating

    system you are using.

    I think to mention this would be a great help for cadsoft in eliminating

    these errors.

    I don't have this error on my windows xp sp3.

     

     

    Using the files linked-to in this thread I can reproduce the fault under

    Eagle 6.0.0 and Eagle 6.0.2 in Windows 7 x64.

     

    I was also seeing this leftover airwires problem on Linux x64 (but with

    a different (production!) board) using 6.0.0.

     

    The exchange of messages in this thread, between Jorge Garcia and Jason

    Tribbeck, suggests that the developers have all they need to be able to

    reproduce this.

     

    Hopefully 6.1 will nail it.  Hopefully soon!

     

     

    Andrew

    0xADF

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I've replicated this on 6.0.0 Mac OS, and Windows XP SP3, and 6.0.2 on Mac OS.

     

    Because this is a fairly UI independant operation, I would imagine it's across all operating systems (so I'm not surprised to see it in Linux).

     

    The video should show that it's Mac OS that I had originally found it on, but I'm sure if Jorge wanted to know what platforms it was failing on, he would've asked image

     

    It doesn't happen all the time, and it did take a while to come up with an example that is guaranteed to fail. It normally occurs when you're being complacent and not expecting it to happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to dukepro

    Hi Chuck,

     

    By default, you should receive email notifications for any discussion thread that you have posted in.  On this page, there is a Actions widget near the top on the right hand side where you can disable email notifications for this thread.  Additionally, you can view all your email notifications and disable as desired by clicking 'Manage email notifications' in the Actions widget on your profile page.

     

    There had been an issue with delivery of email from element14 that impacted some users.  This issue was resolved recently, and, thus, you may now be receiving notifications that you had not previously.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to e14 Contributor

    Why am I suddenly receiving email copies of posts?

     

     

    On 01/12/2012 01:49 PM, Jason Tribbeck wrote:

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 12.01.2012 15:22, schrieb Jason Tribbeck:

    I've replicated this on 6.0.0 Mac OS, and Windows XP SP3, and 6.0.2 on Mac OS.

     

    Because this is a fairly UI independant operation, I would imagine it's across all operating systems (so I'm not surprised to see it in Linux).

     

    The video should show that it's Mac OS that I had originally found it on, but I'm sure if Jorge wanted to know what platforms it was failing on, he would've asked image

     

    It doesn't happen all the time, and it did take a while to come up with an example that is guaranteed to fail. It normally occurs when you're being complacent and not expecting it to happen.

     

     

    As I wrote it was meant in general. (And not for this special case

    only). Sure cadsoft asks about details but then they have to wait for

    the answer which can take long wasted time. Is it really so difficuilt

    to mention the os? I'm also looking for a fast solution on the v6 trouble.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 12.01.2012 15:22, schrieb Jason Tribbeck:

    I've replicated this on 6.0.0 Mac OS, and Windows XP SP3, and 6.0.2 on Mac OS.

     

    Because this is a fairly UI independant operation, I would imagine it's across all operating systems (so I'm not surprised to see it in Linux).

     

    The video should show that it's Mac OS that I had originally found it on, but I'm sure if Jorge wanted to know what platforms it was failing on, he would've asked image

     

    It doesn't happen all the time, and it did take a while to come up with an example that is guaranteed to fail. It normally occurs when you're being complacent and not expecting it to happen.

     

     

    As I wrote it was meant in general. (And not for this special case

    only). Sure cadsoft asks about details but then they have to wait for

    the answer which can take long wasted time. Is it really so difficuilt

    to mention the os? I'm also looking for a fast solution on the v6 trouble.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to dukepro

    Hi Chuck,

     

    By default, you should receive email notifications for any discussion thread that you have posted in.  On this page, there is a Actions widget near the top on the right hand side where you can disable email notifications for this thread.  Additionally, you can view all your email notifications and disable as desired by clicking 'Manage email notifications' in the Actions widget on your profile page.

     

    There had been an issue with delivery of email from element14 that impacted some users.  This issue was resolved recently, and, thus, you may now be receiving notifications that you had not previously.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to e14 Contributor

    Why am I suddenly receiving email copies of posts?

     

     

    On 01/12/2012 01:49 PM, Jason Tribbeck wrote:

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!