somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
I've literally just spotted that - and worked out how to get it working (was about to post a new message!)
Basically, if you move a component, then the manual routing for that component gets difficult - it doesn't snap the wire to the pad centre.
What you need to do is click on the "Ratsnest" icon - this resets the ends of the air wires.
Or, you can abort your manual route half-way through, and then restart it from where you left off.
I'm beginning to think that V6.0.0 is a bit of a step backwards - and certainly doesn't seem to warrant a major version number upgrade.
ok, ill try, connecting two traces now is really hard, it wont snap to that
i do all my boards manually... and its really hard, id go back to 5.11
but i made a new part, and 5.11 dont like the part.... cause its xml now...
id think somthing simple as manual routing would be fully tested in 6...
it didnt take me but 5 seconds to know its not right
ok, ill try, connecting two traces now is really hard, it wont snap to that
i do all my boards manually... and its really hard, id go back to 5.11
but i made a new part, and 5.11 dont like the part.... cause its xml now...
id think somthing simple as manual routing would be fully tested in 6...
it didnt take me but 5 seconds to know its not right
"Mitch Solomon" <communitymanager@premierfarnell.com> wrote in message
news:1237833760.12311324062535598.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...
i do all my boards manually... and its really hard, id go back to 5.11
but i made a new part, and 5.11 dont like the part.... cause its xml
now...
I made a backup zip file of all my version 5 designs before even starting
version 6. If I want to go back, I can extract the necessary files and
restore them. No worries that something might get over-written or 'updated'
to xml.
Oppie
I think there may be some other triggers for it (such as zooming) - and I'm sure I've had to click it twice in some occasions.
I also do manual routing (I don't trust autorouters), so I bought the professional version without autorouting. It certainly doesn't seem as nice to use as 5.11 did.
(I'm intending to write a review of it later on, when I've had a bit more of a play with it).